• iWave's Expertise in Linux OTA (Over the Air) Update on Embedded Platforms

    Have you ever checked your smartphone or your IoT device and received an alert for software updates? All you have to do is to simply accept the update when you have the network connectivity and the rest will be taken ...
    iWave Systems
    last modified by iWave Systems
  • The Cortex® M4F: Enabling next-generation real-time processing in i.MX8QM SMARC System on Module

    iWave systems recently launched a new SMARC System on Module (SOM) based on the powerful NXP i.MX 8QuadMax applications processors. This high performance SOM features an intelligent blend of MPUs+MCU power in a s...
    iWave Systems
    last modified by iWave Systems
  • XEN virtualization on iWave’s i.MX8QM SMARC System on Module

    iWave Systems, a leading embedded solutions provider company based in Bangalore has successfully demonstrated Xen virtualization hypervisor on their i.MX8 QM SoC based System on Module. The  multi-core SOM compri...
    iWave Systems
    last modified by iWave Systems
  • 移植开源的密码工具箱GmSSL到i.MX平台

    GmSSL是一个开源的密码工具箱,支持SM2/SM3/SM4/SM9/ZUC等国密(国家商用密码)算法、SM2国密数字证书及基于SM2证书的SSL/TLS安全通信协议,提供符合国密规范的编程接口与命令行工具,可以用于构建PKI/CA、安全通信、数据加密等符合国密标准的安全应用。GmSSL项目是OpenSSL项目的分支,并与OpenSSL保持接口兼容。因此GmSSL可以替代应用中的OpenSSL组件,并使应用自动具备基于国密的安全能...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX

    GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secu...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • Do you have a Minute?

    The way in which people digest information is changing, as more distractions lead way to shorter attention spans and multi-tasking becomes even more important.  The new training series from NXP, i.MX RT Tech Minu...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • Sometimes Less is More

    As a marketer, I never like to use the suffix “less” as it usually has a negative connotation.  “Less” means not having; without; free from something. Words like hopeless, motionless, and ...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • MCUXpresso IDE v10.3.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all e...
  • Overview of using the MIMXRT1060(4)-EVK with MCUXpresso IDE

    Updated v1.02  1st March 2019   Please find attached a document detailing various features related to using the iMXRT1060-EVK evaluation board with MCUXpresso IDE v10.3.x and SDK v2.5, including details of...
  • MCUXpresso IDE v10.3.0 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.0 (build 2200) is now available.   This is a major new version of the IDE, and contains many new features and enhancements over the previous v10.2.1 and earli...
  • Overview of using the MIMXRT1020-EVK with MCUXpresso IDE

    First Release   Please find attached a document detailing various features related to using the iMXRT1020-EVK evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.   Yours,   MCUXpresso IDE Support
  • Overview of using the MIMXRT1050-EVK(B) with MCUXpresso IDE

    Now updated to v201   We have updated the attached document detailing various features relating to using the iMXRT1050-EVK(B) evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.x.   Also attached ar...
  • MCUXpresso IDE v10.2.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.2.1 (build 795) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.2.0 release, and we recommend that all e...