• XEN virtualization on iWave’s i.MX8QM SMARC System on Module

    iWave Systems, a leading embedded solutions provider company based in Bangalore has successfully demonstrated Xen virtualization hypervisor on their i.MX8 QM SoC based System on Module. The  multi-core SOM compri...
    iWave Systems
    last modified by iWave Systems
  • 移植开源的密码工具箱GmSSL到i.MX平台

    GmSSL是一个开源的密码工具箱,支持SM2/SM3/SM4/SM9/ZUC等国密(国家商用密码)算法、SM2国密数字证书及基于SM2证书的SSL/TLS安全通信协议,提供符合国密规范的编程接口与命令行工具,可以用于构建PKI/CA、安全通信、数据加密等符合国密标准的安全应用。GmSSL项目是OpenSSL项目的分支,并与OpenSSL保持接口兼容。因此GmSSL可以替代应用中的OpenSSL组件,并使应用自动具备基于国密的安全能...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX

    GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secu...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • Do you have a Minute?

    The way in which people digest information is changing, as more distractions lead way to shorter attention spans and multi-tasking becomes even more important.  The new training series from NXP, i.MX RT Tech Minu...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • Sometimes Less is More

    As a marketer, I never like to use the suffix “less” as it usually has a negative connotation.  “Less” means not having; without; free from something. Words like hopeless, motionless, and ...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • MCUXpresso IDE v10.3.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all e...
  • Overview of using the MIMXRT1060(4)-EVK with MCUXpresso IDE

    Updated v1.02  1st March 2019   Please find attached a document detailing various features related to using the iMXRT1060-EVK evaluation board with MCUXpresso IDE v10.3.x and SDK v2.5, including details of...
  • MCUXpresso IDE v10.3.0 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.0 (build 2200) is now available.   This is a major new version of the IDE, and contains many new features and enhancements over the previous v10.2.1 and earli...
  • Overview of using the MIMXRT1020-EVK with MCUXpresso IDE

    First Release   Please find attached a document detailing various features related to using the iMXRT1020-EVK evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.   Yours,   MCUXpresso IDE Support
  • Overview of using the MIMXRT1050-EVK(B) with MCUXpresso IDE

    Now updated to v201   We have updated the attached document detailing various features relating to using the iMXRT1050-EVK(B) evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.x.   Also attached ar...
  • MCUXpresso IDE v10.2.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.2.1 (build 795) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.2.0 release, and we recommend that all e...