• Certain networking packets cause memory leaks in Windows Embedded Compact 7 on i.MX53

    I have been tracking an elusive bug that causes the system to become unresponsive.   It has been proved that the bug is in the Ethernet area of the i.MX53 WinCE7 BSP which happens in certain network environments...
    Eugen Feraru
    last modified by Eugen Feraru
  • How to add custom system service to AOSP

    Hi Sir,   I am new to iMX and Android AOSP world and studying the Android System. I am using iMX8m mini board and i am able to download and build AOSP for Android 9 for this board.  Now i want to add simp...
    Maneesh Singh
    last modified by Maneesh Singh
  • MFG tool to read a file from imx28 

    whats the command to read from the imx28    i am using the following MFG tool version   i could able to dump the file from host PC to imx28 hardware, but not read from the hardware to PC   tri...
    shashikant h
    last modified by shashikant h
  • Not able to set Bootanimation for i.MX8m mini using Android 9

    Hello, I am having  i.MX 8M Mini EVK and have flashed Android 9 latest version 2.3.0 from NXP site https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/android-os-for-i....
    Sahil Kulkarni
    last modified by Sahil Kulkarni
  • if imx27 support WinCE 2013?

    Hi, I 'd like to check that if imx27 support WinCE 2013? I use it for WinCE6 and update it to WinCE7 in last years. But you know, WinCE 7 is going out of support. So I need do an update or change. There are lots of ...
    Kevin Qu
    last modified by Kevin Qu
  • Is there any documentation available for developing OpenCL application for GC7000Lite GPU on iMX8?

    Hi all,   I need to port an algorithm to OpenCL for execution on the GC7000Lite GPU available on iMX8. I could run execute and build a sample code on Windows MS Visual Studio 2013 environment using the vEmulato...
    Vinay V S
    last modified by Vinay V S
  • Mfgtool2 -noui process needs to be killed when done

    I am using the command line interface of MfgTool2 to program an I.MX6Q processor. This is done in a Windows batch script to simplify our manufacturing process that also involves some other activities, like FPGA config...
    Magnus Persson
    last modified by Magnus Persson
  • Why is MFG tool crashing (i.MX53)?

    I.MX53  Manufacturing tool  Problem      New  install  on Windows 10 Pro PC I downloaded the  Mfgtool file recommended for i.MX53 processors from the NXP website I r...
    Brian Peters
    last modified by Brian Peters
  • Mfg tool for i.MX28 not support USB3.0

    Hi all,   Follow mfg tool I download from freescale, I found it doesn't support USB3.0 PC, do you have any other updated version, or how to modify current version.... Mfgtools-Rel-1.6.2.048     Thank...
    gary lee
    last modified by gary lee
  • How to use nusensor from AOSP to test sensor HAL

    Hi Sir, I am using iMX8M Mini EVK and Android 9 AOSP Framework. I am successfully able to build the AOSP for my board and its running fine.    Now i want to connect DHT 11 sensor to this board at GPIO and...
    Maneesh Singh
    last modified by Maneesh Singh
  • Can't synchronize files from Windows to f_mass_storage

    Our bsp version is based on 4.14.98_2.0.1, I also tried 4.14.98_2.1.0, but still failed to synchronize files: ls command can't shows files created from Windows before rebooting board. Maybe remount should works, ...
    计龙 杨
    last modified by 计龙 杨
  • Hummingboard/Custom Carrier Board IoT Boot Issues

    This thread continues an earlier email conversation between a number of parties. It relates to IoT Core boot freezes where a Quad Core iMX6 Hummingboard has been placed in a third-pa...
    Andrew Kissling
    last modified by Andrew Kissling
  • RT1064 Flashloader to load application image

    Hello, I am working with the RT1064 Evaluation board and I am attempting to set it up to run an application via the MCUBOOT Flashloader (v2.7.0). First, I am generating the flashloader binary image using the els...
    Alin Butoi
    last modified by Alin Butoi
  • the problem when using mfgtool 2.7.0

    I download android_O8.0.0_1.0.0_tools in NXP, to update fw to my imx6sl evk board. if I using mfgtool 2.2.3, it can identify hid device. but using mfgtool 2.7.0 can't identify hid device, before hid d...
    张 松源
    last modified by 张 松源
  • SARBE - iMXS6X-SDB: ethernet - Link is Down

    Hi Team, i am working on iMXS6X-SDB board with our custom linux kernel image version 3.14.28. I have some python reboot tests which gives the reboot command via ssh, waits for some time and this cycle repeats. &...
    PRANAV MONDHE
    last modified by PRANAV MONDHE
  • Why is i.MX53 BulkIO device changing to USB Mass Storage device when I run MFG tool?

    Running  MFG tool  rev 1.6.032  on a windows 10 upgrade of a windows 7 PC with no usb3 ports, every thing is configured correctly best I can tell.  The target board shows up as a  'Freesc...
    Brian Peters
    last modified by Brian Peters
  • The Manufacturing Tool failing to flash

    I'm trying to use the Manufacturing Tool MfgTool2.exe to flash my MCIMX6Q-SDB SABRE board, I've tried both SDCard and eMMC and I'm getting the same results, the tool hangs during the partition step.   From the D...
    Michael Worster
    last modified by Michael Worster
  • MX8MM won't enter fastboot mode

    Hello, I'm using MX8M Mini EVK with Android 9, under Windows 10. *ADB works* fine but I have a real trouble getting into fastboot mode.  I researched hard in all NXP docume...
    mike malgin
    last modified by mike malgin
  • How to run CVE checker on yocto image for iM6SX

    Hi Guys We are using customized yocto linux kernel and running some C++ code for industrial application.   Where i can find CVE (Common Vulnurabilites and Exposures) tools to check for my custom-ed yocto i...
    PRANAV MONDHE
    last modified by PRANAV MONDHE
  • iMX6S Sabre - Frequency stop was detected, probably due to a supply voltage drop

    Hi Guys I am running iMX6 Sabre board with latest yocto image running our C++ software on top of it. While testing, i understand that we are getting frequency stop messages on dmesg   Can you please go through...
    PRANAV MONDHE
    last modified by PRANAV MONDHE