• i.max6 android Ethernet app add eth1

    您好,我正在使用i.max6 (android 6.0.1) 我的裝置上原本就有一個ethernet(eth0) 並且可以透過NXP內建Ethernet app控制eth0 例如使用stacic IP 和DHCP, 而我現在增加了一個裝置USB to Ethernet(eth1) 因此我想要讓eth1也可以透過Ethernet app來設置static ip 但是app裡並沒有eth1的選項 請問app要如何新增一個...
    minyou Hou
    last modified by minyou Hou
  • No HDMI output on SCM-i.MX6DQ

    Hello, I've got a SCM-i.MX6DUal/6Quad Quick Start Board and followed the Quick Start Guide. Unfortunatelly, I do not get any output on two different Monitors connected to the HDMI port. Both monitors work with any ot...
    Stephan Hoffmann
    last modified by Stephan Hoffmann
  • How to download Linux image files through the usb2.0 interface on imx8qm

    Hi NXP:           By default,Imx8qm dewnload linux image files through the type-C interface. As shown in the picture "Default Download". But now i want download linux image files througt the ...
    yingjin yan
    last modified by yingjin yan
  • How to build json on Yocto

    Hi, I am having iMX8M Miini EVK and I am able to build - "core-image-minimal" yocto image for iMX8M Mini.  I am following all the steps given in user guide -         ...
    Maneesh Singh
    last modified by Maneesh Singh
  • I.MX8MMini: OPenCV and QT5

    Hi,   as i am working on neural network and AI, i want to know Does openCv and QT5 package support on the I.MX8mmini board,   If yes, how do we add in yocto   Regards Santhosh
    Santhosh Kumar
    last modified by Santhosh Kumar
  • agl nxp 4.9.88-2.0.0 compile error

    $bitbake agl-demo-platform   ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package: /lib/systemd/system/psplash-network.serv...
    guang zeng
    last modified by guang zeng
  • CDC MBIM Support

    how to add the cdc mbim support of linux3.0.35 kernel?
    yuhundehao yuhundehao
    last modified by yuhundehao yuhundehao
  • QSPI Flash RT1050 failure

    Dear,   I'm working on a project with the NXP i.MXRT1050 family MIMXRT1052DVL6B processor. For preliminary testing I'm using the MIMXRT1050-EVK development kit. For the initial tests we are using the SDX provide...
    Rubens Junior
    last modified by Rubens Junior
  • i.MX6DQPOP Thermal Design

    Is there a thermal design guide for the i.MX6DQPOP products?  Maybe something similar to section 6 in the IMX6DQSCMHardwareDevelopersGuide? Are the POP parts closer to the SCM in regards to thermal management th...
    AMANUEL TIBEBU
    last modified by AMANUEL TIBEBU
  • Why new kernels is worse than previous ones?

    Hello Everybody  I tried to find best kernel.I have  three different kernel version which i tested on same board IMX6Q with QT cinematic experience app.There are huge differences each others. Firstly Kernel...
    Muhammet Emin ŞAHİN
    last modified by Muhammet Emin ŞAHİN
  • SGTL5000 INTERFACING WITH SPI THROUGH MSP430F5529

    Hello Every one, Good morning to all   I am using a sgtl5000 in my console mixer project, I have interfacing through spi , Also I have set all the registers of sgtl5000 , but it doesn't respond any thing.  ...
    vikash chandra raman
    last modified by vikash chandra raman
  • Opencv - based image acquisition, qt display

    Opencv - based image acquisition, qt display Everybody is good Imax6q board, qt creator of 5.9.5, kernel 4.1.15   I collect the camera of v4l2 with opencv and display it with the label of qt.Currently it can be ...
    袁 野
    created by 袁 野
  • Patching u-boot "can't find file to patch", how to fetch source?

    I'm trying to patch mx6dqscm.c in u-boot IMX with a bbappend file in my custom layer. I get the following error: ERROR: u-boot-imx-2016.03-r0 do_patch: Command Error: 'quilt --quiltrc /home/ubuntu/imx6/ build-x11/tmp/...
    Steven Snyder
    last modified by Steven Snyder
  • HID detection issue

    I have been facing HID Detection issues. Few boards get detected. Whereas the detecting boards are found to have the same issue sometimes. There are no hardware changes that can be differentiated between detecting and...
    Annie Varshitha
    last modified by Annie Varshitha
  • IMX6 CSI Register Settings on Linux

    Hi   How can i see the csi registers in linux command line? If i need to update any kernel or u-boot code is ok for me.   I just want to see    IPU_CSI_SENS_FRM_SIZE IPU_CSI_ACT_FRM_SIZE IOMUX...
    ümit kayacık
    last modified by ümit kayacık
  • How to get clock on CCM_CLKO1 for imx6q

    Hi,   I am working on imx6q board. I am trying to get clock on CCM_CLKO1 (D16 Pin) 24MHz or 12MHz.   while ov5640_mipi is loading i am getting clock for 1 sec later it is disabled. Some times it is showing...
    Vasu Sriram
    last modified by Vasu Sriram
  • How to configure RDC?

    The board what i used is i.MX 8MQuad Assessment Suite, And the MCUXpresso SDK is version 2.6 Now i testting Contex m4 pwm demo with pwm4 which under driver_examples folder. It will be successful output waveform when ...
    yingjin yan
    last modified by yingjin yan
  • IMX6 VIDIOC_DQBUF failed issue

    Hi,   While tring below commands my v4l driver generates below error.   ./mxc_v4l2_tvin.out -ow 720 -oh 480 -ot 20 -ol 20 -c 10 -m 0 -tb -f YUYV   ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_coun...
    ümit kayacık
    last modified by ümit kayacık
  • Sabre Imx6q BT656 video capture with NVP6124

    Hi,   I want to take video from analog camera(ahd) with NVP6124 and display it on HDMI. I made the connection of 8bits data to CSI port (OV5642 connected side) and communication via I2C seems OK that i tested it...
    ümit kayacık
    last modified by ümit kayacık
  • SARBE - iMXS6X-SDB: ethernet - Link is Down

    Hi Team, i am working on iMXS6X-SDB board with our custom linux kernel image version 3.14.28. I have some python reboot tests which gives the reboot command via ssh, waits for some time and this cycle repeats. &...
    PRANAV MONDHE
    last modified by PRANAV MONDHE