• i.MX Power Profiling System: Instrumenting A Board

    Instrumenting A Board To instrument a board, the connection between the power supply and the target device needs to be broken, usually via a series resistor that's placed on the board. Sometimes the inductor needs to ...
    David G Dicarlo
    last modified by David G Dicarlo
  • How PF1550 can discharge lithium battery only when VBUSIN is lost?

    We have a design with a PF1550 PMIC. System is powered by a main power feeding VBUSIN almost permanently and a rescue lithium-ion battery. Our goal is to keep our rescue battery charged in case mai...
    Anthony Loiseau
    last modified by Anthony Loiseau
  • i.MX Power Profiling System: Smart Current Sensor and Aggregator Shield

    NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator.   NOTE: See this link to instrument a board with a Smart Sensor.   Over...
    David G Dicarlo
    last modified by David G Dicarlo
  • i.MX Power Profiling: Triple-range Smart Current Sensor

    NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator.   NOTE: See this link to instrument a board with a Smart Sensor.   This...
    David G Dicarlo
    last modified by David G Dicarlo
  • [i.MX6] Suspend/resume implementation for dw_hdmi-imx.c

    Hi, I am having imx6 Dual board with Linux Kernel 4.9 running on it. It is also connected to HDMI display. But, I see that suspend/resume implementation is missing from imx hdmi driver: drivers/gpu/drm/imx/dw_h...
    PINTU KUMAR
    last modified by PINTU KUMAR
  • How to run CVE checker on yocto image for iM6SX

    Hi Guys We are using customized yocto linux kernel and running some C++ code for industrial application.   Where i can find CVE (Common Vulnurabilites and Exposures) tools to check for my custom-ed yocto i...
    PRANAV MONDHE
    last modified by PRANAV MONDHE
  • iMX6S Sabre - Frequency stop was detected, probably due to a supply voltage drop

    Hi Guys I am running iMX6 Sabre board with latest yocto image running our C++ software on top of it. While testing, i understand that we are getting frequency stop messages on dmesg   Can you please go through...
    PRANAV MONDHE
    last modified by PRANAV MONDHE
  • dpms mode change with wayland on iMX.6

    drm imx-drm etnaviv wayland imx6 processor   Hi, Can someone tell me how to change DPMS mode for Wayland based display system ?   I have a iMX.6 (arm 32) board with custom Linux Kernel 3.10 (and heavily p...
    PINTU KUMAR
    last modified by PINTU KUMAR
  • i.MX Power Profiling System: Aggregator Shield Details

    NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator.   The aggregator portion of the i.MX Power Profiling System sits between the...
    David G Dicarlo
    last modified by David G Dicarlo
  •     iMX8QM A0 CPU Soft Reset Issue

    Hi,   We are working on iMX8QM custom board with 4.14.98 Kernel BSP release with 'imx-scfw-porting-kit-1.2' SCFW. The iMX8QM B0 CPU is able to do soft reset (reset command in u-boot & reboot command in kerne...
    prashanth kumar
    last modified by prashanth kumar
  • Android(Nougat) UI not comming

    I am working with IMX6solo processor, and I bring-up the board with Android Nougat, and upto filesystem its fine, but Android UI is not comming, I don't know why I got this issue anybody have suggestion please let me ...
    Winston Jacob
    last modified by Winston Jacob
  • i.MX8Mmini EVK SNVS RTC can't backup

    Hi     We test CPU SNVS RTC backup function. When we set "reboot" command. We see CPU date in first login time.   BSP is Linux-4.14.78 We use 4.14.78 default demo image       Log fi...
    Apollo Chang
    last modified by Apollo Chang
  • PF3000 and IMX6SX bsp

    Hi,   We are developping a board based on Imx6SXSabresd. I downloaded Freescale bsp and followed "i.MX_6_BSP_Porting_Guide.pdf" and "Freescale_Yocto_Project_User's_Guide.pdf". I get the sources with "repo init...
    Florian GERMAIN
    last modified by Florian GERMAIN
  • IMX8M WoWLAN(Wake on WIFI) from Low power mode(Ideal DDR167MHz) and USB wake-up disable

    Dear Team,   I am using IMX8M Eval board,One of my use case I need to wake-up this system from WIFI WoWLAN (USB-WIFI dongle).     I am putting system into low power mode(IDEAL DDR-167MHz mode): -----...
    Venkatesh P
    last modified by Venkatesh P
  • PMIC for i.mx6 ULL

    PF3000 vs PF3001 on i.mx6 ULL   Our board is very similar to the evaluation board:  https://community.nxp.com/docs/DOC-339884 but we have the ULL processor instead of the UL.  I can't undestand the ...
    Elisa Sacchi
    last modified by Elisa Sacchi
  • Why INTB in PF100 regulator is always low

    Hi,   I'm using iMX6 and PF100 regulator. The PF100 INTB is connected to iMX6 GPIO0. I found the INTB is always low, even there is not any interrupt is unmasked. What causes the INTB to be in low state?   ...
    Yan Gao
    last modified by Yan Gao
  • LDO-Bypass affecting i.MX WDT, enabled in U-Boot

    Hello folks,   We're using 4.14 GA release for i.MX6Q SabreSD rev 1.2. Our use-case dictates enabling the WDT in U-Boot, and ping it in userspace via systemd. So we do by enabling IMX_WATCHDOG, HW_WATCHDOG and s...
    ehson
    last modified by ehson
  • The status of FET in PMIC_ON_REQ pin

    Hi all,   I have a question about the status of FET in PMIC_ON_REQ. The FET of PMIC_ON_REQ will be open drain when the voltage of VDD_SNVS_IN is input. Am I correct ?   The FET stay GND before the voltag...
    ko-hey
    last modified by ko-hey
  • MMPF0100F1AEP Coin Cell polarity protection

    MMPF0100F1AEP Coin Cell polarity protection - is there any need for polarity protection on the coin cell input?
    Paul Sayles
    last modified by Paul Sayles
  • MMPF0100NPAEP Power-off

    Hi, We are using MMPF0100NPAEP for powering a general purpose SoC. PWRON is connected to VSNVS (1.8V) using a pull-up resistor and a pushbutton switch and in OTP, PWRON_CFG bit is set to 0.   When VIN power is a...
    Naveen HN
    last modified by Naveen HN