• Missing iMX 8M Mini support for Media controller API

    Hi, I am using iMX 8M Mini with several MIPI CSI sensors (OV, IMX). The Linux kernel is based on codeaurora imx_4.19.35_1.1.0 (v4.19.35-5188-g8507afc3a397).   It's very important to have the media controll...
    Krzysztof Kozlowski
    last modified by Krzysztof Kozlowski
  • eglinitialize depends on /dev/galcore and not available for sometime causing delay in weston boot

    NXP BSP Version: is4.14.98_2.0.0_ga U-Boot and kernel completes @ 3.7sec. systemd started galcore module. and in parallel weston started. Weston takes 1.2sec to complete initialization. But if we delay weston sta...
    Arunkumar Rajagopal
    last modified by Arunkumar Rajagopal
  • Android 9(Pie) Bringup issue on imx based custom Board : Problem with surfaceflinger

    Hi, We are trying to bringing up Android 9-pie on imx based custom board. We are facing problem with board bring up. Device is not booting properly and continuously rebooting. We noticed problem with surfaceflinger. S...
    aks aks
    last modified by aks aks
  • Custom camera driver adaptation on iMX8M Mini

    Dear experts,   I'm in the process of porting a custom camera to iMX8M Mini from its original driver dedicated to Nvidia Jetson platforms. I've finished the control part via I2C bus. However, I've got following...
    Khang Le Truong
    last modified by Khang Le Truong
  • IMX8MM - MIPI CSI 

    Hi,  The IMX8MM board configuration fsl-imx8mm-evk.dts file is configured to mipi ov5640 camera.   I am using high defination HDMI camera and using bridge IC  converting from HDMI to MIPI data. The M...
    Santhosh Kumar
    last modified by Santhosh Kumar
  • Occasional Rolling Video mx6 & adv7282-m

    Hello,   There is some relation to this questions and other posts on this forum, i figured it would be best to start a new thread though?  So i have followed advice on posts like this one:  iMX6, ...
    Jarrod Cook
    last modified by Jarrod Cook
  • reboot and shutdown are not working in custom imx7 board..?

    Hi all,   i am working on custom board base on imx7d, my board is freezing after a while when i reboot or shutdown, also i tried reset command from uboot here also it is freezing can anyone suggest me any solut...
    Flaby Jacob
    last modified by Flaby Jacob
  • Flashing i.MX8M Nano EVK using UUU Tool

    Hello,    I am trying to flash i.MX8M Nano EVK using UUU Tool on Ubuntu 16.04. I have configured boot switches to Serial Download Mode and connected USB cable and Power. I am giving following command: $ sud...
    Rohan Mathuria
    last modified by Rohan Mathuria
  • ISL79987 and adv7180 de-interlace driver for iMX8QXP boards

    adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • i.MX6 Quad PCI-E hang issue

    Hi,   We have encountered a hang issue regarding PCI-E initialization/enumeration using our i.MX6 Quad custom board.   This is the part where we encounter the issue. imx6q-pcie 1ffc000.pcie: PCI host bridg...
    Benedick Montales
    last modified by Benedick Montales
  • OTA upgrade for smartlocker in i.MX7ULP kernel

    This package is a OTA upgrade implementation for smartlocker in i.MX7ULP kernel. The bootaux command for i.MX7ULP can also be applied to other projects. File description: smartlocker OTA upgrade user manual. Modifie...
    terry_lr
    last modified by terry_lr
  • IMX8QM-MEK Power Management difference between Linux and Android

    Dear NXP,   I got observation when I try to send  suspend-to-ram command ( echo mem > /sys/power/state ) from Android and Linux   Suspend to Ram in Android OS,       ...
    vinothkumar s
    last modified by vinothkumar s
  • imx8mq接三星evo 970 ssd硬盘

    各位版主好,请问imx8mq的usb1作为3.0的host,接ssd固态硬盘出现这个现象是什么问题导致的?   有时候又出现这个信息
    小辉哥
    last modified by 小辉哥
  • How to use kdump in signed kernel

    Dear Team,   Currently, I'm using i.Mx8x based custom board. BSP version is, imx-yocto-L4.14.98_2.0.0_ga.   My query is, I want to capture the crash log when the ker...
    Raana
    last modified by Raana
  • How to capture crash log using kdump

    Dear Team,   Right now, I'm using i.Mx8x based custom board. BSP version is, imx-yocto-L4.14.98_2.0.0_ga   There I'm trying to capture the crash log of my standard kernel if any panic occurs. I'm using '...
    Raana
    last modified by Raana
  • generate DEK blob from user space command line?

    Trying to use encrypted secure boot. All works, but I want to be able to generate a DEK blob while sitting at the Linux command prompt on the device itself. I understand that I am able to burn fuses and lock the proce...
    Colby Conklin
    last modified by Colby Conklin
  • Custom boot.img with android_p9.0.0_2.3.0

    Hello! We're attempting to create a custom boot image alongside other pre-made image files for a custom Android build. Currently, we're using the IMX8mm EVK for development and separate hardware that we've written c...
    Dylan Johnson
    last modified by Dylan Johnson
  • Yocto imx8m tensorflow-lite

    I would like to build C++ code and use tensorflow as a library. What do I have to ad to the Yocto image recipe to have header and required libs in SDK?  For the rootfs it seems that IMAGE_INSTALL += "...
    Arno Steffens
    last modified by Arno Steffens
  • Booting sequence of IMX8QM-MEK

    Dear NXP,   Will you please give me the short notes for booting sequence of IMX8QM-MEK with Arm Cortex-M4.   Some times resources (Display and Camera)  are occupied by Arm Cortex-M4     ...
    vinothkumar s
    created by vinothkumar s
  • Parallel RGB driver is not worked on i.MX8QXP MEK board

    Hello experts, In order test imx8qxp parallel RGB LCD Interface, I download  L4.14.98_2.3.0_images_MX8QXPMEK.zip from nxp site and test it on imx8qxp mek board as below steps: 1. hw board:  imx8q...
    Ping Wu
    last modified by Ping Wu