• Udoo Neo Full is loading imx6q-udoo-hdmi.dtb

    Hi Everyone! I'm newbie in linux system! After checking /sys/var/term.log, I saw linux OS of my udoo board, it load imx6q-udoo-hdmi.dtb and it dose not load any *.dtb file in /boot/dts folder. I tried to at this li...
    Anh Pham Tuan
    last modified by Anh Pham Tuan
  • PMIC read error | imx6q sabreAI

    Hi All, I am working on imx6q based sabre AI custom board, running android 7.1.Everything works fine on our first version but in our latest version of our custom board,it is showing PMIC read and write error and boot...
    RICHU C J
    last modified by RICHU C J
  • Downloading binary to SDCARD(SD4 Slot) using MfgTool on the MCIMX6SX-SDB board

    Hi,   I'm using MfgTools in Windows 10. The MfgTool_MultiPanel(Library: 2.7.0) was performed by executing the mfgtool2-yocto-mx-sabresd-sdcard-sd4.vbs of L4.9.88_2.0.0_mfg-tool. LOG : MfgTool_Initial.log ...
    DongHyun Kim
    last modified by DongHyun Kim
  • console log do not output after uart cable plug out and re-connect

    Dear Nxp       i use the imx6solo and  run the linux , the kernel is 4.14.78.       the ttymxc0 is the debug port, i pass the parameter "console=ttymx...
    Vecio Lin
    last modified by Vecio Lin
  • i.max6 android Ethernet app add eth1

    您好,我正在使用i.max6 (android 6.0.1) 我的裝置上原本就有一個ethernet(eth0) 並且可以透過NXP內建Ethernet app控制eth0 例如使用stacic IP 和DHCP, 而我現在增加了一個裝置USB to Ethernet(eth1) 因此我想要讓eth1也可以透過Ethernet app來設置static ip 但是app裡並沒有eth1的選項 請問app要如何新增一個...
    minyou Hou
    last modified by minyou Hou
  • i.MX6SX can not get into the steady link state with x86

    Greetings,   Hereafter we ourself are debugging the issues about pcie between imx6sx and x86, after configuring the pcie clock, device type(EP mode) and inbound in imx6sx, data can be accessed into imx6sx f...
    zengxing yuan
    last modified by zengxing yuan
  • I.MX8MM (Mini) cannot find eMMC slot.

    Hi communicators.   I knew how can porting the OS from i.mx8 board. (as SD Card) (As you may already know, sdcard is mmc. and emmc is embeded mmc.)   I recently completed to porting Android OS through SD ...
    lim eon
    last modified by lim eon
  • SDMA support for SAI in iMX6 SoloX

    Hi, I have been trying to add support for SDMA in the SAI driver for iMX6SX. I am using the SAI1 interface for TX of audio data. The SAI driver is functional with interrupts mechanism of transfers and i can successful...
    Mahad Saleem
    last modified by Mahad Saleem
  • LCD and GPU on i.MX6Solox

    Hi NXP,  I need to understand differences between i.MX6Solox SoCs part no.  MCIMX6X1CVO08AC  and MCIMX6X3CVO08AC in terms of LCD interface. After reading information about LCD interface of the...
    Musadjan Alim
    last modified by Musadjan Alim
  • Wake Up A9 core from the Sleep in imx6sx

    Hi,   We are using imx6sx custom board and we need sleep and wakeup functionality based on  GPIO interrupt. Our requirement: 1) put linux into sleep mode using echo mem > /sys/power/state command,...
    Nilesh Patel
    last modified by Nilesh Patel
  • SDK for IMX6 SDMA

    Hi, I have been working on developing SDMA driver for IMX6 SoloX. I am unable to trigger memory to memory SDMA transfers. Can i get a reference driver implementation or SDK for IMX6 SDMA driver?   Thanks!
    Mahad Saleem
    last modified by Mahad Saleem
  • LCD interface and GPU of i.MX6Solox

    Hi NXP and Community friends,  I need to understand differences between i.MX6Solox SoCs part no.  MCIMX6X1CVO08AC  and MCIMX6X3CVO08AC in terms of LCD interface. After reading information abou...
    Musadjan Alim
    last modified by Musadjan Alim
  • imx-yocto-L4.14.98_2.3.1 Release Notes

    Hello,   I have a question about the release notes of imx-yocto-L4.14.98_2.3.1. You have written that the tested version for imx-gpu-g2d is 6.2.4.p4.8. I am unable to request the file because it cannot be found....
    Patrick Jakob
    last modified by Patrick Jakob
  • i.MX6Qsabresd Board and  Murata 1MW WiFi/BT connection problem

    I connected the two boards to page 28 of themurata_quick_start_guide_linux.pdf manual.At the same time, I built the new mirror file as described in the following post in the community https://community.nxp.com/th...
    zh_y
    last modified by zh_y
  • Need document perform encryption on IMX6Q and IMX6SX based boards

    HI All, We are working on product based on imx6q and imx6sx for that we have requirement of to encrypt rootfs partition. I am trying to access following document but it seems that I am not authorized to access these ...
    Jemish Patel
    last modified by Jemish Patel
  • Facing issue in yocto zeus u-boot compilation

    Hi Experts,   I downloaded and successfully compiled the "core-image-base" for yocto zeus, I am able to compile the standalone kernel with some modification. Similarly when i am able to compile the u-boot even w...
    Nikhil sahu
    last modified by Nikhil sahu
  • MCIMX6ULL-EVK + LCD 8K3T board hangs during boot-up

    Hi All, Please could someone help, I'm new to Linux !! Would be great to start with an out of the box working platform.   Boot error: U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Nov 05 2016 - 01:13:3...
    Richard Seymour
    last modified by Richard Seymour
  • How to include memtool in the core-image-base ?

    Hello guys,   We are trying to include the memtool utilities from imx-test packages, but I can't figure out how to do it. Hereunder is the content of my local.conf file :   MACHINE ??= 'imx6ulevk' DISTRO...
    matt67
    last modified by matt67
  • i.MX Android常见问题解答

    [中文翻译版] 见附件   原文链接: i.MX Android Frequently Asked Questions 
    Leo Lin
    last modified by Leo Lin
  • 如何理解i.MX6Q ESAI模块的“多个重置功能”

    [中文翻译版] 见附件   原文链接: How to Understand "Several Reset Functions" Of i.MX6Q ESAI Module 
    Leo Lin
    last modified by Leo Lin