• Yocto error : sh: no job control in this shell

    I'm getting the error "sh: no job control in this shell" when i run my custom yocto image. I found out after some experiments and test that adding an IMAGE of one of my drivers in the local.conf file is making my imag...
    Hector Sanchez
    last modified by Hector Sanchez
  • OV5640.C   Questions to ask

    Hi: now I have a problem. i'd like to add a new one sensor,  the new sensor does not need to be initialized. Do I need to refer to OV5640.c? help me ,thank you!
    袁 野
    last modified by 袁 野
  • Pad register value for i.mx6

    Hii, How do we determine/set the value of pad register value in dtsi file?? I mean how do we calculate it exactly?? For example,  MX6QDL_PAD_KEY_COL2__FLEXCAN1_TX    0x1b0b0, On which factor is the&...
    deexithamba@gmail.com
    last modified by deexithamba@gmail.com
  • How does the IMX6 SPI use DMA to transfer data?

    Hello everyone I am using the IMX6Q development board of NXP official website. When I was using SPI for communication, I found that the SPI only uses DMA transfers when the bytes I transfer are larger than 64 bytes. W...
    其东 刘
    last modified by 其东 刘
  • iMX6Q display adjustment

    Hi   I would like to control of display brightness, contrast, hue and color saturation on iMX6Q. But I could not find the control interface on kernel sources. Is there any sample source code or documents ? &#...
    Taro Yamamoto
    last modified by Taro Yamamoto
  • Patch for iMX6 BSP to support interlaced display on HDMI and LCD interface

    1. Description     1) Support HDMI interlaced display mode, the followed format had been verified.         CEA format 5: 1920x1080i @60Hz     ...
    Qiang Li - Mpu Se
    last modified by ebiz_ws_prod
  • 4GB RAM with GPU - Galcore driver issue

    hi,   We are using a IMX6 Quad core SOM with 4GM RAM. we are using the Vivante/galcore driver and having problems with the integration if we are using the 4GB RAM. If we limit the kernel(in linux OS) to hav...
  • Board Lock-Up on Watchdog Reset

    Developed a custom board based on the i.MX6Q. We are using the internal watchdog timer and the watchdog reset works fine when we perform a reboot command.The WDOG_B signal is being routed to the POR signal of the i.MX...
    Paul DeMetrotion
    last modified by Paul DeMetrotion
  • I.MX6Q of HDMI hardware design

    I have a client who wants to project our display using HDMI,I refer to the design board,I find that need IC of CM2020,Can we not use this IC design?Whether there is a reference design?
    tommy duan
    last modified by tommy duan
  • Oreo BTcrash, unable to get scan results on Android GUI

    Hi,   I am porting our BT module into OREO, able to ON BT from GUI and getting BT device MAC address,but I am unable to get list of BT scanned devices on GUI, I am seeing this crash on logcat, Please help me to ...
  • IMX6Q Android8.0 Ethernet Static IP Not work

    Hi, I have one imx6q device which run Android 8.0 system, I need to set Static IP, so I use com.fsl.ethernet to do that, I can set the right IP, but I can't communication to other. I use follow command to test: ...
    leavs lee
    last modified by leavs lee
  • I.MX6Q Mic. Recording Problem!!

    Good Day! My name is Jason Oh from Korea(South).   I have ported android 7.1.2 successfully to our custom  i.mx6q board. CPU       : i.MX6Q OS     &...
    Jason Oh
    last modified by Jason Oh
  • Can someone help me,ERROR: ExpansionError during parsing /home/imax6/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-graphics/vulkan/vkmark_1.0.bb

    When I first compiled it,i have the error, ERROR: ExpansionError during parsing /home/imax6/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-graphics/vulkan/vkmark_1.0.bb   The project has been com...
    袁 野
    last modified by 袁 野
  • Question about VPU EncOpenParam

    Hi all,     Let me ask about a EncOpenParam for VPU operation.   Q1. If EncOpenParam's bitRate is set to something other than "0", will it exceed the specified bitRate? * Will it be controlled at a ...
    ko-hey
    last modified by ko-hey
  • yocto  add pam module

    hi,    How can make the  pam module to rootfs?  i use imx6  yocto enviroment!   1. i  add this in the local.conf  IMAGE_INSTALL_append += " pam"   2. then,  b...
    一海 陈
    last modified by 一海 陈
  • Any way to reboot i.MX6 via MfgTool2 WITHOUT returning to serial download mode?

    I am attempting to reboot an i.MX6 based system after deploying new uboot/kernel/rootfs images via MfgTool2.  I am not on location, so I don't have access to the physical unit in order to perform a hardware reset...
    Erik Schumacher
    last modified by Erik Schumacher
  • Serial communication permissions Nitrogen 6x Android 7.1

    I am trying to configure a Nitrogen 6x board (uses i.MX6 quad processor) running Android 7.1 to communicate with another board via Serial Port.  I am getting a permission denied error within the application I am ...
    Jonathan Nisbet
    last modified by Jonathan Nisbet
  • RTOS & Linux in i.MX6 quad

    Hi,   We're planning to transfer our app from OMAPL138 dualcore to a modern environment. i.MX6 dual/quad core is a very potential candidate. We need to run RTOS in at least one core while rest of the cores are r...
    Risto Hedman
    last modified by Risto Hedman
  • i.mx6q RGMII DATA IO LEVEL

    I use i.mx6q as my cpu,now i want to use RGMII,and i know its working electric level is 1.5V. The RGMII IO link to a ETH Switch,but the ETH Switch is working at 3.3V,2.5V or 1.8V. How can i use the RGMII at this sit...
    REN YUNSAI
    last modified by REN YUNSAI
  • IMX6Q EIM (16bit :D0~D15) problem

    We're using i.MX6Q with EIM interfacing to an FPGA, using synch 16 bit none multiplexed mode with burst mode. we use EIM_D0~EIM_D15 as DATA bus; address and data bus work well except EIM_D6 and EIM_D7:   when i...
    jianmin li
    last modified by jianmin li