• lost async page write and murata wifi

    Hi. I have an imx6qp_sabrea board and I am testing with android_p9.0.0_2.2.0-ga demo image.   First question I want to have write permission to the / vendor folder. If you do "mount -o remount, rw / vendor", yo...
    An jin ho
    last modified by An jin ho
  • imx-yocto-L4.14.98_2.3.1 Release Notes

    Hello,   I have a question about the release notes of imx-yocto-L4.14.98_2.3.1. You have written that the tested version for imx-gpu-g2d is 6.2.4.p4.8. I am unable to request the file because it cannot be found....
    Patrick Jakob
    last modified by Patrick Jakob
  • fail to download, mfgtool

    Hi. I have an i.mx6qp sabrea board and I want to download Android Q8.0.0_1.0.0 demo image. I downloaded 2 mfg tools. 1.https: //www.nxp.com/webapp/Download? ColCode = ANDROID-THINGS-MFG_TOOL & location = null 2....
    An jin ho
    last modified by An jin ho
  • rcu_sched detected stalls on CPUs/tasks

    Hi,all:    I'm meeting a very serious problem on the chip of imx.6(linux version:4.1.15)。the system maybe suspend when run sometimes, and print rcu stall in sometimes just as show below,is anyone meet ...
    hongjian zhao
    last modified by hongjian zhao
  • Why do SDK libraries and rootfs ones should match?

    Hello guys,   I am curious about the above subject, and I couldn't easily understand that. when I build my app with SDK and make executable file, this file means a just binary and can executable in target machi...
    Yibeom Han
    last modified by Yibeom Han
  • opencv with gstreamer in VideoCapture doesn't work

    Hello guys, I have built imx-image-multimeia in yocto(kernel 5.4.3.1) and added opencv some packages such as CORE_IMAGE_EXTRA_INSTALL += " opencv-apps opencv-samples python3-opencv".   and then bitbake ima-ima...
    Yibeom Han
    last modified by Yibeom Han
  • I can't set Target Architecture in Yocto Projcet ADT in preferences in eclipse

    Hello NXP community, I got some problem to install eclipse setup for sdk in yocto. I have followed Setting up the Eclipse IDE for Yocto Application Development. but, I can't click OK button in "Yocto Project ADT" a...
    Yibeom Han
    last modified by Yibeom Han
  • mfgtool, No Device Connected.

    Hi.   I have an i.mx6qp sabred board and I want to download it using mfgtool. However, the PC does not recognize the device. SW6 dip switch is set to 00001100. When a USB OTB connector is connected to a PC, it i...
    An jin ho
    last modified by An jin ho
  • fail to mount ( rw option, type 1DX... )

    I purchased the i.MX6QP SABRE Board. Here is an SD card with Android porting. And I want to connect murata type 1dx wifi module to i.MX6qp saber. The murata guide document says to copy the Type 1DX firmware to the "/e...
    An jin ho
    last modified by An jin ho
  • i.MX6Qsabresd Board and  Murata 1MW WiFi/BT connection problem

    I connected the two boards to page 28 of themurata_quick_start_guide_linux.pdf manual.At the same time, I built the new mirror file as described in the following post in the community https://community.nxp.com/th...
    zh_y
    last modified by zh_y
  • fsl_sensor_fusion crashing in Android 7.1.2

    Hi, I'm using fxos8700 accelerometer/magnetometer and fxas2100x gyro with Android 7.1.2 (release android_N7.1.2_2.0.0 for iMX6QP). All sensors are detected in kernel. FreescaleAccelerometer, FreescaleGyroscope and, Fr...
    zbigniewbauer
    last modified by zbigniewbauer
  • imx6qp GUI hang | IPU issue

    Hello team,   setup: We are having a custom board based on imx6qp with 4G DDR. On software side we are using yocto with kernel 4.14.78 and xfce desktop environment. The board is booting successfully and we can ...
    Arun Kumar
    last modified by Arun Kumar
  • IMX6QP SARBEAUTO with TP2854 MIPI CSI2 work fail?

    Hi everyone! I am having a iMX6qp sarbeauto board and tp2854 mipi-csi2 board I just followed this document from Qiang Li and add modified patch files for imx6qp on Linux BSP 4.14.98  iMX6DQ TP2854 MIPI CSI2 72...
    Ho Tan Ha
    last modified by Ho Tan Ha
  • Printing characters on to the LCD display

    Hi,   We're using i.MX6QP processor to communicate with the external LCD display through LVDS-Bridge interface. But LVDS Bridge seems to be more like a buffer, which simply transmits Differential-ended sign...
    Srikanth Vemula
    last modified by Srikanth Vemula
  • How to include memtool in the core-image-base ?

    Hello guys,   We are trying to include the memtool utilities from imx-test packages, but I can't figure out how to do it. Hereunder is the content of my local.conf file :   MACHINE ??= 'imx6ulevk' DISTRO...
    matt67
    last modified by matt67
  • i.MX Android常见问题解答

    [中文翻译版] 见附件   原文链接: i.MX Android Frequently Asked Questions 
    Leo Lin
    last modified by Leo Lin
  • 如何理解i.MX6Q ESAI模块的“多个重置功能”

    [中文翻译版] 见附件   原文链接: How to Understand "Several Reset Functions" Of i.MX6Q ESAI Module 
    Leo Lin
    last modified by Leo Lin
  • How to configure vpu enc when recording video on imx8qm

    Hardware platform: imx8qm software platform: imx-p9.0.0_2.1.1-auto-ga-android   I wrote an application for recording 4-way videos, the application using Camera 1.0 Api. When the recording application is st...
    yingjin yan
    last modified by yingjin yan
  • I assume all builds takes 2 ~ 3 days, I think it is too long.

    I think it takes too long to complete each of do_compile, it sometimes reached to almost one hour each of do_compile. I am using imx-yocto-LF_L5.4.3_1.0.0 with distro is xwayland and graphics backends is qt5, and eva...
    Yibeom Han
    last modified by Yibeom Han
  • about how to flash android images to sd card?

    first:our board usb typec device is not work well ,so i want,Is there anyways to flash android images to sd card without board?
    zhou wei
    last modified by zhou wei