• How to setup QSPI LUT to work as DTR (Double Transfer Rate) ?

    Any reference code would be appreciated.
    Ronen Avihav
    last modified by Ronen Avihav
  • runqemu imx8mmevk not working

    i build the yocto image for hardware imx8mmevk by following steps 1)Downloaded meta-freescale-thud bsp and added at poky_thud directory and mentioned layed in bblayer.conf 2)changed machine at local.conf to imx8mmev...
    Omkar Teli
    last modified by Omkar Teli
  • Handling Heap/Stack - Sample application RT1050

    Dear friends,   In developing of a project with i.MXRT1052, I are having difficulty testing the handling of Heap / Stack regions so that the program runs on external RAM (64Mb) rather than internal RAM (96kb). P...
    Rubens Junior
    last modified by Rubens Junior
  • QSPI Flash RT1050 failure

    Dear,   I'm working on a project with the NXP i.MXRT1050 family MIMXRT1052DVL6B processor. For preliminary testing I'm using the MIMXRT1050-EVK development kit. For the initial tests we are using the SDX provide...
    Rubens Junior
    last modified by Rubens Junior
  • LOCSC Interface

    Dear collegues! Happy 2020!   Does anyone know of an interface called locsc for NXP processors?   Best regards. Rubens Júnior.
    Rubens Junior
    last modified by Rubens Junior
  • LOCSC Interface

    Dear collegues! Happy 2020!   Does anyone know of an interface called locsc for NXP processors?   Best regards. Rubens Júnior.
    Rubens Junior
    last modified by Rubens Junior
  • RT1050 x CMOS Image Sensor

    Dear collegues,   I would like an example of communication, for example I2C, of the RT1050 family processor with a CMOS image sensor, for example the BF3901CS (BYD Manufacturer) sensor. Can someone help me? ...
    Rubens Junior
    last modified by Rubens Junior
  • Fixed chip ID reporting in FXOS8700 driver

    Fixed bug in FXOS8700 driver where chip ID would always be reported as 0x0 in an error message when chip id read fails or returns unexpected value during FXOS87000 initialization.
    venkata shuressh
    last modified by venkata shuressh
  • SGTL5000 INTERFACING WITH SPI THROUGH MSP430F5529

    Hello Every one, Good morning to all   I am using a sgtl5000 in my console mixer project, I have interfacing through spi , Also I have set all the registers of sgtl5000 , but it doesn't respond any thing.  ...
    vikash chandra raman
    last modified by vikash chandra raman
  • a simple task fails for TCM_L and works well  for flash.

    hello Maybe it is an obvious question but i do not see correct answer. i use mx6sx mcu (a9 and m4 cores inside) and had created a FreeRTOS little test project for TCM_L memory of m4. The project has one little task -...
    oleg scherbinin
    last modified by oleg scherbinin
  • PCIe: Virtual channels

    Hey all,   I need to know which NXP MCUs/MPUs supports more then one Virtual Channel (VC) for PCIe.   I need to realize isochronous data transfers over PCIe.   Thanks in advance!
    Julian Dietrich
    last modified by Julian Dietrich
  • Opencv - based image acquisition, qt display

    Opencv - based image acquisition, qt display Everybody is good Imax6q board, qt creator of 5.9.5, kernel 4.1.15   I collect the camera of v4l2 with opencv and display it with the label of qt.Currently it can be ...
    袁 野
    created by 袁 野
  • U Boot how to make SPI Flash configuration

    Hi guys,   I'm working on i.MX6UL custom board. Trying to configure SPI Flash (Model = Winbond W25Q128JV), Here's the changes that I've made and the parts that I've added; ## arch/arm/dts/imx6ul-14x14-evk.dts; ...
    berkay ercan
    last modified by berkay ercan
  • HID detection issue

    I have been facing HID Detection issues. Few boards get detected. Whereas the detecting boards are found to have the same issue sometimes. There are no hardware changes that can be differentiated between detecting and...
    Annie Varshitha
    last modified by Annie Varshitha
  • How to switch EIM control pin to GPIO mode?

    Hello everyone!       Now I can use EIM and FPGA communication in normal use of imx6sx. the bsp is 4.14.98.CS pin and other control pins are used in EIM.       As the pins are relatively...
    long hao
    last modified by long hao
  • IMX6 CSI Register Settings on Linux

    Hi   How can i see the csi registers in linux command line? If i need to update any kernel or u-boot code is ok for me.   I just want to see    IPU_CSI_SENS_FRM_SIZE IPU_CSI_ACT_FRM_SIZE IOMUX...
    ümit kayacık
    last modified by ümit kayacık
  • How to get clock on CCM_CLKO1 for imx6q

    Hi,   I am working on imx6q board. I am trying to get clock on CCM_CLKO1 (D16 Pin) 24MHz or 12MHz.   while ov5640_mipi is loading i am getting clock for 1 sec later it is disabled. Some times it is showing...
    Vasu Sriram
    last modified by Vasu Sriram
  • IMX6 27MHz on CSI_MCLK

    Hi,   I am tring to take 27Mhz from IMX6 Sabresd board from GPIO_0_CLKO pin.     How can i do that? I guess 24Mhz is default set in DTS but i couldnt see any clock in this pin on ossiloscope? Do i n...
    ümit kayacık
    last modified by ümit kayacık
  • How to configure RDC?

    The board what i used is i.MX 8MQuad Assessment Suite, And the MCUXpresso SDK is version 2.6 Now i testting Contex m4 pwm demo with pwm4 which under driver_examples folder. It will be successful output waveform when ...
    yingjin yan
    last modified by yingjin yan
  • How to enable the drivers of camera module in imx-warp7

    Hi,       I have problem with enabling the drivers of the camera module. I have configured the menuconfig according to the attached document what they have explained and I have enabled the MX...
    vinod hulagabali
    last modified by vinod hulagabali