• LVDS format in the device tree

    hi i am connecting my imx8m-mini to a custom LVDS screen. i changed the device tree LVDS timing but still did not get a picture. at the end i change the lvds-format value from 1 to 2 and it fixed the LVDS output. I t...
    ran gree
    last modified by ran gree
  • OPENCV Error in I.MX8MMini

    I am getting the below error when i try to run a simple opencv code   terminate called after throwing a[24778.491458] audit: type=1701 audit(1579182772.146:15): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=42...
    Santhosh Kumar
    last modified by Santhosh Kumar
  • Create new /device/company/product-name/device-name

    Starting with the NXP Android 10 BSP for imx8mm, has anyone been able to add a new device?   Basically today in the NXP BSP for android 10 there is /android_build/device/fsl/imx8m/evk_8mm/ . I want to create a n...
    suly goonetilleke
    last modified by suly goonetilleke
  • Android 10 - i.MX8MMini - g2d rotation issue

    Hi,   I've found an issue with the G2D HWC layer on i.MX8M Mini, here is my setup: - Android 10.0.0-1.0.0 release - i.MX8M Mini EVK platform - MIPI display (1280x800 in my case) - SF_PRIMARY_DISPLAY_ORI...
    Gary Bisson
    last modified by Gary Bisson
  • /opt/imx-gpu-sdk directory

    Hi Venessa, i have build imx-gpu-sdk for imx8mqevk, and in the /opt/ i find imx8mqevk:/opt/imx-gpu-sdk# ls Console GLES2 GLES3 OpenCL OpenVG Window   Does all these apps run on GC7000 gpu (vivante driver) ?how...
    Manivannan s
    last modified by Manivannan s
  • i.max6 android Ethernet app add eth1

    您好,我正在使用i.max6 (android 6.0.1) 我的裝置上原本就有一個ethernet(eth0) 並且可以透過NXP內建Ethernet app控制eth0 例如使用stacic IP 和DHCP, 而我現在增加了一個裝置USB to Ethernet(eth1) 因此我想要讓eth1也可以透過Ethernet app來設置static ip 但是app裡並沒有eth1的選項 請問app要如何新增一個...
    minyou Hou
    last modified by minyou Hou
  • what's the reletion of pll and phy pll in imx8mm dsi

    HI  :         I found that , there is two descriptions about pll in imx8mm dsi:   what's the relation of them ? The "DPHY PLL" Fout max is 750M only, but PLL up to 2....
    jiang yaqiang
    last modified by jiang yaqiang
  • Starting Gstreamer for imx8mqevk

    If i have to start development of gstreamer based applications for imx8mqevk , what is the reference document or any sample application to refer, please share ?
    Manivannan s
    last modified by Manivannan s
  • HDMI Output in i.MX 8QuadMax

    Hello everyone,   I'm trying to get output via HDMI on a i.MX 8QuadMax but so far without any success. I've already followed the steps described here Getting an HDMI output on IMX8QMLPDDR4ARM2 for a similar prob...
    Cláudio Maia
    last modified by Cláudio Maia
  • i.MX8QXP gamma tuning - a gui test code

    SW: Linux 4.14.98_2.2.0 bsp release , gpu sdk 5.3.0 and patch in this doc HW: i.MX8QXP MEK board   Inspired by the GIMP adjust color curve tool,  I write similar gui test code for i.MX8QXP gamma curve tuning...
    PengFushi
    last modified by PengFushi
  • iWave i.MX8M Mini Board with NXP eIQ ML Software Enables Low Cost Facial Recognition System

    Have you recently been sceptical of usinga contact-based access system in your office or a public place? This trait is a major concern in most places for a valid reason. An access surface in a public place is used by ...
    iWave Systems
    last modified by iWave Systems
  • Chromium browser 72 i.MX6 HW acceleration

    Hi, I share here a patch for enabling i.MX6 hardware acceleration for chromium browser 72 release. Environment is yocto thud and patch is based on GitHub - Freescale/chromium-imx. In addition to modifications ...
    fr5
    last modified by fr5
  • iMX8M nano Processor Power Down

    Hi All,   I want to know more about the iMX8M nano processor, in this processor it has 4x A53-cortex(core0 , core1, core2, core3) and 1x M7-cortex would be there, my queries are as below 1) How to do the Power ...
    nandish sg
    last modified by nandish sg
  • WiFi Display Sink (Miracast) in imx8QM

    Hi Team, We have seen Wi-Fi Display Sink in i.MX6 Android release it says Miracast is successfully validated in imx6. We are using imx8qm with android automotive is Miracast supported?   Also We do have im...
    Abdul Redwan
    last modified by Abdul Redwan
  • How does the LCD keep the uboot logo displayed to the kernel?

    Hi all:     The chip I used is imx6sx, and the BSP version is 4.14.98,and the LCD drive mode is rgb565.Now I can display the logo in Uboot and kernel respectively, but during kernel startup, there will...
    long hao
    last modified by long hao
  • Do we need LVDS bridge (like TI SN65DSI83) for LVDS interface display (like Mitsubishi aa123af01) for i.mx8qx?

    Dear Sir/Madam,   Hello,   We are developing an IVI/Cluster common hardware platform for commerical cars with i.mqxp based on the   MXQXP- MEK board. We consider to connect an LVDS interface...
    Mehmet Ipin
    last modified by Mehmet Ipin
  • IMX8QM cross connection of the clock signals of i2c_lvds 0/1

    Hi, expert,       I am looking at the imx8qm DTS file in linux-imx kernel git branch imx_4.14.98_2.0.0_ga.  The IMX8qm SoC has two I2C buses for each ldb brdige.   But in the file: ...
    minskey guo
    last modified by minskey guo
  • how to change size in title bar?

    Hi All,   I'm using imx-4.14.98-2.0.0_ga in xwayland backend, my display is a 7" WVGA LCD, currently I found the buttons on application's title bar are too small to click, does anybody know how to change the siz...
    Sun1z
    last modified by Sun1z
  • How does IMX8QXP drive a problem with dual channel LVDS?

    hi,       On the software 4.9.88 software, I have configured the ldb node, and the corresponding configuration is as follows:           ...
    Jinlong Bai
    last modified by Jinlong Bai
  • Can we configure 4 lane MIPI as 2 lane MIPI and it will work with i.MX6 solo?

          we are using imx6 solo as per our requirement we need to interface 4 lane MIPI display and as imx6 only supports only 2 lane MIPI display. Can we configure 4 lane MIPI as 2 lane MIPI and it will ...
    abhay patil
    last modified by abhay patil