Skip navigationLog in to follow, share, and participate in this community. I failed to build fsl-yocto-L4.1.15_2.0.0-ga, build-x11/conf/local.conf PACKAGE_CLASSES ?= "package_ipk" please help me. thank you ! system : WARNING: Host distribution "Ubuntu-16.04" has no... failed to build fsl-yocto-L4.1.15_2.0.0-ga
BackHello, Does i.MX8 VPU encode support V4L2_Y12 format input source to make avi or mp4? use unit_test/V4L2_VPU/ or GSTL VPU used demo Thanks Hi, I am working with imx6ull-evk with a bluetooth board . I use bluez and HSP profile . When I connect a smartphone(TEL0) over bluetooth, tha board imx6 is the audio interface of the smarphone. When I do a call from... Bluetooth audio local-echo
BackHi, We designed a custom board based on IMX6UL. Everything works well except the ENET (phy chip: KSZ8081RNB). We got a very high error / frame rates (around 30-50%)in "ifconfig". Error number ... ENET1 frame errors/rx_crc errors
BackI'm using a customized board based on the iMX6ULL 14x14 evk board. My board uses 2x SMSC 8710A phys. NXP Linux Kernel 4.1.15 ENET1: link up is shown, didn't get a IP address ENET2: link up is shown, got IP ad... i.MX6ULL using both ethernet ports, but ENET1 won't work
BackHi, I'm using the 4.14.98 GA BSP where I need to use native chip-select (i.e. dedicated SPI chip-select pin instead of GPIO chip-select) for one of our device. I have gone through the "spi-fsl-lpspi.c" file where t... Native chip-select support on spi-fsl-lpspi.c
BackHello, i want to use the EIM-Interface for comunication between an IMX6Q and an FPGA for data transmission. I am using it in 16bit multiplexed A/D synchronous mode, using CLK, CS1, LBA, OE, RW, 0..15 of Data and want... EIM random clock-level in idle-state
BackHello , NXP community. I'm trying to confirm OTA update by recovery process for iMX8mm with Android 9 OS. however the recovery process is not complete because of the error after reboot for recov... OTA recovery process failure for iMX8mm
BackHello, BSP:IMX8 MINI EVK Linux imx8mmevk 4.14.78-imx_4.14.78_1.0.0_ga+g21fc82c I am using IMX8 Mini EVK (yocto)and I try to play music using Bluetooth A2DP. So far, I am able to pair and connect to my pho... Failed to play Bluetooth audio
BackWe are using an imx6-based board running Linux with Wayland. I need use the Vivante GPU's imxeglvivsink to display video inside a GTK+3 window with GStreamer. The problem is that the video with the imxeglvivsink plugi... imxeglvivsink inside a GTK window in Wayland
BackHello! I'm currently using yocto to build the system imx6sxsabresd (IMX6 Solo X). I have successfully built the image however I want to add some a script to init.d to turn on a led. I'm appending to the linux-... Bitbake not installing files from recipe to rootfs
BackHi Yuri I need "L3.0.35_4.1.0_130816_source.tar.gz" I can't find "L3.0.35_4.1.0_130816_source.tar.gz" file Could you send me "L3.0.35_4.1.0_130816_source.tar.gz" ?? Re: : i.MX6 LTIB installation, can't find download link
BackHi, I am using i.MX8QXP custom board with 4.9.88_beta 2 SDK to develop. We connect 2 spi slave devices to the LPSPI3 port, but I found the SPI3_CS1 can not config to GPIO. ... (i.MX8) How SPI driver control the LPSPI3 CS1 pin if it can not config to GPIO ?
BackHello I met a problem on NXP imx6 yocot system, that is the photo display is distorted. The phenomenon is as follows photo files. please helps to analyze what causes it and how to solve it Version: Linux 4.14.... Imx6 yocto photo display distortion
BackHi all, I have a question about resolution for EPDC. I found two different description of resolution for EPDC. Datasheet P7: 2048x1536 resolution at 106 Hz Reference Manual P1035: 1650 x 23... EPDC resolution in i.MX6UL
BackDear NXP, I am working in Android porting on imx8 processor for download the android source code I am following the "Android_User_Guide,pdf". 3.1 Getting i.MX Android release source code The i.... Android Source Code Download for IMX processor
Backhello, i use mcimx8-8x-bb ,linux kernel is started,USB connection is normal with USB flash drive,and can read data。 but connect to the computer, the computer(win10) does not have any prompt. usb cable is fine,becau... Hello, The description of USBNC_n_CTRL2 register in i.MX8MM Reference Manual V2 (chapter 11.1.42, page 2822) mentions DIG_ID_SEL field and IOMUXC_USB_OTG*_ID_SELECT_INPUT registers, however these registers are... i.MX8MM USB OTG ID Documentation
BackHello everyone, I have a custom board with imx6qp and ar8035, and i want to get into ar8035's 1000M Ethernet test mode.I had already set the reference clock to 125MHz, but it can't ping the gatewayip in u-boot... How to get into AR8035's 100M/1000M Ethernet Test mode for Compliance Test
BackThe IMX8MM reference manual section on the G2D specifies support for BT.601 and BT.709 YUV to RGB color conversions, including the formulas used. How are these set as they are not exposed in the G2D API? ... How to set IMX8MM colour space for G2D conversions
Back