• work with 3840x412 LCD

    Hi all!   I want to work with i.MX6 Quad with linux and LCD display with 412 vertical by 3840 horizontal pixel resolution. Does i.MX6 support it? Thanks!   Artur.
    Artur Null
    last modified by Artur Null
  • MFGTool Error when flashing a MX6SX 14x14 board with eMMC

    Hello all,   I'm trying to boot a board based on SABRESD design. The board had passed the memory test, but  mfgtools won't flash it.   Last error I can see in the log is 'Failed to Initialize memory!'...
    Victor Palacio
    last modified by Victor Palacio
  • imxvideoconvert_ipu Gstreamer plugin

    Dear all, I am using Variscite's DART-MX8M-MINI platform, running Yocto Sumo (i.e. sumo-fsl-4.14.98-mx8mm-v2.2) I would like to test some features that combines a prosperity algorithm with gstreamer elements. ...
    Nissim Beja
    last modified by Nissim Beja
  • How to use usb 2.0 and Type-c connectors at the same time on i.mx8mini

    Hello I used a USB hub on i.mx8mini to make 4 usb ports. By the way, if I use Type-c and usb 2.0 together, I don't know how to configure   i.mx8mini has two USB ports One used for FW download The other one will...
    Danny KIM
    last modified by Danny KIM
  • Boot Hang issue in iMx8DX6

    Hi Sir, iMx8DX6 board stops at boot level and after we switch off and on the board it starts working I have attached the working and non working  logs for your reference   When the boot hangs it stop...
    sheraz ali shah
    last modified by sheraz ali shah
  • imx28 - very high CPU usage, system running slow

    we are running the linux-fslc kernel 4.9 on imx28 alongside a filesystem built with Yocto (Morty). It seems that any amount of work is 'too much' for the cpu. for example, under idle conditions, top shows 'us' loading...
    msardar@accu-time.com
    last modified by msardar@accu-time.com
  • /dev/ttyACM* missing after reboot

    Hi I was working without any problem with a MODEM connected via /dev/ttyACM* to my IMX6ULL in aour custom board.   I executed a reboot on the processor without switch off (both MODEM and IMX6ULL)   the /d...
    fabio mario poiatti
    last modified by fabio mario poiatti
  • Display pixel clock limitation to 74.25 MHz

    Hi,   I'm using a board with the IMX8 SoC and 4.14.98 IMX kernel.   I'm trying to add support for a MIPI-DSI display (800x480@60Hz) that needs a pixel clock of ~25MHz.   The problem is that there is ...
    Sebastian Panceac
    last modified by Sebastian Panceac
  • I.MX8M would automatically crashes under do not do anything

    Hello experts ,   I found my I.MX8M board would automatically crashes under do not do anything, ( can't output log or key any command )     it might happen between 1~2 hour,   but after &#...
    Dylan Lin
    last modified by Dylan Lin
  • Linux BSP can suspend only one time.

    Hello community,   I'm trying to suspend/resume function with i.MX6Q SABRE-AI + base board. Using Linux BSP is a L4.19.35-1.1.0   In first time, it is success to suspend by following command and success t...
    Takayuki Ishii
    last modified by Takayuki Ishii
  • How to verify if the signed iMX6 image works?

    Is there any such tool to verify before burn the eFuse and load the signed image to the device? ##iMX6 HAB#
    Jiang Zhang
    last modified by Jiang Zhang
  • How to apply patch in poky layer (outside receipe)

    Dear All,   Right now, I'm trying to apply the patch from the below link to my Yocto base manually. [warrior-next,54/54] cve-check: backport rewrite from master - Patchwork  It's working fine.   I w...
    Raana
    last modified by Raana
  • i.MXRT1064 EVK PCB file

    Dear NXP Deam,   Kindly help me on this customer support.   We want to study the i.MXRT1064 EVK PCB file which is in Allegro tool. We want to open it in Altium, for that ASCII file generated from Allegro...
    BALASUBRAMANIAN M.S.
    last modified by BALASUBRAMANIAN M.S.
  • i.MX8M HDMI KEEP_ALIVE remain zero

    On customer board with i.MX8M Quad Lite revision 2.1, HDMI can't output. After trace code, found HDMI software keep alive counter keep remain zero.   API_General.c\hdp\imx\video\drivers - uboot-imx - i.MX U-Boo...
    m.c
    last modified by m.c
  • 2 LVDS screens on imx6 - How to get one fbdev device per screen?

    Hello, I've found many questions that looked similar but still could not find an answer for my problem. I'm trying to set up 2 screens on imx6q. I want to be able to display different applications on each screen. &#...
    Fabien Pollet
    last modified by Fabien Pollet
  • About IMX8QM Decode With Gstreamer

    Hi I want to test the VPU decode on  the IMX8QM board with Gstreamer plugin. I use these two gst command the video can display right  gst-launch-1.0 v4l2src device=/dev/video3  io-mode=dmabuf num-buf...
    Xu Liu
    last modified by Xu Liu
  • MIMXRT1010 Boot

    I have recently bought the MIMXRT1010-EVK and have been playing around with it. I managed to get the SDK Samples loaded and debugger working. However, I now have the board in a state where it will no longer jump ...
  • KSZ9131RNX Porting to i.MX8

    Hi   we are using microchip KSZ9131RNX as our ethernet phy,according to i.MX reference user manual the fec driver will auto-probes the external adaptor (PHY device).but we can not probe KSZ9131 Is there a...
    Neil Chang
    last modified by Neil Chang
  • i.MX8M Mini PCIe Ethernet hang

    HW: i.MX8M Mini LPDDR4 EVK SW: Linux 4.14.98 eth0: on board eth1: PCIe RTL8119 PC1 iperf client PC2 iperf server PC1 <-> eth0 <-> eth1 <-> PC2 ifconfig eth0 192.168.127.254 ifconfig eth1 192.1...
    m.c
    last modified by m.c
  • imx8qxp can't recoginse USB_OTG2

    Hi,     imx8qxp can't recoginse USB device.kernel startup log as following:     [ 0.561921] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator [ 0.67738...
    liu yonggang
    last modified by liu yonggang