Skip navigationLog in to follow, share, and participate in this community. Hi , Which firmware I need to put on PN7462AU for FCC test? Is there any sample firmware available in SDK ? Please help me in this Thanks Aswin I have an OM5577 demoboard and tried to install the demo software for a Raspberry Pi 3, OM5577 Raspberry Pi Linux demo image. I allways get a rainbow screen when the Pi is booting. With an other application the Pi is ... OM5577 - Raspberry Pi3 Rainbow Screen
BackHello, I need to read UIDs of all Type V tags in front of the reader. I have extended the NfcrdlibEx5_ISO15693 example and changed PHAC_DISCLOOP_CONFIG_TYPEV_DEVICE_LIMIT and PHAC_DISCLOOP_CFG_MAX_VICINITY_CARDS_SUPPO... Stay quiet example for ICODE SLIX2?
BackHi, I'm tring to modify the fw of our UHF reader to read the Brand identifier of tag UCODE8/8m. Could you please tell me how to set the parameter of select command? According to the standard th... UCODE 8/8m TAG - brand identifier
BackHello, I'm trying to check the NTAG413 originality signature. Unfortunately the document “an260412 - AN11350 NTAG Originality Signature Validation (1.2)” concerns only the 32-byte signatu... How to check NXP signature on NTAG413
BackI'm working on a card reader using the SAM AV2 chip that will read cards using key diversification. I understand the diversification algorithm, but there are steps to "encrypt x using AES". I assume AES is... Hi, We would like to make use of the additional general purpose outputs of the CRLC663 chip in a future project to save pins on a MCU. We would like to use the Pins OUT0 to OUT3 which are usually for the... CRLC663: general purpose output functionality
BackMy task is to design a antenna to read a mifare tag. I try to describe the application: Imagine a credit card shaped tag, but way smaller (25mm long, 11mm high, 3mm thick). This tag travels trough a tu... Very special antenna design
BackDear Sir: I am trying to add support for PN548 to Rockchip PX30 platform, which runs on Android 8.1. I use NFC_NCIHALx_AR00C0.8.4.0_OpnSrc to integrate to our platform. I have followed steps of Doc AN11690, ... NFC PN548 porting on Android Oreo 8.1
BackWhen testing with PN7150, with tag moving in and out of field... A NCI_RF_INTF_ACTIVATED_NTF message was received with invalid data: 61 05 15 01 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF F... NCI_RF_INTF_ACTIVATED_NTF corrupted
Backhi i have developed the card reader device using mfrc630plus, Our device can read and write mifare classic card. but desfire, jcob card doesn't response about request ALL. I not sure that this issue is about ... MFRC630 no response ATQA to request ALL
BackDuring operation I sometimes get a reset notification after sending a start discovery command. The reset shows reason code is A3. Before the reset an I2C request to start discovery had been sent. ... Workaround for intermittent PN7150 reset after sending start discovery request?
BackDuring testing with PN7150, I started getting error status response to the start stop commands. 41 03 01 06 and 41 06 01 06 What is the meaning of the 06 error code? Where can I find d... Error status 6 in response to start/stop discover cmd
BackHello , I am working on PNEV7462C development board. I am using MCUXpresso IDE and i have run all the example codes on the board which worked perfectly. But after i tried to flash the code in to EEPROM using... Good morning, I want to know, basically, if I can read Android HCE cards with the NXP 663 chip. Currently, we are using this chip for reading MiFare Ultralight and Classic cards in our business, but now we wan... CRLC633 and Android HCE cards
BackHi, We are using a Deskfire EV.2 in a tag. The tag is connected to an i-phone XS. When inductive charging the i-phone the Deskfire chip is damaged. How can we avoid this? Deskfire EV.2 destroyed while inductive charging an i-phone.
BackDear All: 我使用PN7120做读卡器,卡放在读卡器上,从发送读卡指令到读到数据大概要1s多的时间,请问这是否正常? 使用官方示例程序“NXP-NCI_LPC82X_example”用开发板测试,等待时间也差不多,请问是否可以通过设置参数调整该时间? 谢谢! Now ,I encounter a question . when I put the 3100 from indoor temperature 25 into fridge temperature -17,and set the measurement interval 1 second ,the 3100 temperature value decline to fridge t... NHS3100 Temperature sensor not sensitive ?
BackI have been working with NFC tags for a while, and have been using the TagWriter app by NXP on Android to encode single NFC tags with a URL. This has worked great when tag quantities are small, but it is not easy... Are there different encoding requirements for iOS vs Android?
Backhi everybody! I’m having problems with MRFC522, does anyone have some code using spi and Lpc1769? I will be greatful!