• Explore-NFC compatibility with ISO-14443 Type 4B tags

    Hello guys,   I have downloaded the NFC Reader Library from http://www.nxp.com/pages/:NFC-READER-LIBRARY. I downloaded the previous Version "NFC Reader Library for Linux" version 4.040.05.011646". Because the la...
    Manoj Rohit Vemparala
    last modified by Manoj Rohit Vemparala
  • DESFIRE EV1 ans SAM AV2 authentication

    Hello, I try to authenticate a DESFire EV1 card with a SAM AV2 with command SAM_AuthenticatePICC, but that do not run correctly. First of all, I want to say the card authentication run correctly when I read the sessi...
    Christophe Lallement
    last modified by Christophe Lallement
  • Developing app with Xamarin for access control with NFC tags

    Hi, I'm developing an app for Android, Windows Phone and IOs with the purpose of control the access of users to certain locations: First the location nfc tag is read and after that the users nfc tags are read. The a...
    Roberto Menes
    last modified by Roberto Menes
  • MCUXpresso crash after debug launch

    Hi, I installed MCUXpresso on my PC following the instructions in the UM10883 PN7462AU Quick Start Guide. I also installed the plugin for PN7462AU and sample software projects. When debugging any of the projects (whic...
  • PN532使用设计注意哪些问题

    PN532作为NFC控制器在使用时,需要注意哪些问题?片子在使用时要不要烧录什么程序,还是直接用MCU驱动。天线设计敷铜线比其他天线有什么不同?
    meng wang
    last modified by meng wang
  • Advice

    One of my friends who work in the jewellery and watch industry wants to develop some bracelets with NFC functions for mobile payment and/or lighting control. Now, he wants to know the suitable NFC chipset to be select...
    sam khaukha
    last modified by sam khaukha
  • NFC PN544 bring up on Android M

    Hello, I was trying to bring up NFC PN544 on Android M. But no success. Followed the document "AN11690 NXPNCI Android Porting Guidelines". Getting the following error in the logcat log. Please help.     01-...
    Venkatesh Gowda
    last modified by Venkatesh Gowda
  • PN5180 BGA signal definitions

    Hello all,   Has anyone used PN5180 in BGA package? I have got the pinouts for the package (under NDA) but there seems to be couple of signals which do not have proper definitions.    Signal #1: PRD ...
    Ismail Bari
    last modified by Ismail Bari
  • PN5180天线寄存器设置

         大家好:         最近在调试PN5180的天线,需要设置天线的载波信号幅值、Q值、调制深度等参数,需要设置哪些寄存器,有什么需要注意的地方?
    hao peng
    last modified by hao peng
  • Best NFC Inlay for Access Badge Manufacturing?

    Hi there!   I own an event credentials company that provides assess badges, wristbands, etc. to event organizers. We would like to start offering access badges with NFC RFID inlays to our customers for event acc...
    Josh Campbell
    last modified by Josh Campbell
  • NHS3100 endurance

    Dear Support After reading the NHS3100 documentation, I understood that the device stores data in the eeprom and then moves it to Flash. Assuming a logger application where all measurement are to be stored, and a sa...
    Martins Marco
    last modified by Martins Marco
  • 关于调试PN532低功耗问题

    根据手册PN532/C1 8.5.4介绍对PN532进行配置,始终达不到40微安的低功耗电流。 配置完成D1H寄存器、 SVDD寄存器、RF寄存器、PCON寄存器后,电流是5.5毫安左右。还需要配置哪些寄存器,才可以实现45微安的低功耗?
    F P
    last modified by F P
  • TDA8026 Issue

    Hi, One of my customer doing IOT POS handheld on AM3354 platform. In the design they used our TDA8026 smart card IC. The basic communication level I2C bus is Ok and able to probe the tda8026 driver that mean the I2C...
  • PN71xx internal AGC behavior and Rrx adjustment advices

    The PN71xx NFC controller includes internal AGC function attenuating the Rx signal coming from the antenna to reach optimum receiver input voltage (preventing against signal saturation).      ...
    Jeremy Geslin
    created by Jeremy Geslin
  • SL3S4011FHK: UCODE I²C - Parasitic capacitance

    Hello!   We are working on this project at university with UHF RFID Tags, and we are facing some problem at achieving the same results with simulation and real experimentation. We are using NXP SL3S4011FHK: UCOD...
    Samuel Morais
    last modified by Samuel Morais
  • Embrace E20智能卡平台

        平台的资料哪里可以下载到?
    hao peng
    last modified by hao peng
  • PN7462 Program Flash Tool Error

    Hello, i have a problem when i use he "Program Flash Tool" present in LPCXpresso with my PN7462. If i  perform a "Mass erase", after i can't connect the debugger to the target, the error was   15: Target ...
    Matteo Zoppi
    last modified by Matteo Zoppi
  • Interfacing PN7150 module with Mediatek MT6572 in Android Platform

    Hi,    i am interfacing the PN7150 module with Mediatek MT6572 processor in Android platform(Jelly Bean - 4.2.2 ). I downloaded the Android patches for support of NCI based NXP NFC Controllers in Android(K...
    Vinothraj M
    last modified by Vinothraj M
  • NTAG-nt3h2211-class6 antenna cannot read/write use Samsung mobile phone

    Hi, my hardware: NTAG+class6 antenna(demo antenna download for nxp web) In my project,i use Ntag Pass-through mode.I installed "NTAG I2C DEMO"APP,when i try to operate my NTAG,the app prompt:"Communication failed Th...
    jie xu
    last modified by jie xu
  • Cake8026_02_D schematic and PCB file

    hello,   Do you have Cake8026_02_D's schematic and PCB source file?  I just found UM10319 in pdf version.It will be useful for customer's design if we have Altium design file or candence file. Thanks.
    Wenxue Wang
    created by Wenxue Wang