• TagXplorer does not work with NTAG I2C Plus

    I tried to use the TagXplorer (v1.2) Application on Windows 7 with a NXP Pegoda CLRD710 Reader and a NTAG I2C Plus (NT3H2111W0FTTJ). Unfortunately there seems to be a bug in the software, the NTAG I2C Plus tag is reco...
    Stefan Jardot
    last modified by Stefan Jardot
  • Academic Assistance Request Regarding Conductive Ink Application on RFID

    Hi Everyone, My name is Davina Chang, and I'm currently an MBA student from HEC Paris.  For my term project (which could turn into a full business upon graduation) I'm working on an entrepreneurship project in...
    Davina Chang
    last modified by Davina Chang
  • how to automatic RF field on PN5180 EVB

    hello,    i have a pn5180 evb now,then it can be triggered by click RF fielded on button in NXP NFC Cockpit,but i want to turn on RF field automatic without NXP NFC Cockpit when pow...
    sadad sadad
    last modified by sadad sadad
  • how to p2p read mode?

    hello. l use ncf3340 chip. I success p2p write mode for android. but, i want p2p read mode from android. I know I can get a message when I am in p2p target mode, and I can send a message when I am in p2p2 initiat...
    semikim kim
    last modified by semikim kim
  • FCC Test for PN7150

    Hi, i am working with PN7150 in our project for NFC. as part of project requirement i am doing FCC testing. for PN7150, i am trying to set Active mode and Standby mode. What should the wave pattern look like an ideal...
    Shaik Sameem
    last modified by Shaik Sameem
  • How to check the firmware version of preprogrammed PN7120 IC

    We are using PN7120 NFC controller for our project. The proof of concept was carried out using OM5577/PN7120ARD evaluation kit from NXP. Recently we made our own custom PCB and started the testing. We have the re...
    ANJU H V
    last modified by ANJU H V
  • SRAM Mirror update via NFC

    I'm wanting to write a few bytes to the SRAM via NFC on the NTAG I2C plus NT3H2211 device, and was wondering if this can this be done in SRAM mirror mode or is this only possible in pass through mode?   Thanks &...
    David Adams
    last modified by David Adams
  • Missing software for PN7150 via USB

    Hi,   I purchased the following product:   NFC USB Dongle - NFC Reader-Writer based on NXP’s PN7150 | MikroElektronika    It includes the PN7150.   On their product page they link to...
    Nick Daskalou
    last modified by Nick Daskalou
  • PN7150 - Example code issues

    Hi,   I am evaluating an PN7150 dongle for possible future use. I compiled the code in Visual Studio, and ran into these issues:   1) When starting the application the first time, it seems t...
    Oyvind Idland
    last modified by Oyvind Idland
  • NFC Library Porting Help

    I'm starting to look at porting the CLRC663 NFC library to an STM32F103 and am hoping I can get some direction/guidance here. I've downloaded the library and as far as I can tell I need to reproduce the functionality ...
    danielbujak
    last modified by danielbujak
  • P2P exchange + Powerdown timing problem

    Hello, I bougth two PN532. I implement P2P communication with DEP protocol in active mode. After communication, both PN532 receives the command "POWERDOWN 0x88 0x01"  (=Wake up on RF field & I2C and Generate ...
    Romane Schelkens
    last modified by Romane Schelkens
  • NFC Reader Library on Github

    It would be nice to see NFC Reader Library on Github so we (users) can post bug reports, bugfixes and even pull requests with additional functionality.
    troky
    last modified by troky
  • ESD robustness of ICODE SLIX

    Hi Team, We are using ICODE SLIX right now. Could you let me know which bonding method is strong for ESD, 2 pads bonding or 4 pads bonding? If you could recommend the 2pad bonding, please let me know...
    Naoki Okazaki
    last modified by Naoki Okazaki
  • NFC embedded applications for automotive?

    As the increasing popularity of NFC in the consumer market, demand for NFC applications in automotive has raised; we are offering a How to Develop Automotive Near Field Communication (NFC) Applications for Embedded Sy...
    Toño Hernández
    created by Toño Hernández
  • How to porting NQ210 &NQ220 to Android 8.0?

    How to porting NQ210 &NQ220 to Android 8.0? How to prove the success of the transplant?
    Zhang Xiangyong
    last modified by Zhang Xiangyong
  • NFC MIRROR FAILED

    hello Now I want to develop a project to use nt3h2111 NFC chip, system general' working process is like this, there is a card reader, and a controller in the system, card reader and the controller transmission ...
    Sun Xin
    last modified by Sun Xin
  • GetVcList description unclear

    If a mifare implementation supports vc entries range 0-0x15 and if no virtual cards are created yet and i send GetVcList command with vc entry range 0 to 0x15, filter criteria MSB 0x7F and LSB 00, what should be the r...
    Eshwar Chandra Pavaganda
    last modified by Eshwar Chandra Pavaganda
  • Security system using MFRC522 and Micro controller (NXP or Atmel)

    Hi, I am working on a security system and I am planning to use RFID chip MFRC522 and the micro-controller that will manage the communication with the RFID will be pic18F452, is this a right combination from the point ...
    Moustafa Eldysouky
    last modified by Moustafa Eldysouky
  • NFC Tags Memory Explanation

    Where can I find a document(s) that explain what I'm reading from a specifc tag (NFC Forum Type 2 Tag)?  Meaning, is there a document that explains how the memory is formatted with all the bytes I'm reading ...
    michaelsteffenfae
    last modified by michaelsteffenfae
  • NHS3100 data storage and external reader

    Dear Support How can I confirm/change the Total storage capacity of the NHS3100 (demo.tlogger firmware) Also, I can we access the Logging data without using the andoird app? Thanks
    Martins Marco
    last modified by Martins Marco