SRAM Mirror update via NFC I'm wanting to write a few bytes to the SRAM via NFC on the NTAG I2C plus NT3H2211 device, and was wondering if this can this be done in SRAM mirror mode or is this only possible in pass through mode? Thanks &... Missing software for PN7150 via USB Hi, I purchased the following product: NFC USB Dongle - NFC Reader-Writer based on NXP’s PN7150 | MikroElektronika It includes the PN7150. On their product page they link to... PN7150 - Example code issues Hi, I am evaluating an PN7150 dongle for possible future use. I compiled the code in Visual Studio, and ran into these issues: 1) When starting the application the first time, it seems t... NFC Library Porting Help I'm starting to look at porting the CLRC663 NFC library to an STM32F103 and am hoping I can get some direction/guidance here. I've downloaded the library and as far as I can tell I need to reproduce the functionality ... P2P exchange + Powerdown timing problem Hello, I bougth two PN532. I implement P2P communication with DEP protocol in active mode. After communication, both PN532 receives the command "POWERDOWN 0x88 0x01" (=Wake up on RF field & I2C and Generate ... NFC Reader Library on Github It would be nice to see NFC Reader Library on Github so we (users) can post bug reports, bugfixes and even pull requests with additional functionality. ESD robustness of ICODE SLIX Hi Team, We are using ICODE SLIX right now. Could you let me know which bonding method is strong for ESD, 2 pads bonding or 4 pads bonding? If you could recommend the 2pad bonding, please let me know... NFC embedded applications for automotive? As the increasing popularity of NFC in the consumer market, demand for NFC applications in automotive has raised; we are offering a How to Develop Automotive Near Field Communication (NFC) Applications for Embedded Sy... How to porting NQ210 &NQ220 to Android 8.0? How to porting NQ210 &NQ220 to Android 8.0? How to prove the success of the transplant? CLEV6630B External MCU Connection Questions I have a question. I wonder if you can debug the sample project by connecting an external MCU (eg STM32F4 series) to the CLEV6630B without using the MCU in CLEV6630B. Because there is no LPC-Link2, I want to debug us... NFC MIRROR FAILED hello Now I want to develop a project to use nt3h2111 NFC chip, system general' working process is like this, there is a card reader, and a controller in the system, card reader and the controller transmission ... GetVcList description unclear If a mifare implementation supports vc entries range 0-0x15 and if no virtual cards are created yet and i send GetVcList command with vc entry range 0 to 0x15, filter criteria MSB 0x7F and LSB 00, what should be the r... Security system using MFRC522 and Micro controller (NXP or Atmel) Hi, I am working on a security system and I am planning to use RFID chip MFRC522 and the micro-controller that will manage the communication with the RFID will be pic18F452, is this a right combination from the point ... NFC Tags Memory Explanation Where can I find a document(s) that explain what I'm reading from a specifc tag (NFC Forum Type 2 Tag)? Meaning, is there a document that explains how the memory is formatted with all the bytes I'm reading ... NHS3100 data storage and external reader Dear Support How can I confirm/change the Total storage capacity of the NHS3100 (demo.tlogger firmware) Also, I can we access the Logging data without using the andoird app? Thanks Android App to connect to SSDP Connected Device After a day and a half of trial and error, I am still unable to build the sample application. I am also not able to build a blank application from scratch as outlined in the instructions. Specifically, I am follo... NDA for MIFARE DESFire EV1 card info I understand the required information for decrypting/accessing information on MIFARE DESFire cards is under NDA and I would need to sign one in order to gain access to the require documents. Would anyone know wh... Is there any mandatory certifications for NFC tags? I want to use NFC function as parameter setting, which replace DIP switch. Is it used as NFC tags for electronic applicaion? is there any mandatory certifications for NFC tags? Does CE/FCC certification con... NTAG23xF FD pin is not changing level when RF-field is present. Hello, It's my first time working with NFC technology and I'm trying to use the FD-pin on a NTAG213F to send data to a microcontroller. At least use the signal transition to wake up the microcontroller from a sleep st... NFC Controled RGB LED using LPC812 This project demonstrate the controlling of RGB led over NFC by smartphone. LPC812 MAX board is interfaced with NTAG I2C board (NT3H1101). The pin connections are here, P0_11 -> SCL_NTAG P...