• Error in USB initialization PN7462.

    Hello. I found an error in init of USB of pn7462. I am working with library ver5.12, but it also exist in last version (5.22). In function VCom_Init(void) (cdc_main.c) there are such strings:     ...
    Dmitriy Nechaev
    last modified by Dmitriy Nechaev
  • phNfcLib_Initialization.c Bug

    Hi, I found the following bug: the gphNfcLib_Key variable are defined with a size of 6, but in the phNfcLib_Init when call the: PH_CHECK_NFCLIB_INIT_FCT(wStatus, phKeyStore_SetKey(&gphNfcLib_Params.sKeyStore...
    Carlos Alberto Fernandez
    last modified by Carlos Alberto Fernandez
  • How to make NPC300 controller be one of wake-up sources of Windows 10 platform ?

    Scenario :  Step 1. Make sure windows 10 platform goes into modern standby mode or screen off mode. Step 2. Tap an NFC card on device to wake up it.
    Wilson Chien
    last modified by Wilson Chien
  • SL3S4021FHK: UCODE I²C enabling SCL interrupt

    Hello, I have question about UFH tags SL3S4021FHK: UCODE I²C. We had implemented this kind of chips on our boards considering usage of possibility of generating interrupts on SCL line. Actually we are able to pr...
    Krzysztof Plec
    last modified by Krzysztof Plec
  • CLRC663 MIFARE DESFIRE example not found

    I am also missing and searching for Desfire example 10, can support send me a link, please. We have signed NDA. Thanks!   Edit: We need the version for CLRC663, we are developing firmware for MCU.
    karthik k
    last modified by karthik k
  • Tech question for SL3S1013FTB0,115

    Dear NXP team,   Thank you for supporting us. This is Takashi from Digi-key.   I have customer question below;   Costumer is using SL3S1013FTB0,115 of NXP Semiconductors. In his experiments, the se...
    Takashi Matsumura
    last modified by Takashi Matsumura
  • Comments related to the PN7150 NFC library

    Hi,   I just managed to adapt the source code example for PN7150 for the EVK-RT1064 board and for the Arduino PN7150 board (source code: evkmimxrt1060_PN7150).   I used the latest versions of MCUxpresso ID...
    Neculai Agavriloaei
    last modified by Neculai Agavriloaei
  • i.MX RT1064 and PN7150 NCI Library

    Hello,   I have adapted the NXPNCI-PN7150 software example to work with the iMX RT1064 microcontroller. For this purpose I used the MIMXRT1064-EVK development board and the Arduino PN7150 board (OM5578 / PN7150S...
  • NFC Tandem concept: combine NFC reader and connected tag solution

    See NFC Tandem concept: combine NFC reader and connected tag solution.   
    Jeremy Geslin
    created by Jeremy Geslin
  • PN7150 NFC Controller on i.MX8M mini evk running Yocto

    See PN7150 NFC Controller on i.MX8M mini evk running Yocto.
    Jeremy Geslin
    created by Jeremy Geslin
  • Easy set-up of NFC on Raspberry Pi

    See Easy set-up of NFC on Raspberry Pi.
    Jeremy Geslin
    created by Jeremy Geslin
  • PN7150 NFC Controller on i.MX8M mini evk running Android Pie

    See PN7150 NFC Controller on i.MX8M mini evk running Android Pie .
    Jeremy Geslin
    created by Jeremy Geslin
  • NXP TagWriter App support of SLIX2

    Hi,   Recently updated the Android version of (the great) NXP Tagwriter app- Version 4.8.1 Seems that I've lost support for the SLIX2 IC, will still work perfectly with other NTAG 213 ICs Same tags will read p...
    Stephen Cocking
    last modified by Stephen Cocking
  • TagXplorer does not work with NTAG I2C Plus

    I tried to use the TagXplorer (v1.2) Application on Windows 7 with a NXP Pegoda CLRD710 Reader and a NTAG I2C Plus (NT3H2111W0FTTJ). Unfortunately there seems to be a bug in the software, the NTAG I2C Plus tag is reco...
    Stefan Jardot
    last modified by Stefan Jardot
  • Academic Assistance Request Regarding Conductive Ink Application on RFID

    Hi Everyone, My name is Davina Chang, and I'm currently an MBA student from HEC Paris.  For my term project (which could turn into a full business upon graduation) I'm working on an entrepreneurship project in...
    Davina Chang
    last modified by Davina Chang
  • how to automatic RF field on PN5180 EVB

    hello,    i have a pn5180 evb now,then it can be triggered by click RF fielded on button in NXP NFC Cockpit,but i want to turn on RF field automatic without NXP NFC Cockpit when pow...
    sadad sadad
    last modified by sadad sadad
  • how to p2p read mode?

    hello. l use ncf3340 chip. I success p2p write mode for android. but, i want p2p read mode from android. I know I can get a message when I am in p2p target mode, and I can send a message when I am in p2p2 initiat...
    semikim kim
    last modified by semikim kim
  • FCC Test for PN7150

    Hi, i am working with PN7150 in our project for NFC. as part of project requirement i am doing FCC testing. for PN7150, i am trying to set Active mode and Standby mode. What should the wave pattern look like an ideal...
    Shaik Sameem
    last modified by Shaik Sameem
  • How to check the firmware version of preprogrammed PN7120 IC

    We are using PN7120 NFC controller for our project. The proof of concept was carried out using OM5577/PN7120ARD evaluation kit from NXP. Recently we made our own custom PCB and started the testing. We have the re...
    ANJU H V
    last modified by ANJU H V
  • SRAM Mirror update via NFC

    I'm wanting to write a few bytes to the SRAM via NFC on the NTAG I2C plus NT3H2211 device, and was wondering if this can this be done in SRAM mirror mode or is this only possible in pass through mode?   Thanks &...
    David Adams
    last modified by David Adams