• Using PN7462 to interact with Mifare Ultralight c

    Hello NFC community,  as you may know the The PN7462 family consists of 32-bit Arm® Cortex®-M0-based NFC microcontrollers offering high performance and low power consumption. It has a simple instru...
    Jonathan Iglesias
    last modified by Garabo
  • NFC reader library porting guide for LPC11u37h(Ver 5.12) - Switching the NFC frontend

    As NFC reader library 5.12 also supports PN5180, switching the NFC frontend from CLRC663 to PN5180 is quite easy based on previous porting. The porting also includes the hardware settings and software modification. &#...
    Kan_Li
    last modified by Kan_Li
  • Multiple NDEF records visualized in TagXplorer

    Hello NFC Community!   This document demonstrates that multiple records can be also read from a Tag with TagXplorer. Please follow the steps below.   Let's begin...   Please make sure that ...
    IvanRuiz
    last modified by IvanRuiz
  • Writing multiple NDEF text records with TagWriter app

    Hello NFC Community,   This document describes how to write multiple NDEF Text Record by making use of NFC TagWriter app by NXP.     First of all, download the TagWriter app from the Play Store: NFC ...
    IvanRuiz
    last modified by IvanRuiz
  • Interfacing PN7150 or PN7120 to Kinetis Freedom Boards with KSDK v1.3

    Hello NFC community:   NXP released the new PN7150 NFC Controller chip with enhanced power output, and there is also the new Arduino compatible demokit OM5578/PN7150ARD. See more information in the next pages: &...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • Installation of Linux CCID driver For NFC Reader

    Recently, some NFC customer want to use CCID driver to communcate with NFC reader on Linux platform, but they encontered some errors during installing CCID driver for linux. I tested it and installed it to ubuntu 16.0...
    Wigros Sun
    last modified by Wigros Sun
  • NFC reader library porting guide for LPC11u37h(Ver 5.12) - Porting other demos

    Based on NFC reader library porting guide for LPC11u37h(Ver 5.12) ,We have a partial ported NFC reader library like below: Now, it is time to port other demos in this project. You may choose any demo, but here Nfcr...
    Kan_Li
    last modified by Kan_Li
  • NFC reader library porting guide for LPC11u37h(Ver 5.12) - Porting NfcrdlibEx1_BasicDiscoveryLoop

    The latest NFC reader library supports lpc1769 which is a cortex M3 controller with LPCopen lib supports, so in theory , it should supports other controllers supported by LPCopen, but we have to test this, so we choos...
    Kan_Li
    last modified by Kan_Li
  • Prepare CLEV663B board for NFC reader library porting

    The latest NFC reader library for CLRC663 just supports LPCXpresso1769 and FRDM-K82 boards, so when customers want to porting the library to other host controller, they have to make a custom board at first, or use OM2...
    Kan_Li
    last modified by Kan_Li
  • Activating multiple Tags using NFC Reader Library

    Hello NFC enthusiasts,   In the NFC communication protocol, when a device acts as a NFC reader (it provides its own field), it is waiting for a tag to approach. When this occurs, the reader energizes the tag and...
    IvanRuiz
    last modified by ebiz_ws_prod
  • Porting Guide for NXP-NCI example

    The NXP-NCI example is based on NXP-NCI lib and LPCopen lib, and due to the good consistency, the porting is mainly focus on LPCopen lib switching.   Software setup download lpcopen package via http://www.nxp.c...
    Kan_Li
    last modified by ebiz_ws_prod
  • NXPNCI-KDS_Example with KSDK v2.1

    The NXPNCI-KDS_Example for the PN7120/PN7150 Arduino interface boards available in NXP webpage at the time of publishing this document includes a project compatible with KSDK v2.0 for FRDM-K64F platform. With the late...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • NTAG I2C Plus interface to Kinetis Freedom boards

    Hello NFC and Kinetis enthusiasts,   NTAG I2C plus tag ICs offer both, a contact (I2C) and a contactless interface (NFC) to ease the development of IoT, home-automation and consumer applications.    ...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • A trick to run NXP-NCI_LPC11xx_example with OM5577

    The latest NXP-NCI example is rev 1.6, and when you run this demo with the lpc11xx board, for example, lpc1115 rev A, and the OM5577, you may meet the following issue: The problem is due to two aspects: one is hard...
    Kan_Li
    last modified by ebiz_ws_prod
  • Copying NDEF text messages from one Tag to another

    Hello NFC enthusiasts,   The following topics will be covered in this document: Activation of multiple Tags. For more information, please refer to Activating multiple Tags using NFC Reader Library  R...
    IvanRuiz
    last modified by IvanRuiz
  • Program the firmware to PNEV5180B board

    When the PNEV5180B cannot work with the Cockpit, you can re-program the firmware to the board. Below are the steps show you how to program the firmware to the board again.   1. If you don't have the MCUXpresso, ...
    jimmychan
    last modified by jimmychan
  • NFC PN7120 on the  i.MX6Q

    INTRODUCTION REQUIREMENTS KERNEL DRIVER DEVICE NODE NFC LIBRARY TESTING NFC READER REFERENCES       1. INTRODUCTION   This document is a step by step guide of the AN11697 PN7120 Linux Sof...
    Jorge_Gonzalez
    created by Jorge_Gonzalez
  • PN7150/PN7120 NFC Controller SBC Kit for Arduino on the i.MX6SX

    This is a step by step guide on setting up and running a simple NFC Demo App using the PN7150 NFC Controller SBC Kit for Arduino (OM5578/PN7150ARD) with a UDOO NEO board which uses an i.MX6SX and it's Arduino pin comp...
    gusarambula
    last modified by gusarambula