• NFC Reader Library Porting FRDM_K64F

    The NFC Reader Library is a complete software support library for NFC Frontend ICs. Designed to give developers a faster and simpler way to deliver NFC-enabled products. This multi-layer library, written in C, makes i...
    Ricardo Zamora
    last modified by Ricardo Zamora
  • How to sell NFC

    You are a salesperson or FAE and are looking for ways to sell more Near-Field-Communication (NFC) products? This community provides ideas, information, and materials that help you to successfully sell more N...
    Louisa Dybowski
    last modified by Anup Shukla
  • Overview of supported NFC/MCU Combinations

    This page contains information about the supported NXP MCU/MPU and NXP NFC product combinations which have ready to use packages. These can be used as a reference. The table below contains link to where you can find t...
    Ali Khan
    last modified by Richard Schmidmaier
  • Guide for using NTAG 5 with LPC55S69

    This post contains step by step guide of how to use NTAG 5 with LPC55S69. The goal of this post is to enable developers to use NTAG 5 and LPC55S69 together, quickly and easily.    Attached with this post a...
    Yadhnyaseni Kayande
    last modified by Yadhnyaseni Kayande
  • Bluetooth Pairing example porting from KW41Z to KW36

    Hello NFC community,   The purpose of this document is to show the steps to port the Bluetooth pairing example for NTAG I²C Plus from KW41Z to KW36.    Setup   For this, we will work w...
    IvanRuiz
    last modified by IvanRuiz
  • MIFARE DESFire Light read and write demonstration

    This demonstration is based on RFIDDiscover full version and Pegoda EV710. You may refer to the following links for more details. RFIDDiscover | NXP  PEGODA Contactless Smart Card Reader | NXP    Bef...
    Kan_Li
    last modified by Kan_Li
  • Using NFC Reader Library with LPC55S69

    This post contains a guide of how to use the NFC Reader Library with LPC55S69. A ready to use package for using the “Basic Discovery Loop” example from the NFC Reader Library with LPC55S69 and CLRC663 plu...
    Ali Khan
    last modified by Ali Khan
  • Using NFC Reader Library with LPC845 (With Reduced Size)

    This post contains a guide of how to use the NFC Reader Library with LPC845 using the Basic Discovery Loop example. The vanilla Basic Discovery Loop example is larger than the flash size of LPC845 (64KB), so the proje...
    Ali Khan
    last modified by Ali Khan
  • Getting data from NFC, LPC8N04 MCU

    Hello NFC Community,   This document focuses to the configuration of the LPC8N04 to be controlled by the data it receives though the NFC interface.       The document is based on the nfc_eeprom ...
    IvanRuiz
    last modified by IvanRuiz
  • Using LPC55S69 with SE050 and CLRC663plus for Secure Access to industrial IOT

    DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS:   This post contains a guide of how to use LPC55S69 demoboard with other NXP demoboards to demonstrate Access control using NFC, one embedded secure element and a...
    Rodolfo Veltri Gomes
    last modified by Rodolfo Veltri Gomes
  • Using i.MXRT1050 with SE050 and CLRC663plus for Secure Access to industrial IOT

    DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS: This post contains a guide of how to use i.MXRT1050 demoboard with other NXP demoboards to demonstrate Secure access to industrial IOT, using NFC, embedded secure elem...
    Rodolfo Veltri Gomes
    last modified by Rodolfo Veltri Gomes
  • NFC Reader Library Porting to i.MX RT1050

    This document provides a step by step guide of how to use the CLRC663 plus with i.MX RT1050. For this purpose, we need to port the NFC Reader Library to i.MX RT1050.  There are two zip files attached to this doc...
    vicentegomez
    last modified by Ali Khan
  • NFC Antenna Design

    Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful.   Training Fi...
    jimmychan
    last modified by jimmychan
  • Using NTAG I²C plus kit with LPC55S69

    This post contains step by step guide of how to use the NTAG I²C plus with LPC55S69. This is easy and straightforward to do, since the MCUXpresso SDK Builder tool has an option to add NTAG I²C plus example d...
    Ali Khan
    last modified by Ali Khan
  • Using PN7150 with LPC55S69

    This post contains a step by step guide of how to use PN7150 with LPC55S69.  This document is structured as follows:   Overview of PN7150:  Overview of LPC55S69:  Hardware requirements:...
    Ali Khan
    last modified by Ali Khan
  • Guide for using PN7150 with i.MX RT1060

    This post contains a step by step guide of how to use PN7150 with i.MX RT1060. This document is structured as follows:   Overview of PN7150 Hardware Requirements Using PN7150 with i.MX RT1060 Hardwa...
    Ali Khan
    last modified by Ali Khan
  • Guide For Creating PN7462 SPIM demo based on NFC reader library

    SPIM module is one of the master interfaces provided by PN7462 , which is a 32-bit ARM Cortex-M0-based NFC microcontroller, and users may use this interface to connect with up to two SPI slave devices. The NFC read...
    Kan_Li
    last modified by Kan_Li
  • How to Use Linux CCID driver for PN7462 DEMO Board

    Environments & Devices --Hardware 1、PN7462 DEMO Board(PNEV7642B) --Software 1、Ubuntu 16.04 desktop 2、Test tools ---libusb ---pcsc-lite ---ccid driver ---opensc        &...
    Wigros Sun
    last modified by Wigros Sun
  • Guide for using NTAG I²C plus with i.MX RT Boards

    This post contains step by step guide of how to use NTAG I²C plus with i.MX RT MCUs. The goal of this post is to enable developers to start developing their NFC Applications using NTAG I²C plus and i.MX RT M...
    Ali Khan
    last modified by Ali Khan
  • Mifare Ultralight C - Changing default password and protecting page address

      Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect co...
    Jonathan Iglesias
    last modified by Jonathan Iglesias