• Using LPC55S69 with SE050 and CLRC663plus for Secure Access to industrial IOT

    DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS:   This post contains a guide of how to use LPC55S69 demoboard with other NXP demoboards to demonstrate Access control using NFC, one embedded secure element and a...
    Rodolfo Veltri Gomes
    last modified by Rodolfo Veltri Gomes
  • Using i.MXRT1050 with SE050 and CLRC663plus for Secure Access to industrial IOT

    DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS: This post contains a guide of how to use i.MXRT1050 demoboard with other NXP demoboards to demonstrate Secure access to industrial IOT, using NFC, embedded secure elem...
    Rodolfo Veltri Gomes
    last modified by Rodolfo Veltri Gomes
  • Overview of supported NFC/MCU Combinations

    This page contains information about the supported NXP MCU/MPU and NXP NFC product combinations which have ready to use packages.These can be used as a reference . The table below contains link to where you can find t...
    Ali Khan
    last modified by Ali Khan
  • NFC Reader Library Porting to i.MX RT1050

    This document provides a step by step guide of how to use the CLRC663 plus with i.MX RT1050. For this purpose, we need to port the NFC Reader Library to i.MX RT1050.  There are two zip files attached to this doc...
    vicentegomez
    last modified by Ali Khan
  • How to sell NFC

    You are a sales person or FAE and are looking for ways to sell more Near-Field-Communication (NFC) products? This community provides ideas, information and materials that help you to successfully sell more N...
    Louisa Dybowski
    last modified by Anup Shukla
  • NFC Antenna Design

    Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful.   Training Fi...
    jimmychan
    last modified by jimmychan
  • Using NTAG I²C plus kit with LPC55S69

    This post contains step by step guide of how to use the NTAG I²C plus with LPC55S69. This is easy and straightforward to do, since the MCUXpresso SDK Builder tool has an option to add NTAG I²C plus example d...
    Ali Khan
    last modified by Ali Khan
  • Using PN7150 with LPC55S69

    This post contains a step by step guide of how to use PN7150 with LPC55S69.  This document is structured as follows:   Overview of PN7150:  Overview of LPC55S69:  Hardware requirements:...
    Ali Khan
    last modified by Ali Khan
  • Using NFC Reader Library with LPC55S69

    This post contains a guide of how to use the NFC Reader Library with LPC55S69. A ready to use package for using the “Basic Discovery Loop” example from the NFC Reader Library with LPC55S69 and CLRC663 plu...
    Ali Khan
    last modified by Ali Khan
  • Guide for using PN7150 with i.MX RT1060

    This post contains a step by step guide of how to use PN7150 with i.MX RT1060. This document is structured as follows:   Overview of PN7150 Hardware Requirements Using PN7150 with i.MX RT1060 Hardwa...
    Ali Khan
    last modified by Ali Khan
  • Guide For Creating PN7462 SPIM demo based on NFC reader library

    SPIM module is one of the master interfaces provided by PN7462 , which is a 32-bit ARM Cortex-M0-based NFC microcontroller, and users may use this interface to connect with up to two SPI slave devices. The NFC read...
    Kan_Li
    last modified by Kan_Li
  • How to Use Linux CCID driver for PN7462 DEMO Board

    Environments & Devices --Hardware 1、PN7462 DEMO Board(PNEV7642B) --Software 1、Ubuntu 16.04 desktop 2、Test tools ---libusb ---pcsc-lite ---ccid driver ---opensc        &...
    Wigros Sun
    last modified by Wigros Sun
  • Guide for using NTAG I²C plus with i.MX RT Boards

    This post contains step by step guide of how to use NTAG I²C plus with i.MX RT MCUs. The goal of this post is to enable developers to start developing their NFC Applications using NTAG I²C plus and i.MX RT M...
    Ali Khan
    last modified by Ali Khan
  • Mifare Ultralight C - Changing default password and protecting page address

      Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect co...
    Jonathan Iglesias
    last modified by Jonathan Iglesias
  • Using PN7462 to interact with Mifare Ultralight c

    Hello NFC community,  as you may know the The PN7462 family consists of 32-bit Arm® Cortex®-M0-based NFC microcontrollers offering high performance and low power consumption. It has a simple instru...
    Jonathan Iglesias
    last modified by Garabo
  • NFC reader library porting guide for LPC11u37h(Ver 5.12) - Switching the NFC frontend

    As NFC reader library 5.12 also supports PN5180, switching the NFC frontend from CLRC663 to PN5180 is quite easy based on previous porting. The porting also includes the hardware settings and software modification. &#...
    Kan_Li
    last modified by Kan_Li
  • Multiple NDEF records visualized in TagXplorer

    Hello NFC Community!   This document demonstrates that multiple records can be also read from a Tag with TagXplorer. Please follow the steps below.   Let's begin...   Please make sure that ...
    IvanRuiz
    last modified by IvanRuiz
  • Writing multiple NDEF text records with TagWriter app

    Hello NFC Community,   This document describes how to write multiple NDEF Text Record by making use of NFC TagWriter app by NXP.     First of all, download the TagWriter app from the Play Store: NFC ...
    IvanRuiz
    last modified by IvanRuiz
  • Interfacing PN7150 or PN7120 to Kinetis Freedom Boards with KSDK v1.3

    Hello NFC community:   NXP released the new PN7150 NFC Controller chip with enhanced power output, and there is also the new Arduino compatible demokit OM5578/PN7150ARD. See more information in the next pages: &...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • Installation of Linux CCID driver For NFC Reader

    Recently, some NFC customer want to use CCID driver to communcate with NFC reader on Linux platform, but they encontered some errors during installing CCID driver for linux. I tested it and installed it to ubuntu 16.0...
    Wigros Sun
    last modified by Wigros Sun