• USB FLASH download, programming, and security tool (DFUSec)

    The LPC18xx/43xx DFUSec utility referred to in this article should NOT be used. It has been replaced by LPCScrypt. Use of LCT will result in a very old firmware version, which will contain bugs and not support so...
    jorge_plascencia
    last modified by Brendon Slade
  • LPC11U6x USB to I2C Bridge Implementation

        The LPC11U6x USB to I2C Bridge project utilizes NXP’s USB Serial I/O (LPCUSBSIO) library to demonstrate the I2C sensor control via the full speed USB functionality on LPC11U6x. The project is ...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC-Link 2 Configuration Tool

    The LPC-Link 2 Configuration Tool (LCT) has been replaced by LPCScrypt and should no longer be used. This content is provided for informational purposes only.   The LPC-Link 2 Configuration Tool (LCT) is a Windo...
    Diana Torres
    last modified by Brendon Slade
  • WinUSB driver installation (LPC18xx/LPC43xx)

    This procedure no longer applies to DFUSec/LCT. As of v2.00 of the LCT, you no longer need to manually install .NET or the WinUSB driver package - the LCT installer will do that for you if it already isn't installed. ...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • IOH Libraries

    IntroductionThis page gives a quick overview of the available IOH libraries. A description of the library, its specifications and its requirements are summarized on this page. The the following downloads are attached ...
    jorge_plascencia
    last modified by Juan Padilla
  • LPC USB Serial I/O Library

    IntroductionThe LPC USB serial I/O (LPCUSBSIO) is a generic API provided to PC applications programmer to develop applications to communicate with serial I/O devices connected to LPC micro-controller. LPCUSBIO library...
    jorge_plascencia
    last modified by Juan Padilla
  • Smartphone Quick-Jack solution

    NXP Smartphone Quick-Jack SolutionTransform the audio jack of a smartphone into a multi-purpose, self-powered data port. This hardware/software platform, designed for use with iPhone® and Android® smartphone...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • NXP MCORE48/64/100 Evaluation Board + Demo Code

    IntroductionThe MicroCore48/64/100 has been developed to evaluate, test and demonstrate general purpose Microcontrollers from NXP Semiconductors.  The Microcore48/64/100 demo, evaluation and test board supports N...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LCD controller design examples using the LPC247x

    The LPC247x microcontrollers have integrated LCD controllers. These microcontrollers support Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) graphic display panels up to 1024 x 768 pixels, from monochrome u...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC Motor Control Library (nxpMClib)

    The NXP motor control library (nxpMClib) supports various types of motor control for the Cortex-M family. Built on CMSIS2.0 math and DSPLIB. Supported by motor control GUI with selection for each supported type. Inclu...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • Motor Control with NXP Microcontrollers

    IntroductionElectric motors drive motion in all kinds of applications, from washing machines and exercise treadmills to the HVAC (heating, ventilation, and air conditioning) systems in commercial buildings. The drawba...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • MLC extractor tool build

    Before you can use the MLC extractor tool (MET), you need to customize it for your hardware and rebuild it. You will need the CodeSourcery GNU toolchain (EABI version) to build the files. Download the CodeSourcery too...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • u-boot build procedure

    Before building u-boot, you'll need a machine that can run Linux (such as Fedora or Ubuntu). You can setup a Virtual Machine and install Linux on it if you don't have access to a physical Linux machine. 1. Start by do...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • USB host mass storage class (MSC) example

    NXP Semiconductors and OnChip Technologies have partnered to provide USBHostLite software for our LPC1000, LPC2000, and LPC3000 families of microcontrollers with USB host capability. These include members of the LPC17...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • DFUSec programming API

    A simple programming API is available that allows custom development of programming algorithms for different memory types such as NOR or NAND FLASH or EEPROM based memory. By mixing programming algorithms and differen...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC32xx Common Driver Library (CDL)

    IntroductionNXP Semiconductors provides a free Common Driver Library (CDL) software package for use with LPC32xx microcontrollers. This software package provides a generic set of drivers which highlight how specific p...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC43XX Dual Core Examples

    1.      Important Notes    1.    Please read the build section of Libraries and Example before building anything     2.    Never giv...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC4088 Closed Payment Loop Demo

    IntroductionThe LPC4088 based Closed Loop Payment demo shows how a basic closed loop payment system can be created using NXP’s ARM Cortex-M4 based LPC4088.  The leading industry-standard MIFARE contactless ...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • LPC32x0 S1L/kickstart build example

    IntroductionI get asked lots of questions on how to build and deploy the kickstart loader and S1L to a new LPC32x0 based board. This topic will go through the procedure step-by-step for the FDI3250 and the PHY3250 boa...
    jorge_plascencia
    last modified by ebiz_ws_prod
  • IOH: Getting started with the example projects

    IntroductionThe IOH application examples provide a great and easy way to get started with I/O Handler. All provided IOH examples come with project files for LPCXpresso, Keil MDK and IAR EWARM. This page will give an o...
    jorge_plascencia
    last modified by ebiz_ws_prod