• Simple example LPCOpen I2C

    Content originally posted in LPCWare by Rosfudum on Fri Apr 17 03:05:30 MST 2015 Hi all, I need to read/write an M24C16 Eeprom with LPC1115 using LPCOpen. I read I2c example but it's pretty complicated. It use Maste...
    lpcware
    last modified by lpcware
  • LPC 1820 - GPIO - DMA - SRAM speed

    Content originally posted in LPCWare by kellykan on Sat Mar 05 14:02:58 MST 2016 Hi Guys, I've been working on a project for a while where we implemented a GPIO DMA transfer to memory to capture 2 bit parallel data ...
    lpcware
    last modified by lpcware
  • DMA ADC sync

    Content originally posted in LPCWare by rouxfederico on Sat Jul 12 10:03:52 MST 2014 Hello, this is my first post here. I always find the answer to my programming problems but I haven't found for this. The problem is...
    lpcware
    last modified by lpcware
  • Getting start with LPCXpresso54608 & emWin Graphics;

    This tutorial explains some basic knowledge about drawing texts and images on  LPCXpresso54608 TFT screen using emWin library.   Tools Required: ->MCUXpresso IDE ->LPCXpresso54608 SDK 2.0.0 ->em...
    Ashok Ra
    last modified by Ashok Ra
  • SD CARD communication and TX UNDERRUN error

    Hi all,   with reference to the LPC1788 microcontroller, I have some problems with the SD CARD routines. I'm using  the lpc177x_8x_mci.c routines 2.0 version but I have frequently TX UND...
    Nico Aprile
    last modified by Nico Aprile
  • LPC43xx Chip_Clock_EnableCrystal Hard fault advisory

    I am posting this as I ran into this issue after starting some new development with the LPC4357.   The function void Chip_Clock_EnableCrystal(void) in the chip support library has a while loop delay to paus...
    Eli Hughes
    last modified by Eli Hughes
  • PLU inputs assignment (lpcxpresso55s69)

    Below is of the C code generated by the PLU configuration tool which is equivalent to an AND function.    This code configuration the chosen LUTs input/puts with the chosen PLU input/outpus. ...
    Randa Zarrouk
    last modified by Randa Zarrouk
  • LWIP phy problem

    MCU: LPC4333   Harware is custom.   I'm trying to get my DP83848 ethernet phy to work in RMII mode based on the lwip_tcpecho example.   The link status is good and the PHY_LINK_CONNECTED bit is ...
    Julian Winpenny
    last modified by Julian Winpenny
  • LPC54018JxM:XIP erase and program internal SPIFI Flash

          Attached demo is sample project to show how to erase and program LPC54018JxM’s internal flash(embedded 2MB/4MB W25Q Flash)  through SPIFI0 interface.       As ...
    S.z. Liang
    created by S.z. Liang
  • LPC55S69 with BT815

    Check out my LPC55S69 system with the HS SPI interfaced to an BT815 running at 50Mhz SPI clock. LPC55S69 With BT815 and ESP32-WROOM - YouTube 
    chris gulick
    last modified by chris gulick
  • Need urgent help - Isochronous IN transfer with LPC1837 USB-HOST

    Content originally posted in LPCWare by stefko on Thu May 28 12:01:17 MST 2015 Hi all ! I'm working on a test project where I need to connect a USB camera to LPC1837 demo board. The LPC1837 is configured to use USB...
    lpcware
    last modified by lpcware
  • LPC804 Github Project and Examples with Focus on PLU Setup

    Hi All   I have stared to document my own experience withthe LPC804 and its PLU on a github project: GitHub - olikraus/lpc804_plu: LPC804 toolchain with PLU compiler and Flash-ROM upload tool    Addi...
    Oliver Kraus
    last modified by Oliver Kraus
  • Error while integrating the PLU code? this could be a reason. (LPC55S69_cm33_core0.h))

    Programmable Logic Unit (PLU) offers an interesting functionality in the MCU world. It allows the possibility of creating small combinatorial and/or sequential logic networks including state machines.  ...
    Randa Zarrouk
    last modified by Randa Zarrouk
  • Mass Storage Device (MSD) with external SPI flash sst25vf064c ussing LPC1769

    Content originally posted in LPCWare by javos on Thu Oct 04 08:30:54 MST 2012 Hi everybody!!! I am working on a hand-held device, it will be a dataloger. My idea, is to download the data through USB. So my device wil...
    lpcware
    last modified by lpcware
  • LPC54608 Deep Sleep Mode exit

    Hello,  I am attempting to verify LPC54608 power management with OM13092 dev board. The case i am trying to verify is exiting Deep Sleep Mode using pin interrupt (SW5 on OM13092). I am able to exit Sleep Mode wi...
    Santosh balakrishnan
    last modified by Santosh balakrishnan
  • [LPCOpen][LPC17xx] I2C master freeze

    Content originally posted in LPCWare by pgr on Thu Apr 10 01:56:38 MST 2014 Dear all, I am using I2C0 as a master on a LPC1763 with LPCOpen stack. Sometimes randomly the I2C driver freeze inside Chip_I2C_EventHandler...
    lpcware
    last modified by lpcware
  • Issue in configuring the GPIOs in LPC1778

    Hi all,   I'm having difficulties in initializing the GPIO into the Input/ Output mode. I'm using LPC1778FBD144, wherein I'm trying to use some GPIOs for the specific task that required reading as well as w...
    sakib khan
    last modified by sakib khan
  • State FlipFlops for PLU (LPC55S69)

    Hello,  I have some questions regarding the FF deployment in the PLU module:   Point 1: "The outputs of up to four of the LUTs can be captured in one of the four state flip-flops" UM  Do this me...
    Randa Zarrouk
    last modified by Randa Zarrouk
  • LPC54628 HOST USB Issue

    I cannot seem to detect the insertion of a USB device (Phillips 16GB stick using an Insignia USB On-the-Go adapter).   I am trying to use the USB HOST example with fatfs and FreeRTOS on the OM13098 development b...
    Adrian Neal
    last modified by Adrian Neal
  • Getting Started with LPC55S69, LPC55S69-EVK, Cortex® M33 and TrustZone®

    I've been really, really impressed with the LPC55S69 and its enablement (LPC55S69-EVK, MCUXpresso IDE, MCUXpresso SDK and the Config tools). Now that I've used the part for some time, I thought that it would be helpfu...
    Mark Dunnett
    last modified by Mark Dunnett