• X-ray the Monkey!  Mini-Monkey Rev B Update

    I had some design updates for “Rev B” of my Mini-Monkey design that I wanted to get in the "queue" for testing.  For the next revision, I wanted to try PCB:NG for the board fabrication and assemb...
    Eli Hughes
    last modified by Eli Hughes
  • reading data from Grideye Sensor

    I have been working on this project to read the data from Grideye Sensor which is interfaced with LPC1768 via I2C. but I do not receive any data. when I debugged it probably don't even enter the start condition. can s...
    pooja singh
    last modified by pooja singh
  • QEI - INX CNT can not count, when A / B(SIGMODE =0) stop. 

    中文 : 功能說明 : 設計Z偵測到脈波輸入時,觸發中斷,清除AB向脈波計數值。   問題描述 : QEI - 當AB相沒有收到任何輸入脈波時,INCNT無法計數。 當AB相有偵測到輸入脈波時,INCNT才會計數。 這現象會導致,編碼器AB 輸入停止時,無法成功清除AB相計數值。 有其他方法可以讓Z 計數獨立計算,不受INGATE(index gating configuration) 影響嗎?   Engl...
    yansin lee
    last modified by yansin lee
  • I want to use an SSD1306 display with a LPC1549 mcu

    I know that there are different possibilities to use this kind of display with Arduino based boards but for a small project i would like to use the LPC1549 (which has all i need aboard) in combination with an small SS...
    Serge De Maseneer
    last modified by Serge De Maseneer
  • Driver for LCD ST7735, LPC1768/9

    Hi,   I have a LCD driver for a LPC1768 or (LPC1769) device. It works somehow. But, it is far from being efficient, it is slow. Even though I played with SPI speed from 1Mhz up to 25Mhz, it didn't make any diffe...
    senersoft@outlook.com
    last modified by senersoft@outlook.com
  • MCU Suggestion

    Hello,   I need an advice about MCU for my project. I have LPC54608J512BD208 on my board and 512K Flash is not okay for my project. Is there any MCU with the same or nearly similar to LPC546 pin design(I don't w...
    Fatih ozen
    last modified by Fatih ozen
  • Emwin runtime orientation

    Hi all,   I've got a successful implementation of the emwin libraries running on a LPC54608 hooked up to a ST7789 driven display (320x240, 18bits per pixel) working well displaying text and graphics and can...
    Ian Norman
    last modified by Ian Norman
  • OM13098 Demo sources ?

    Hello, I recently got my ordered eval board (OM13098/LPCXpresso54628), and have already tried some example projects. It came with a nice graphics demo, including touchscreen interaction. My main question -...
    frank meyer
    last modified by frank meyer
  • Mini-Monkey is Here!

    Open video

    Eli Hughes
    last modified by Eli Hughes
  • OKDO E1 Unboxing

    Open video

    Eli Hughes
    last modified by Eli Hughes
  • LPC55S69 Mini-Monkey Build Update – Off to Fabrication!

    The Mini-Monkey is now officially “out the door”.   I just sent the files to Macrofab and can’t wait to see the result.   Before I talk a bit about Macrofab, we will look at what ...
    Eli Hughes
    created by Eli Hughes
  • "Mini-Monkey" Part 1: How to design with the LPC55S69 in the VFBGA98 package

    Now that we have discussed the LPC5500 series at a high level and investigated some of the cool features,  it is time to roll up our sleeves work on some real hardware.    In this next series of ar...
    Eli Hughes
    last modified by Eli Hughes
  • LCD refresh rate

    Hello,   I'm using a 5" (800x480 px) display on a LPC54608 controller. We have 16MB onboard Video RAM. It's a "DE-Mode" display, so it ignores VSync and HSync. Data sheet: https://shop.lcd-module.de/media/attac...
    Lutz Herrmann
    last modified by Lutz Herrmann
  • Getting start with LPCXpresso54608 & emWin Graphics;

    This tutorial explains some basic knowledge about drawing texts and images on  LPCXpresso54608 TFT screen using emWin library.   Tools Required: ->MCUXpresso IDE ->LPCXpresso54608 SDK 2.0.0 ->em...
    Ashok Ra
    last modified by Ashok Ra
  • SCT -  PWM 200K Hz 100puse,not use interupt to STOP。

    SCT0產生一個200KHz AB pulse輸出波形,當user設定100次pulse(200KHz AB) 後,自動將SCT0關掉. (不用中斷去關掉SCT0,因為隨MCU的負載量變大,會導致來不及去關掉SCT0,導致額外多輸出101次的波形) SCT0有甚麼方法可去完成這個應用?不使用中斷。 -----------------------------------------------------------------...
    yansin lee
    last modified by yansin lee
  • SCT  applicaion - count PWM pluse number

    how to count PWM  pulse  by SCT ? for example . sent 200K 100pulse(duty 50~40%) to SCT。 SCT can count 100 pulse(can not use SCTinterupt)  please give me example.thanks.   -------...
    yansin lee
    last modified by yansin lee
  • LPC51U68 How to achieve PWM output and continuous low level switching?

    Hi Everyone:         I would like to ask how to achieve PWM output and continuous low level switching?         I saw that the LPC51U68 imple...
    云龙 赵
    last modified by 云龙 赵
  • emWin 5.38 Libraries for NXP Cortex M3 are not for Cortex M3!

    If you try to compile with these libraries, many error like the following will be reported:   Error: L6366E: GUIAA_Char2.o attributes are not compatible with the provided cpu and fpu attributes . Object GUI...
    Marco Aversa
    last modified by Marco Aversa
  • uart baud rate ?

    hai          in my Lpc824 have 3 uart protocol   . can i use the uart0 in 9600 baud rate and the uart1 as 115200 , if it is possible to use different baud rates in single code  ...
    Aravind palanisamy
    last modified by Aravind palanisamy
  • lpc824 external adc reading?

    hai             I need to read ADS1115 sensor values through the i2c protocol . i am, using lpc824 mcuxpresso i am, try last 2 week referred the ads1115 datasheet and lpc824 datashe...
    Aravind palanisamy
    last modified by Aravind palanisamy