• How to use S32K144 and MPC5744P Side-by-Side Controller

    in an S32K144 or MPC5744P Development Kits. Do you want to know how? Follow this topic for the next weeks and you'll find out more details.  - it is a big event -it has to do with Model-Based Design - it is ...
    jack ryan
    last modified by jack ryan
  • Motor Control Reference Solution Packages for ACIM, Release V1.2.0

    Dear all,   Let me inform you that Motor Control Reference Solution Packages for ACIM, Release V1.2.0  is fully available on NXP web page including full set of documentation (DRM, AN and UG).   Supp...
    Pavel Sustek
    last modified by Pavel Sustek
  • Freemaster error symbol definition missing

    I am working with HVP MC3PH, I got motor controller examples for hvpkv46f150m for MCUXpresso  Project Example: hvpkv46f150m_mc_pmsm   But while opening the freemaster project pmsm_float  it is ...
    Harshawardhan Kumbhar
    last modified by Harshawardhan Kumbhar
  • New release of BLDC Motor Control SW Package V1.2.0

    Dear all, Let me inform you that Motor Control Reference Solution Package for BLDC, Release V1.2.0 is available on NXP web pages including full set of documentation (DRM, AN and UG). More information, all relate...
    Pavel Sustek
    last modified by Pavel Sustek
  • MC3PHACVP

    Hi, I have a few questions about the MC3PHACVP. 1) Can I use it to build a variable frequency drive? 3) With this controller programming is not necessary. Right?  4) Do I need a programmer or anything else to us...
    Pedro Gobbo
    last modified by Pedro Gobbo
  • CAPACITORS ON BOARD CONTROL ENGINE

    Ever board to control BLDC or PMSM motor, have three capacitors in paralel. I did not understand their work, I noticed they always capacitance of 220uF and are polarized..... I will change the capacitors because I wo...
    Andre Luiz de Oliveira
    last modified by Andre Luiz de Oliveira
  • Simulink Library "svm_std_flt" output saturation to square wave

    Hi all,    I'm trying to simulate the FOC of PMSM with simulink. Could anyone please explain why the "SVM_STD_FLT" saturates to [0 ; 1] output values (instead of the standard output waveform shown in t...
    Abdelmouneim Charkaoui
    last modified by Abdelmouneim Charkaoui
  • Motion Control & Power - Become Approved Engineer Consultant

    We are a small team, a motion control and power experts, located in Israel and provide services to Israel, Europe and Far east Please visit our web-site www.gal-rnd.com We provide entire motion control &am...
    Gal Lior
    last modified by Gal Lior
  • 设计一个DCDC输入24V输出0-20V,0-100A的电源,使用KV3

    请问: 目前计划设计一个数字闭环的DCDC,只用作降压。 1,输入6-24V 2、输出0-20V,0-100A,因为只用作降压,所以输出电压只能低于输入电压 3,电压和电流输出精度要求0.3%FS 4,瞬态响应不做要求 请问这样的性能要求使用MKV30F64VLH10这个芯片可以吗。或者能不能推荐一个合适的芯片,只要ARM核心的。 有没有一个可以参考的设计或者资料。 谢谢!
    li longjie
    last modified by li longjie
  • FreeRTOS based PMSM Sensorless Control application available

    Dear all,   Let me inform you that new application note AN5309 Sensorless PMSM Field-Oriented Control on Kinetis KV31 with FreeRTOS & eGUI is fully available on NXP web pages including application software ...
    Pavel Sustek
    last modified by Pavel Sustek
  • Safety Class B with PMSM Sensorless Drive & RTCESL 4.3 available on nxp.com

    Dear all,   Let me inform about latest MC software product update: New application note AN5321 Safety Class B with PMSM Sensorless Drive is fully available on NXP web pages including application software AN5321...
    Pavel Sustek
    last modified by Pavel Sustek
  • Kea  drive stepper motor  by  mc34932 with the  software  MVHBridge

    Dear Expert, Now There is a project which  use the KEA64  drive a stepper motor by mc34932 with the  software  MVHBridge. I want to set the peak current of the driver from   0.2A  to...
    kiger Zhang
    last modified by kiger Zhang