• Automotive Math and Motor Control Library MPC577xC uses SPE 2.0

    Hi,   I downloaded the free Automotive Math and Motor Control Library Set NXP MPC577xC rev 1.1.4. When looking at either Diab or GHS archive MPC577xC_AMMCLIB.a, I realized that the archive was compiled with SPE ...
    Etienne Alepins
    last modified by Etienne Alepins
  • Kinetis Motor Suite cannot communicate because .elf file does not match. It refuses to accept the user directory where the .elf file resides. The whole installation is simply default options.

    The only .elf files are in a User subdirectory. This doesn't seem to be an acceptable directory. I am using FRDM-VV31F with NXP Freedom Development Platform for Low-Voltage, 3-Phase PMSM Motor Control. KDS can comm...
    Doug Wong
    last modified by Doug Wong
  • how to debug the motor control example by KDS with MKV31F128VLH10?

    hello, I'm new to KDS, and I want to control an induction motor by V/F method. I use MKV31F128VLH10 and I downloaded the motor example which is available in NXP.com But it does not work and I don not know how to modi...
    armaghan bahari
    last modified by armaghan bahari
  • Freemaster V2.0 communication lost after opening project

    Need Help please !   I am Working with KDS Version: 3.2.0 with a TWR_KV11Z75M Development Kit. I use the predefined Project pmsm_ref_sol build release code and let it run using seggerlink V512g for communication...
    Bernhard David
    last modified by Bernhard David
  • In the "TWR-KV58F220M_Quick Start Package" there is a example in the "Precompiled Examples" called "pmsm_demos_twr-kv58f.bin" where is there the example KDS project for this binary?

    The "pmsm_demos_twr-kv58f.bin" is a nice demo but would like to see the KDS project for this example. Did find the "Example source code for Kinetis 3 Phase BLDC Motor Control using TWR-MC-LV3PH", is this the project u...
    Dale Dalke
    last modified by Dale Dalke
  • FreeRTOS based PMSM Sensorless Control application available

    Dear all,   Let me inform you that new application note AN5309 Sensorless PMSM Field-Oriented Control on Kinetis KV31 with FreeRTOS & eGUI is fully available on NXP web pages including application software ...
    Pavel Sustek
    last modified by Pavel Sustek
  • Safety Class B with PMSM Sensorless Drive & RTCESL 4.3 available on nxp.com

    Dear all,   Let me inform about latest MC software product update: New application note AN5321 Safety Class B with PMSM Sensorless Drive is fully available on NXP web pages including application software AN5321...
    Pavel Sustek
    last modified by Pavel Sustek
  • KEA128BLDCRD Sensor-less BLDC

    I have the KEA128BLDCRD demo board.  No problems getting it up and running with the included motor.  I am trying to drive a custom sensor-less BLDC motor - 3 phase, 10 magnetic poles.  I cannot get it...
    Carlos Hidalgo
    last modified by Carlos Hidalgo
  • MISSING library file for PMSM operation in KV10

    Hi,I am using my own board of MKV10Z32VLC7 which belongs to Cortex-M0+ Based Microcontroller. While I trying to porting the code I found that there is no ALPHA and BETA coordinates for the M0 based microcontrolle...
    VIGNESHKUMAR P
    last modified by VIGNESHKUMAR P
  • BLDC sensorless control Using LPC17xx

    Hi guys, recently I've been working on LPC1768 for sensorless control of BLDC motors, but I have numerous problems regarding of ADC sampling for BEMF zero crossing detection and in short position estimation. Actually ...
    Milad Mohammadi
    last modified by Milad Mohammadi
  • How to calculate AMCLIB_PMSMBemfObsrvAB_A32 in C programming without the library file.

    Hi I'm using my own board of MKV10Z32VLC7(CM0 based device). Unfortunately the AMCLIB_PMSMBemfObsrvAB_F16 is not available for CM0 based devices. It's based on FOC control of PMSM motor.   We are processing with...
    VIGNESHKUMAR P
    last modified by VIGNESHKUMAR P
  • Suitable H-Bridge Part To Driver Mirror Motor / Actuator

    Does NXP Has Similar Solution Like ST's L9953XP Series For Door Zone Motor Control? I Find Some Part Like H-Bridge Gate Driver In This Demo Article Car Mirror But It Seems Not Really Well For Retractabl...
    Bright Wang
    last modified by Bright Wang
  • Combined PWM Generation on FTM2

    Hello, please;   How I could do to configure FTM2 module of the MKE02Z64 microcontroller to generate a combined PWM signal (complementary + deadtime) in channels 0 and 1, approximately 25kHz? So many registrars ...
    Daniel Tonn
    last modified by Daniel Tonn
  • Kea  drive stepper motor  by  mc34932 with the  software  MVHBridge

    Dear Expert, Now There is a project which  use the KEA64  drive a stepper motor by mc34932 with the  software  MVHBridge. I want to set the peak current of the driver from   0.2A  to...
    kiger Zhang
    last modified by kiger Zhang
  • Motor Control Reference Solution Packages for ACIM, Release V1.2.0

    Dear all,   Let me inform you that Motor Control Reference Solution Packages for ACIM, Release V1.2.0  is fully available on NXP web page including full set of documentation (DRM, AN and UG).   Supp...
    Pavel Sustek
    last modified by Pavel Sustek
  • Kinetis motor control appropriate for micro pump?

    Hello,   I'm an EE undergraduate student, recently assigned to a research team designing a pump for liquid CPU cooler. The pump impeller is approximately 2 inches (50 mm) in diameter and has slots for permanent ...
    Jerrold Erickson
    last modified by Jerrold Erickson
  • High Voltage EV Kit for BLDC Motor

    Hello,   I have tested HVP-MC3PH. The below option is test condition of Motor.    - KDS : KDS 3.2.0  - S/W : MCRSP_BLDC_V1.3.0  - Used to HVP-KV46F150M Card  - Free master : 2.0.2.4...
    Jeongtae Park
    last modified by Jeongtae Park
  • MCAT Question?

    In MCAT , What array f16TransferCharError[65]  in MID_SM_states.c is used for ? how do I get init value when declaring variables?  
    sung bryan
    last modified by sung bryan
  • Need of PMSM(BLDC) FOC codes for KINETICS KV1x series

    Hi, I am using my own board of MKV10Z32VLC7 , which uses FOC algorithm to control the PMSM(BLDC) motor. I just ported the codes from MC56F82726 that is working fine with that algorithm. But after the porting and and c...
    VIGNESHKUMAR P
    last modified by VIGNESHKUMAR P