• KMS GUI command set and syntax

    Hello, Is there a publicized KMS UART command set and syntax requirement/example document for the KV31? I’d like to multipurpose UART0 for the KMS-GUI, our own command set and possibly our own automated configur...
    Mark Grillo
    last modified by Mark Grillo
  • Running Motor Tuner on my own Motor

    Hello,   I am trying to run the Motor Tuner on a Brushless DC Motor that I have. It is a 24VDC, 0.6AMP (0.42AMP RMS), 500RPM, 15OZ-IN, 2 Pole Pair motor.   I determined the number of pole pairs by running...
    Jacob Andrade
    last modified by Jacob Andrade
  • Measuring Linix Motor's Rotor Flux

    Hello,   I am trying to measure the Rotor Flux of the Linix Motor, but I am getting the "KMS has detected a sensor issue. Please confirm usage of an incremental encoder...." error.   I have tried multiple ...
    Jacob Andrade
    last modified by Jacob Andrade
  • KV31 fixed point math

    Hi,    I am using FRDM-KV31F and FRDM-MC-LVPMSM boards to control a PMSM motor using Kinetis Motor Control, and I noticed that fixed point math is used for the FOC algorithm. Is it possible to use floa...
    Marius Rad
    last modified by Marius Rad
  • Problem connecting TWR-KV46F150M with KMS

    Wondering if anyone has used TWR-KV46F150M with KMS I am having the following message.   " An issue has prevented communication with target MCU: The ping message was not acknowledged. Please check physical ...
    Abdullah mamun
    last modified by Abdullah mamun
  • How to connect HVP-46F150M to KMS?

    Hello, I am developing a 3-PHASE ACIM motor control using a HVP-46F150M and a HVP-MC3PH. At first I tried using the freeMaster solution, where I was able to run my motor, but the calibration process was not succesful...
    Eduardo Carletti
    last modified by Eduardo Carletti
  • How to use KMS with a resolver feedback

    Is it possible to use kinetis motor suite with resolver feedback?     Thanks and Regards Athulya varier Hexmoto controls.
    Athulya Varier
    last modified by Athulya Varier
  • Can't connect HVP-KV31F120M with KMS

    Hi,      When i connect the HVP-Kv31f120M with KMS I'm getting an error message which is the same as discussed in forum " Problem connecting KMS to FRDM-KV31F". All the solutions as discussed have been...
    Athulya Varier
    last modified by Athulya Varier
  • FRDM-KV11z + MCUXpresso IDE + KSDKv2 + I2C example for external sensor

    Can someone help me with a simple I2C example with no interrupt. I tried the SDK example. But doesnt working for an external sensor (TCS3471).
    anoja
    last modified by anoja
  • Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

    I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.  I now would like to create an applicati...
    Randy Fields
    last modified by Randy Fields
  • Motor Measure issue in position control

    Dear,        When i start a position with LINIX-45ZWN24-40 BLDC motor(24V, 2P, 4000R/M) and EB38S6A-1000-3L G2 Encoder, i found a problem in motor measure step as below. Could you tell me how to r...
    Banson Dou
    last modified by Banson Dou
  • Low RPM application

    I need to operate my motor over a speed range that starts below 1 RPM.  Does the motor firmware and Kinetis Motor Suite support this range?
    Randy Fields
    last modified by Randy Fields
  • How to test KMS project with Freemaster

    I have completed one kms project. And i want to test this software with freemaster. So how to do?
    Banson Dou
    last modified by Banson Dou
  • Round robin ADC on HVPKV31

    I'm trying to modify the KMS generated code to enable the round robin sampling of analog inputs on our custom board.  I'm looking in the ADCS_getUserSamples function within the HVPKV31F120M_POS_MXP_1_2_...
    Matt Schafer
    last modified by Matt Schafer
  • Getting errors using FRDM-MC-LVBLDC shield

    I recently bought an NXP development kit for BLDC motor control. The kit includes the following NXP parts FRDM-KV31F MCU development board FRDM-MC-LVBLDC motor interface shield FRDM-MC-LVMTR motor   My objec...
    Belenie Amoranto
    last modified by Belenie Amoranto
  • UART COMMUNICATION BETWEEN K64F AND KV31F

    I am trying to control the PMSM motor connected to KV31F based on trigger I receive from FRDM-K64F via UART using Kinetis Motor Suite (KMS). UART0 in KV31F is being used for PMSM motor control and I'm using UART1 to e...
  • MCZ33976EG电机归零问题

    MCZ33976EG电机驱动芯片,进行电机归零时,两路输出gauge0和gauge1有先后执行顺序之分吗?我在进行步进电机归零时,我用了4个33976的芯片,分别控制8个步进电机,归零时首先让其逆时针旋转到最大角度,然后让其分gauge0和gauge1两组分别发送归零指令,发送完成之后,给定6ms的反弹时间。 1)当指针在零位附近时,归零相对比较准确; 2)当指针未在零位附近时:@       ...
    r z
    last modified by r z
  • Motion Sequence Builder will not compile

    When using the Motion Sequence Builder tool in the Kinetis Motor Suite, I am having trouble compiling the code. Everything works fine when I am working in sensored velocity, but when I am in sensored position it ...
    Michael Bray
    last modified by Michael Bray
  • A problem connecting the KMS to a custom hardware

    Hello, I have a problem connecting the KMS to a custom hardware. I'm working on a Windows 10(32 bit) machine, using the MCUXpresso v10.1.0 and KMS 1.2.0. I do the flash programming and debugging using a SEGGER j-link...
    rumen pasev
    last modified by rumen pasev
  • How to get RDB

    I want get a PMSM RDB,how to get it。   Thanks。     KEA128BLDCRD: 3-phase Sensorless BLDC Motor Control Reference Design Based on Kinetis KEA128 MCUs
    chuntian cai
    last modified by chuntian cai