• Kinetis K60 ADC readings ar way off

    Hi --   I am designing a Kinetis K60 into a project.  I have two boards that both basically work, but the ADC readings don't match.  For simplicity I will focus on the readings from the bandgap, but al...
    GARY OLMSTEAD
    last modified by GARY OLMSTEAD
  • external RAM for Kinetis KV5x (MKV58F1M0VLQ24)

    Hi all,   we are using the Kinetis MKV58F1M0VLQ24 on a custom pcb and plan to implement an additional, external RAM (>= 512kB) via the FlexBus interface, as the memory of the µC doesn't suffice our need...
    Julian Schork
    last modified by Julian Schork
  • K70 and DDR2 SDRAM unstable work

    Hi All, on our custom board ( based on MK70FX512VMJ15 and MT47H64M16HR-3 AAT:H TR) we have problems that appear randomly in the field. The device can work up to 20 days without any problems. Then one DDR byte lane can...
    Vitaliy Avramenko
    last modified by Vitaliy Avramenko
  • K70 DDR2 read failure with increasing temperature

    Hello everybody.   We are using K70 controller (MK70FN1M0VMJ15 rev. 3N96B). Architecture is the same as the tower TWRK70F120 supplied by NXP.   To reproduce the issue, we are running a simple test softwa...
    spiderman
    last modified by spiderman
  • KV46 ADC accuracy issue

    We are now using Kinetis KV46 series controller and want to have all ADC results with less than < 4 counts swingings, given a very stable source.   In our setting, all of the ADC ch are enabled with ADCA...
    Zabel A
    last modified by Zabel A
  • Cyclone FX error $00000007

    Hello, I asked the question to the P&E support but I think I can also ask the question here:   On the Cyclone Fx: Version / Revision: Rev A - v10.13-2.3 Operating System: Windows 10 64-bit Hello, I'm usin...
    arnogir
    last modified by arnogir
  • I2C issues depending on Release/Debug(MKL02Z32)

    Hi, I have been using the I2C code for couple of month and it has been working from time to time. The problem is that sometimes the I2C bus is busy and sometimes not after reset. It seems like when running in Release ...
    claes kjellstrom
    last modified by claes kjellstrom
  • sprintf with float specifier - how to make it work?

    I'm using KDS 3.2.0 with the MKE02Z64VLC4 processor and need to use the sprintf/snprintf functions with the float specifier %f.  However, it will not work.  It shows nothing.  I some other posts that ha...
    Bill Sousan
    last modified by Bill Sousan
  • Is enabled security and disabling Mass Erase enough to protect Kinetis K63 based devices from unauthorized access?

    Hi,   We are developing a product using Kinetis K63. As the security is of paramount importance for the application, we want to make sure that once the product is deployed in field it can not be accessed by anyo...
  • FTM counter synchronization of KV31

    In the KV31F Sub-Family Reference Manual,I can see “However,the FTM counter must be synchronized only by the enhanced PWM synchronization” from 37.4.11.10 FTM Counter Synchronization. I think this sentenc...
    相国 尹
    last modified by 相国 尹
  • S9KEAZN64: How to disable the watchdog?

    Good morning. My name is Daniele Fingolo and I am a software developer of SMH Technologies. I'm trying to program the S9KEAZN64 device in question with a programmer that we developed. We are able to communicate with ...
    Daniele Fingolo
    last modified by Daniele Fingolo
  • is there any i2c (master) to spi (slave)  bridge conerter

    Hi,    we need spi(salve ) to i2c(master) converter for one of our applications, Is there any module available like that? we found i2c(slave) to spi(master) converter SC18IS602B. But our application requi...
    jhansi palepu
    last modified by jhansi palepu
  • MKL16 UART can not receive

    Hi , I had some questions about Uart receive when i use uart base on MKL16 . I had create project by PE(Driver Suite v10.4) ,now uart can send data ,   but can not receive data . Belows is my codes: ...
    Li ADai
    last modified by Li ADai
  • Internal flash memory security

    Hello, I am using Kinetis k64 and configuring it's internal flash memory to be secured. In NXP's memory security application notes AN4507.pdf  its written that "This means that firmware residing in the fla...
    dotan goldberg
    last modified by dotan goldberg
  • KV58: Acessing ITCM

    I plan to create a few data variables in ITCM (RAM Partition 2) to run a few memory tests on a MKV58F1M0VLQ24 MCU. Do I have to configure register(s) to enable ITCM? If yes then which register(s)?
    lsrbigfoot
    last modified by lsrbigfoot
  • Bare Metal DMA, Changing DMA_DCR destination address during mid transfer

    Hi all,   I'm currently working on a project that requires me to PWM a few LEDs at varying duty cycles. I was thinking of using DMA from a static buffer to the target TPM channel value register. The target ...
    Matthew Mak
    last modified by Matthew Mak
  • Not jumping to application from secondary bootloader

    I have gone through many related threads on this forum, like "Jump from Seondary...", "Kinetis bootloader...", etc. but haven't found the answer.   For failsafe update of firmware we have implemented a...
    Mohsin Butt
    last modified by Mohsin Butt
  • MCUXpresso IDE v11.2.0 Now Available

    We are pleased to announce that MCUXpresso IDE v11.2.0 (build 4120) is now available. This is a major new version of the IDE, and contains new features, enhancements and bug fixes over the previous versions, incl...
  • HID-HOST with FRDM-KL25

    Open video

    Adrian Cano
    last modified by Adrian Cano
  • RTC issue in K66 Custom Board

    Hi All,   We are using Kinetis K66 controller(MK66FN2M0VLQ18) for our custom board. Actually this board is an upgraded version,old one is having K60 controller. Now we are facing an issue in RTC. Out of 10 board...
    ANAND S
    last modified by ANAND S