• NXP PCA9517 B-side Vol的数值与SMBUS2.0协议中Vol的数值有出入,烦请解答一下?

    NXP PCA9517 B-side Vol的数值与SMBUS2.0协议中Vol的数值有出入,烦请解答一下?   PCA9517规格书中 B -side Vol Min = 0.4V Max = 0.6   SMBUS2.0协议 Vol Max = 0.4V
    michael yang
    last modified by michael yang
  • SC18IS602B: Activating all four GPIO disables SPI interface?

    I intend to use the SC18IS602B to control a multiplexed line of LEDs using i2c. For this, I would need to use three GPIO pins to control a 3:8 demux chip and one GPIO pin to toggle the latch enable signal of a sh...
    Bo Thompson
    last modified by Bo Thompson
  • Hdmi lcd interface in NXP® i.MX 6SoloX processor using TDA19988 driver ic

    Hello,   I am using NXP® i.MX 6SoloX related board and I want to connect one 1024x600 hdmi touch screen display with it so I buy one display which is (https://www.waveshare.com/7inch-hdmi-lcd-c.htm ) &...
    hiten chauhan
    last modified by hiten chauhan
  • Sensorless Field Oriented Control using MC56F84x

    Are there any resources available for FOC motor control using the MC56F84x or MC56F83x microprocessors (eval boards, software, application note)?    I saw this for the "MX RT Series Crossover MCUs and on V ...
    Craig Asgaard
    last modified by Craig Asgaard
  • 74LVC4066BQ

    Hi, we have chosen 74LVC4066BQ chip and need to provide Pullup resistor in enable pin's (nE). So please share the nE pin required current details. Not able to identify the value in datasheet.   Thanks &am...
    panneerrajangunasekaran
    last modified by panneerrajangunasekaran
  • Repeat LIN failure with TJA1020

    Hello. I'm just a mechanic trying to fix a problem car, but here's the story.   I have a vehicle that has had a repeat failure of the LIN bus. This has required the cluster to be replaced each time to get LIN co...
    Mike Adema
    last modified by Mike Adema
  • Suite56 for DSP56311

    I am working on a project to transfer DSP56311 assembly code to C. I need a simulator to run the code to better understand the assembly code. It looks Suite56 could do the job but I cannot find any valid download link...
    zz zz
    last modified by zz zz
  • FORMAT DESFIRE EV1

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying se...
    Leonov Dima
    last modified by Leonov Dima
  • In MPC5744P, how do I reset the count after it stops counting in periodic mode.And the count has not reached the comparison value.

    void ETIMER_DRV_SetTimerTicks(const uint16_t instance, const uint16_t channel, const uint16_t count) { ETIMER_Type * base; DEV_ASSERT(instance < ETIMER_INSTANCE_COUNT); DEV_ASSERT(channel < ETIMER_CH_COUNT)...
    金 雨馨
    last modified by 金 雨馨
  • Freemaster Tools version 2.0

    A customer request Freemaster tools ver2.0, I attach it here so that customer can download the tools from the site. BR XiangJun Rong
    xiangjun.rong
    created by xiangjun.rong
  • 1032TCEA motorola/freescale Datasheet needed

    Dear community, Can anyone help me to get data on the 1032TCEA from Motorola? I have been looking for the past few weeks but information is nowhere to be found. The component is used in some sort of interface between...
    J. D.
    last modified by J. D.
  • SC18IM700IPW Temp Failures

    We are using the SC18IM700IPW  We have had issues at -40C and also at +79 C with the parts not functioning. When they fail they are unresponsive on the bus.   There are 2 applications within our company ...
    John Eckland
    last modified by John Eckland
  • SAF7741HV

    Anybody can help me, I need datasheet  SAF7741HV
  • SGTL5000 MIC BIAS pin

    Hello, I'm using SGTL5000 codec (QFN20) with micro input. I have a question about typical application schematic (figure 20 in datasheet). How must I connect MIC BIAS pin if I use the internal bias resistor? Interna...
    Sylvain Bouriot
    last modified by Sylvain Bouriot
  • DSP56800E QUICK START Version 2.5

    hi. can any one post a link of  DSP56800E Quick Start Version 2.5 for download? thanks.
    milad fozooni
    last modified by milad fozooni
  • floating point to fractional conversion

    Hey,         I have a sample code using calculations in floating point, that i want to use on my MC56F82748 DSC platform using using fractional maths  so i can use the FSE...
    fasihahmed
    last modified by fasihahmed
  • Problem With Quick Start r2.7

    hi every one i use Freescale Codewarrior IDE version 8 (but in about menu ide version is 5.9) for mc56f8006. i have problem with  NXP Stationery New Project Wizard. i cant add this to codewarrior new proj...
    milad fozooni
    last modified by milad fozooni
  • NXP Stationery New Project Wizard in codewarrior ide 5.9

    hi every one i use Freescale Codewarrior IDE version 8 (but in about menu ide version is 5.9) for mc56f8006. i have problem with  NXP Stationery New Project Wizard. i cant add this to codewarrior new proj...
    milad fozooni
    last modified by milad fozooni
  • DB problem of 2874

    BGA2874Adjust to the voltage of 2.5V, 18 mA is almost 10 DB worse. The two tubes on the graph add up to noise, right?
    许泽林 许
    last modified by 许泽林 许
  • TJA1044

    IF THE VI0 pin is active i.e 3.3v and 5 volt for vcc is not active, will the transceiver work. But its told that Vio pin will switch on low-power receiver.
    shubham singh
    last modified by shubham singh