• Suite56 for DSP56311

    I am working on a project to transfer DSP56311 assembly code to C. I need a simulator to run the code to better understand the assembly code. It looks Suite56 could do the job but I cannot find any valid download link...
    zz zz
    last modified by zz zz
  • The tools 56F800e Flash programmer

    I attach the 56F800E flash programmer so that customer can download it. BR XiangJun Rong
    xiangjun.rong
    last modified by xiangjun.rong
  • FORMAT DESFIRE EV1

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying se...
    Leonov Dima
    last modified by Leonov Dima
  • In MPC5744P, how do I reset the count after it stops counting in periodic mode.And the count has not reached the comparison value.

    void ETIMER_DRV_SetTimerTicks(const uint16_t instance, const uint16_t channel, const uint16_t count) { ETIMER_Type * base; DEV_ASSERT(instance < ETIMER_INSTANCE_COUNT); DEV_ASSERT(channel < ETIMER_CH_COUNT)...
    金 雨馨
    last modified by 金 雨馨
  • Freemaster Tools version 2.0

    A customer request Freemaster tools ver2.0, I attach it here so that customer can download the tools from the site. BR XiangJun Rong
    xiangjun.rong
    created by xiangjun.rong
  • 1032TCEA motorola/freescale Datasheet needed

    Dear community, Can anyone help me to get data on the 1032TCEA from Motorola? I have been looking for the past few weeks but information is nowhere to be found. The component is used in some sort of interface between...
    J. D.
    last modified by J. D.
  • SC18IM700IPW Temp Failures

    We are using the SC18IM700IPW  We have had issues at -40C and also at +79 C with the parts not functioning. When they fail they are unresponsive on the bus.   There are 2 applications within our company ...
    John Eckland
    last modified by John Eckland
  • SAF7741HV

    Anybody can help me, I need datasheet  SAF7741HV
  • SGTL5000 MIC BIAS pin

    Hello, I'm using SGTL5000 codec (QFN20) with micro input. I have a question about typical application schematic (figure 20 in datasheet). How must I connect MIC BIAS pin if I use the internal bias resistor? Interna...
    Sylvain Bouriot
    last modified by Sylvain Bouriot
  • DSP56800E QUICK START Version 2.5

    hi. can any one post a link of  DSP56800E Quick Start Version 2.5 for download? thanks.
    milad fozooni
    last modified by milad fozooni
  • floating point to fractional conversion

    Hey,         I have a sample code using calculations in floating point, that i want to use on my MC56F82748 DSC platform using using fractional maths  so i can use the FSE...
    fasihahmed
    last modified by fasihahmed
  • Problem With Quick Start r2.7

    hi every one i use Freescale Codewarrior IDE version 8 (but in about menu ide version is 5.9) for mc56f8006. i have problem with  NXP Stationery New Project Wizard. i cant add this to codewarrior new proj...
    milad fozooni
    last modified by milad fozooni
  • List for DSC bootloaders

    Here is a list for the bootloader projects and their user manual for all of the targets in DSC family
    Fiona Kuang
    last modified by Adrian Puga Candelario
  • NXP Stationery New Project Wizard in codewarrior ide 5.9

    hi every one i use Freescale Codewarrior IDE version 8 (but in about menu ide version is 5.9) for mc56f8006. i have problem with  NXP Stationery New Project Wizard. i cant add this to codewarrior new proj...
    milad fozooni
    last modified by milad fozooni
  • DB problem of 2874

    BGA2874Adjust to the voltage of 2.5V, 18 mA is almost 10 DB worse. The two tubes on the graph add up to noise, right?
    许泽林 许
    last modified by 许泽林 许
  • TJA1044

    IF THE VI0 pin is active i.e 3.3v and 5 volt for vcc is not active, will the transceiver work. But its told that Vio pin will switch on low-power receiver.
    shubham singh
    last modified by shubham singh
  • Demo code for  fxps7400d4

    Demo code for  fxps7400d4?
    zengxing yuan
    last modified by zengxing yuan
  • PCA9698  ERROR

    HI I use PCA9698 to solve the problem of insufficient IO port.   But there are problems in the use process:   I use the IO of pca9698 to control the digital switch(ADG1612),when the control port of the di...
    L SJ
    last modified by L SJ
  • I might change demodulation metod in system-on-chip SAF360x?

    Tell me please, I might change demodulation metod in system-on-chip SAF360x? I must accept a digital signal on the basis of DRM, but modified.
    Grigoriy Chuvilin
    last modified by Grigoriy Chuvilin
  • I did not compile "Hello World" .cpp code in MCUXpresso

    Hello,   I'm working in MCUXpresso IDE 11.0. I'm working in .cpp source file and generate a file with GNU C++ 11(-std=gnu++11) Standard toolchain. I want to Build and compile basic hello world code with this to...
    PRATIK PANCHAL
    last modified by PRATIK PANCHAL