• MC56F802x 56800E core - from ADC value to real Frac16

    Hello,   I'm using MC56F8023 DSC and I would like to better understand relatioship between ADC value read from A/D converter and the Fractional arithmetic. Consider this example (based on AN1911).   We hav...
    sandrom
    last modified by sandrom
  • SCI driver for DSP56309

    Because customer can not receive any email with attachment, I attach the SCI driver here so that the customer can download it from here.
    xiangjun.rong
    created by xiangjun.rong
  • DSC FLASH PROGRAMMER ERROR ON WINDOWS 10 OS.

    ` we are using 56800E software to program controller (MC56F8247) with windows 7 os now we upgrade our pc to windows 10.now we are using freescale dsc flasher to program controller but we have facing error.  ...
    ashok singh
    last modified by ashok singh
  • Download link: Suite56

    Hello everyone,   i cannot find a download link for Suite56 Suite56 for DSP 566xx/DSP563xx|NXP    How to get those files? Is the link still hidden somewhere?
    Vinzent Meier
    last modified by Vinzent Meier
  • DSC56800/E xMAP question

    Tool: Codewarrior tool for DSC56800/E version 8.3 build 091203 target: 56F8367 processor   Could someone help explain the xMAP below.  I have z1_table[] declared as below, and I think the array is in interna...
    brian dang
    last modified by brian dang
  • Getting problem while configuring PLL and using QSCI module

    I am using MC56F82313vlc IC. I wanted to used QSCI0 module with a 9600 as its baud rate.Configure PLL to max frequency i.e OCCS_DIVBY = 0x2071 with default trimming factor i.e 0x220 and using ROSC8M as internal 8MHZ r...
    Shreeram Muley
    last modified by Shreeram Muley
  • Getting problem while configuring PLL and using QSCI module

    I am using MC56F82313vlc IC. I wanted to used QSCI0 module with a 9600 as its baud rate.Configure PLL to max frequency i.e OCCS_DIVBY = 0x2071 with default trimming factor i.e 0x220 and using ROSC8M as internal 8MHZ r...
    Shreeram Muley
    last modified by Shreeram Muley
  • GTL2010 voltage level translator query

    Hi,   I want to use GTL2010 in my design where i have the requirement below:  Voltage translation : 1.8V to 2.8V Direction : Bidirectional Sensing feature : Auto sensing   According to the datashee...
    khemraj suthar
    last modified by khemraj suthar
  • MC56F8255 Flash-Clockdivider

    Hello, i have a question about the MC56F8255 flash-clockdivider (register HFM_CLKD.Div[5..0]): The user-manual http://www.nxp.com/assets/documents/data/en/reference-manuals/MC56F825XRM.pdf says i should avoid: (1...
    Ulrich Neumayer
    last modified by Ulrich Neumayer
  • MC56F8335 program flash size

    Hi, i have a question about the MC56F8335 program flash size. The technical data sheet: http://www.nxp.com/assets/documents/data/en/data-sheets/MC56F8335.pdf says: * Table 4-1: Program Flash 64kB * Table 4-4: Int...
    Ulrich Neumayer
    last modified by Ulrich Neumayer
  • can network communication

    Dear sir       execuse me, I write the send code of can network communication, but the sent data can not be received correctly in codewarrior 10.4, can you give me an example in C language of...
    guo chunhua
    last modified by guo chunhua
  • Porting Legacy DSC Applications to Freescale’s 32-bit DSC Family

      Run DSP Test Sample Projects on an MC56F84789!   Previously the huge collection of Processor Expert Example programs for the DSP5685x devices was not easy to run on recent devices such as the MC56F84789...
    John Winters
    last modified by John Winters
  • How to mass errase a secured device of MC56F82xxx (not MC56F82xx)

    The following script may be used with a USB TAP, or the primitive commands in the latter part of the script may be adopted to other debugging and programming systems.   The script follows.   --------------...
    John Winters
    last modified by John Winters
  • (MC56F84xxx) Debug Reference Manual to be available to flash programmer and debugger vendors

    Please contact your Freescale sales representative and establish an NDA for:   (MC56F84xxx) Debug Reference Manual   It should be available next week.     This document will be made available...
    John Winters
    last modified by John Winters
  • How to use PESL (Processor Expert Software Library) without generating compile errors - here's how:

    To avoid errors, rename the peripheral initialization component to a unique name!  That's it!       This is done by first   --adding the inialization component, selecting advanced at the up...
    John Winters
    last modified by John Winters
  • MC56F82743 Config bug of Quick Start r2.6

    We want to config SCI_0 using Quick Start r2.6, the following two pins are configured as RXD0 and TXD0 independently, then save.the change. GPIO C8     RXD0 GPIO C9     TXD0 ...
    Larry Yang
    last modified by Larry Yang
  • This documents the required initialization sequence for the MC56F8400 series eFlexPWM with micro-edge

    Announcement:       When using the fractional edge delay on the eFlexPWM, there is the requirement to not program pulses narrower than 3 clock cycles. This requirement is only for channels using the ...
    John Winters
    last modified by John Winters
  • 求《AN4813:Encoder Position and Speed Sensing Utilizing the Quad Timer on the MC56F827xx DSCs》这篇文章的工程附件

    求《AN4813:Encoder Position and Speed Sensing Utilizing the Quad Timer on the MC56F827xx DSCs》这篇文章的工程附件。带详细程序的工程附件。 谢谢!
    建雄 惠
    last modified by 建雄 惠
  • Freescale DSC Flasher :: Digital Signal Controller Stand-Alone Flash Programmer

    Access AN4824 at www.freescale.com and AN4824SW for the executalbe.   The Freescale DSC Flasher is a stand-alone flash   programmer for the MC56F8xxx family of Digital Signal   Controller products. It ...
    John Winters
    last modified by John Winters
  • MC56F84789VLL maximum sys_clk_2x signal frequency

    Dear all,   On the reference manual MC56F847XXRM Rev. 2.0, 03/2016, I noticed that the max frequency of sys_clk_2x should not be more than 200MHz, as shown in figure 18-3, page 352. Is it a maximum absolut...
    Federico Gobetti
    last modified by Federico Gobetti