• List for DSC bootloaders

    Here is a list for the bootloader projects and their user manual for all of the targets in DSC family
    Fiona Kuang
    last modified by Adrian Puga Candelario
  • 56800E_FSLESL_r3.0.exe

    Motor control library 56800E_FSLESL_r3.0
    xiangjun.rong
    last modified by xiangjun.rong
  • The Capture feature of eFlexPWM module

    The eFlexPWM module is an important module, integrated in DSC, Kinetis KV, i.mxrt, MPC56xx families, it can output PWM signals. But it has capture function, can accept synchronous captured signal(synchronous  wit...
    xiangjun.rong
    last modified by xiangjun.rong
  • The feature Fraction Delay logic with Micro-Edge Placement for eFlexPWM module

    For switch mode power supply application, the output voltage resolution is dependent on PWM resolution, the PWM resolution is dependent on the PWM module driving clock(IP Bus clock) frequency and PWM signal output fre...
    xiangjun.rong
    last modified by ebiz_ws_prod
  • The eFlexPWM dithering feature FOR MC56f84xxx AND MC56f82xxx

    For switch mode power supply application, the output voltage resolution is dependent on PWM resolution, the PWM resolution is dependent on the PWM module driving clock(IP Bus clock) frequency and PWM signal output fre...
    xiangjun.rong
    last modified by ebiz_ws_prod
  • Suite56 tools downloading

    Now, the DSP56300 and DSP5672x have not roadmap, on the NXP home page, the Suite56 tools is removed. But there are customers who need to use the tools, I put the tools here so that customer can download it free of cha...
    xiangjun.rong
    last modified by ebiz_ws_prod
  • Sleeping Power Supply - A power supply that sleeps a lot of the time in core stop mode

    With a goal of energy conservation, a project is herein documented and attached as a zip file showing how to operate the key peripherals for a simple power supply (which can be embelished as desired).   All of t...
    John Winters
    last modified by ebiz_ws_prod
  • Flash-over-jtag.exe tools

    Hi, all The flash-over-jtag tools is a tools which can program the DSP56F80x family with wiggler, per customer request, I attach it here so that customer can download it directly. BR Xiangjun Rong
    xiangjun.rong
    last modified by xiangjun.rong
  • How to generate duty cycle of PWM_X for  eFlexPWM module

    The documentation talks about the PWM_nX signal, gives the register setting to set up the duty cycle of PWM_X, and tricks to control the timing of PWM_nX, and the restriction for PWM_X.
    xiangjun.rong
    last modified by xiangjun.rong
  • Two or more eFlexPWM synchronization for KV4x, KV5x, MC56F84xxx and MC56F82xxx

    The documentation describes how to have two eFlexPWM module to synchronize based on MC56F84789, give the waveform of PWM signals copied from oscilloscope, which shows that all PWM signals from eFlexPWMA and eFlexPWMB ...
    xiangjun.rong
    last modified by xiangjun.rong
  • Towards more robust start-up code

    Standard DSC startup code most often includes a do loop. That do loop execution assigns a known value to the LA register. If you are using startup code that does NOT include a do loop, you need to explicitly initia...
    John Winters
    last modified by Diana Torres
  • Using the CodeWarrior TAP with the DSC

    The USB TAP for DSC has been used with the DSC for many years. Provision has been made to utilize a newer programming hardware module, the CodeWarrior TAP. Now, with a simple upgrade to software (the ccs directory o...
    John Winters
    last modified by Diana Torres
  • gct_cfg_pinout.zip

    Update for QuickStart GCT V2.6.3, Updates CPU peripherals and pinout page for all supported devices.
    Jaroslav Pajskr
    last modified by Jaroslav Pajskr
  • gct56F800.zip

    Graphical configuration tool for QuickStart 2.6 for DSC, V2.6.31, To apply the update unpack the file to <DSC56800EX_Quick_Start_r2.6_path>\tools\gct\
    Jaroslav Pajskr
    last modified by Jaroslav Pajskr
  • CW_TAP_Overview.mov

    Codewarrior-Tap Overview
    Charlie Wu
    last modified by Charlie Wu