• MCF5216 software reset

    How generate the reset by software on MCF5216.
    paolo ziveri
    last modified by paolo ziveri
  • MC68376

    We have used the MC68376 for replacement of the MC68336 in our product.  But there are two CAN pins (pin1-CANTX0 and pin160-CANRX0) on the MC68376 will not be used for our purposes but need to know how to termina...
    philip vuong
    last modified by philip vuong
  • code portability for legacy 68K devices

    I have an application which runs on legacy 68020 processor with external FPU. This unit was deployed 20 years ago , which requires replacement. Is it possible to port  to the newer coldfire platform without modif...
    vishnu prasad
    last modified by vishnu prasad
  • MC68376

    CAN
    philip vuong
    last modified by philip vuong
  • uTasker 1.4 Unknown USB device

    Hi ! I'm using the uTasker 1.4 for kinetis on a custom board. I followed the steps on this post uTasker Bootloader Porting Guide ,I loaded the bin file and the board goes on bootloader mode but when i connect the USB...
    Alberto Peña
    last modified by Alberto Peña
  • M68EN360 SPI delay between read/write

    Hi,   I am using MC68EN360 for one of the project. I wanted to interface ethernet chip (ENC28J60) using SPI with M68K. I have configured the clock of SPI to 6.25Mhz and the SPI mode  '0' is set . The probl...
    Jagadish C
    last modified by Jagadish C
  • ebook "Designing Embedded Applications with ColdFire"

    Hello, Can someone tell me where or how I can get a copy of the ebook "Designing Embedded Applications with ColdFire" for stritcly private use.   Thank you very much   Werner
    Werner Kurzbauer
    last modified by Werner Kurzbauer
  • Need ee emulation on SPC560

    Does anyone know of an app note or other doc that will detail how to emulate EEPROM on the data flash of an SPC560 / MPC560 ?
    James Teske
    last modified by James Teske
  • How do I unsubscribe from NXP community?

    Can't find link to unsubscribe
    Sagar Sankaran
    last modified by Sagar Sankaran
  • MCF5270 I2C Master receive multiple bytes timing

    Hi-   I've asked this NetBurner Community Forum, but haven't seen any responses.   In I2C Master RX mode, after End of ADDR Cycle, after Dummy Read from I2DR, responding to IIF, not Last Byte to be Re...
    Carl Kugler
    last modified by Carl Kugler
  • sqlite in imxrt

    Hi, I want to port sqlite in IMX-RT. But i am unable to get any help on this. Is there any example available for porting sqlite database to IMX-RT bare metal.
    Vivek Aggarwal
    last modified by Vivek Aggarwal
  • mcf5213 IDE

    Hello,    I need to get the compiler for microprocessor ColdFire MCF5213. And this compiler should be able to run with Window 7 and Window 10.   Do you have any recommendation. I know that Code Warri...
    Darren Gan
    last modified by Darren Gan
  • Failed to execute initialization script

    CW7.2下调试下载出现Failed to execute initialization script
    bingguo zhang
    last modified by bingguo zhang
  • cold fire controller( MC51CN128) Problem

    Hi, we are using coldfire controller for ethernet application. Recently we are getting one issue that PLL is not getting locked. Due to this Phyclock is not getting generated. we are using 25Mhz crystal , when running...
    vamsi Dhanunjaya Rao
    last modified by vamsi Dhanunjaya Rao
  • [嵌入式linux] 两个相同产品间的并机设计

    MCU parallel strategy design Three methods are used: 1. Automatically access the new slave at any time, the power is also automatically added, the master can allow the slave to open the strong after the slave is integ...
    julian cheng
    last modified by julian cheng
  • RT1052 FLEXCAN for any ID communication

    I am testing the RT1052's flexcan demo. How to modify the configuration to receive the data from any ID?
    Yu fuhua
    last modified by Yu fuhua
  • PROBLEM WITH CARD M5235BCC RETURNS VERIFY ERROR WHEN SCHEDULING FILE .S19

    Dear  i having trouble in downloading  archive xxx.S19  returnn verify error   PC WIN 7 32BYTES CFLASHER 3.10 MULTILINK UNIVERSAL  D MC5235BCC AM29LV160DB(1X16) ALGORITM
    EDUARDO ESCOBEDO
    last modified by EDUARDO ESCOBEDO
  • MCF5407 UART interrupt masks seem inverted

    Hi, I am having a lot of trouble configuring the UART on the MCF5407. The only way I was able to make the UART work with the interrupt is to inverse the UIMR bit logic; the datasheet says that we must set TxRDY and FF...
    Jasmin Bolduc
    last modified by Jasmin Bolduc
  • CodeWarrior 5.9 debugging with multilink: unable to put breakpoints on executed instructions.

    I have the following piece of code for coldfire V2 MCF52258:     According CW tutorial, dashes at left column tell us where we can set a breakpoint. As it can be seen, a low red point is tried to be put a...
    Eugenia Suarez
    last modified by Eugenia Suarez
  • MCF51JM Drivers

    Hi!   Using this micro in Windows 7 and 8 it's not possible to be recognized. Under Windows 10 is okey. I haven't found drivers for Windows 7 and 8. I need your help.   Thanks in advance.
    Arturo Sangros
    last modified by Arturo Sangros