• MCF548x DDR Address?

    Hey!  I'm setting up the  SDRAM Controller (SDRAMC) on the MCF5485.   I had a small question.  Once the SDRAMC is initialized, what is the address of the SDR/DDR memory?   If I understa...
    Zachary Wilcox
    last modified by Zachary Wilcox
  • LX2160A Reconstructed Clock

    Hi Team,   The LX2160A has 2 recovered or reconstructed clock. What is the use of these pins? Can I recover the PTP clock from the serdes via these pins. If possible how to do hardware connections.
    Muhammed Mufeed
    last modified by Muhammed Mufeed
  • Problemas con BITIO en la familia MCF5441X

    Hola a todos!   Estoy teniendo problemas con la familia de microcontroladores MCF5441X con algunas librerias del processor expert.  Los componentes de alto nivel (BITIO, TIMERs, etc...) aparece un error ll...
    Juan Luis Lopez
    last modified by Juan Luis Lopez
  • MCF5271 IBIS model?

    Hi!   I'm looking for an IBIS model for the MCF5271 microprocessor.  The website currently just has the BSDL files.  Anyone have one or know where I could get it?   Thank you! Geoffrey
    Geoffrey Burnham
    last modified by Geoffrey Burnham
  • MCF54415CMJ250 BSDL File

    Hi everyone, I'm looking for BSDL file for MCF54415CMJ250 ColdFire Microcontroller. Does anybody can help me?   Greetings!
    Aurelio Siordia
    last modified by Aurelio Siordia
  • AppTRK.elf file missing in MCF5282 pre installed Ulinux

    Hi, I am working on DNP/EVA6(REV 1.2 board) with coldfire MCF5282CVM66. When I read the documentation, it was mentioned that I have to start the AppTRK agent(Apptrk.elf) to have a communication between the evaluation...
  • BITIO with MCF5441X

    Hello everyone!   I'm having problems with the MCF5441X family of microcontrollers with some Processor expert libraries. The high level components (BITIO, TIMERs, etc...) get an error called: "This component is...
    Juan Luis Lopez
    last modified by Juan Luis Lopez
  • Help ID board With MCF5213 processor.

    I have a box of these boards in my stock and cannot figure out if I need them or not, seriously can't find anything on them through my normal database.  I know it's a long shot but was wondering if anyone here ca...
    Matthew Petro
    last modified by Matthew Petro
  • flexCAN message buffer on MCF548x

    Hi all,   I have a question about flexCAN message buffer on MCF548x. flexCAN has 16 MBs for Tx and Rx.   I set 14 MBs(MB#0 ~MB#13) for Rx and 2MBs for Tx. And, I set same ID(i.e. 0x4AA) to MB#2 and ...
    CK Kim
    last modified by CK Kim
  • MCF5485 Flexbus lines level at start up?

    Hey! I have a question as to what level the Flexbus lines come up as on the MCF5485.   The Table 2-1 of the RM shows FBCS[5:0] and BE come up as high. However, table 17-1 shows they come up as Hi-Z
    Zachary Wilcox
    last modified by Zachary Wilcox
  • LS1021ATSN-PA

    根据教程将sdcard.img编程到sd卡中之后,我将sd卡插入板中,加电,然后使用pc将其连接到板中。我发现我的PC无法识别串行端口。
    junbin liu
    last modified by junbin liu
  • mcf5441x, esdhc, BLKATTR question

    Hi all,   working on a Linux driver for this module,   on CMD 18 (and other), from the upper layer, i am getting a value of 0x1200 (4608) for block size (BLKSZE field). As a bit-width, this value can be a...
    Angelo Dureghello
    last modified by Angelo Dureghello
  • Difference between MC68376BGMFT20 and MC68376BGMAB20

    Hi everybody,   I'm looking for the difference between these two µprocessors : - MC68376BGMFT20 and MC68376BGMAB20   I've found some informations in this file : https://www.nxp.com/files-s...
    FABRICE PEDEN
    last modified by FABRICE PEDEN
  • mcf52277,复位输出拉低

    你好,mcf52277成熟系统,最近刚做了一批板子,烧上程序,上电正常运行,上电两三个小时后,突然出现黑屏,发现rtsout(复位输出)拉低,复位信号灯亮了,按复位键没有效果,重启后正常,但启动时间比较长,几秒,请问,什么原因导致复位输出信号拉低?谢谢
    zhang guofeng
    last modified by zhang guofeng
  • mcf52277问题

    你好,mcf52277成熟系统,最近刚做了一批板子,烧上程序,上电正常运行,上电两三个小时后,突然出现黑屏,发现rtsout(复位输出)拉低,复位信号灯亮了,按复位键没有效果,重启后正常,但启动时间比较长,几秒,请问,什么原因导致复位输出信号拉低?谢谢
    zhang guofeng
    last modified by zhang guofeng
  • Problems with FLEXCAN on a MCU52255CAF

    Hi, good morning, I'm tryin to setup de flexcan in a MCU52255CAF. I have a problem setting the baud rate in the microcontroller. I've followed the chapter "32 Flexcan from MCF52259RM." I can't communicate two device...
    Santiago López Pina
    last modified by Santiago López Pina
  • gHaving trouble getting DSPI working with eDMA.

    Using MCF5441x CPU, I have been working on code to manage an SPI link to another CPU.  I was able to configure the DSPI module to operate with the peer processor (we're the slave in the link), but when I attempt ...
    Adam Crowder
    last modified by Adam Crowder
  • Reproduce part of m68000 reference manual in open source project

    Hi, I'm writing an open source extension to vscode  to code in assembly for the m68000. I would like to reproduce some parts of the m68000 reference manual as inline documentation : https://www.nxp.com/fil...
    Paul Raingeard
    last modified by Paul Raingeard
  • Software DEMOJM and other

    Hello. And where can I download a disk image from DEMOJM (or from JMBADGE2008, EVB51JM128, DEMOFLEXISJMSD). And also the files that are used in the manual AN3927?
    sergey ivanov
    last modified by sergey ivanov
  • esdhc, timeout some time after cmd 18

    Hi all,   i am working inside a ColdFire mcf54415 esdhc driver in linux (the sdhci layer is common), so the issue may be visible on chips with same/similar controller too as imx and others.   After i mount...
    Angelo Dureghello
    last modified by Angelo Dureghello