• Question about Coldfire JSR with PC indirect

    I was analyzing the binary output of CodeWarrior v11 for an MCF5485 (Coldfire v4e) bareboard example project.   I found that this inline assembly routine: asm __declspec(register_abi) void _startup(void) { &#...
    Dan Filbey
    last modified by Dan Filbey
  • SDRAM Controller Reg SDMR latch data question

    I'm working with the MCF5485 and setting up DDR DRAM. I'm attempting to set the SDMR register.  It appears it doesn't latch the data unless I also set the command bit. Here's an arbitrary example wher...
    Zachary Wilcox
    last modified by Zachary Wilcox
  • Need help identifying evaluation board EST Wind River 5307

    Hello there. I was trying to get documentation and/or CD with contents (image or zipped file of that) for this particular 5307 Coldfire based board (PC104 format): EST Wind River Ref. MDPBAA-0649    ...
    MOISES SALMERON
    last modified by MOISES SALMERON
  • MCF5484 BSDL File

    Hello, I am looking for the BSDL file for the MCF5484CVR200 Coldfire v4e microcontroller.   Is it possible to get this file?   Thanks.
    Dan Filbey
    last modified by Dan Filbey
  • MCF548x DDR Address?

    Hey!  I'm setting up the  SDRAM Controller (SDRAMC) on the MCF5485.   I had a small question.  Once the SDRAMC is initialized, what is the address of the SDR/DDR memory?   If I understa...
    Zachary Wilcox
    last modified by Zachary Wilcox
  • LX2160A Reconstructed Clock

    Hi Team,   The LX2160A has 2 recovered or reconstructed clock. What is the use of these pins? Can I recover the PTP clock from the serdes via these pins. If possible how to do hardware connections.
    Muhammed Mufeed
    last modified by Muhammed Mufeed
  • Problemas con BITIO en la familia MCF5441X

    Hola a todos!   Estoy teniendo problemas con la familia de microcontroladores MCF5441X con algunas librerias del processor expert.  Los componentes de alto nivel (BITIO, TIMERs, etc...) aparece un error ll...
    Juan Luis Lopez
    last modified by Juan Luis Lopez
  • Which MCU board to choose for in built ethernet and uart?

    Please forgive my neglicence. In my project,I want to accomodate ethernet port as well as an Uart port. Also I want connections for a parallel port also. When I was searching,  I have come across the DNP series b...
  • MCF5271 IBIS model?

    Hi!   I'm looking for an IBIS model for the MCF5271 microprocessor.  The website currently just has the BSDL files.  Anyone have one or know where I could get it?   Thank you! Geoffrey
    Geoffrey Burnham
    last modified by Geoffrey Burnham
  • Merge Bootloader with Application

    Hello everybody!   I have an application to wich I'd like to add bootloader capability. I'm working with CW v6.1 and MCF51QE128. I took the QE bootloader developed by Pual Zhang for the DEMO QE board, did some m...
    sebasira
    last modified by sebasira
  • MCF54415CMJ250 BSDL File

    Hi everyone, I'm looking for BSDL file for MCF54415CMJ250 ColdFire Microcontroller. Does anybody can help me?   Greetings!
    Aurelio Siordia
    last modified by Aurelio Siordia
  • AppTRK.elf file missing in MCF5282 pre installed Ulinux

    Hi, I am working on DNP/EVA6(REV 1.2 board) with coldfire MCF5282CVM66. When I read the documentation, it was mentioned that I have to start the AppTRK agent(Apptrk.elf) to have a communication between the evaluation...
  • BITIO with MCF5441X

    Hello everyone!   I'm having problems with the MCF5441X family of microcontrollers with some Processor expert libraries. The high level components (BITIO, TIMERs, etc...) get an error called: "This component is...
    Juan Luis Lopez
    last modified by Juan Luis Lopez
  • Help ID board With MCF5213 processor.

    I have a box of these boards in my stock and cannot figure out if I need them or not, seriously can't find anything on them through my normal database.  I know it's a long shot but was wondering if anyone here ca...
    Matthew Petro
    last modified by Matthew Petro
  • flexCAN message buffer on MCF548x

    Hi all,   I have a question about flexCAN message buffer on MCF548x. flexCAN has 16 MBs for Tx and Rx.   I set 14 MBs(MB#0 ~MB#13) for Rx and 2MBs for Tx. And, I set same ID(i.e. 0x4AA) to MB#2 and ...
    CK Kim
    last modified by CK Kim
  • MCF5485 Flexbus lines level at start up?

    Hey! I have a question as to what level the Flexbus lines come up as on the MCF5485.   The Table 2-1 of the RM shows FBCS[5:0] and BE come up as high. However, table 17-1 shows they come up as Hi-Z
    Zachary Wilcox
    last modified by Zachary Wilcox
  • DSPI Example Driver for MCF5485

    Hi,   I am looking for some example code for a DMA SPI driver for the MCF5485.    Thanks.
    Prabodh Jhaveri
    last modified by Prabodh Jhaveri
  • LS1021ATSN-PA

    根据教程将sdcard.img编程到sd卡中之后,我将sd卡插入板中,加电,然后使用pc将其连接到板中。我发现我的PC无法识别串行端口。
    junbin liu
    last modified by junbin liu
  • mcf5441x, esdhc, BLKATTR question

    Hi all,   working on a Linux driver for this module,   on CMD 18 (and other), from the upper layer, i am getting a value of 0x1200 (4608) for block size (BLKSZE field). As a bit-width, this value can be a...
    Angelo Dureghello
    last modified by Angelo Dureghello
  • Difference between MC68376BGMFT20 and MC68376BGMAB20

    Hi everybody,   I'm looking for the difference between these two µprocessors : - MC68376BGMFT20 and MC68376BGMAB20   I've found some informations in this file : https://www.nxp.com/files-s...
    FABRICE PEDEN
    last modified by FABRICE PEDEN