• DAP in TWR-LS1021

    How can I use dap in TWR-LS1021 board ?there are two question abou it: 1.How about the firmware for DAP in TWR-LS1021 board,Can I use the standard firmware for the CMSIS DAP ? 2. As I know. the ccs application in Co...
    nine sun
    last modified by nine sun
  • CodeWarrior USB Tap in LS1028ARDB: target connection error

    I'm using a LS1028ARDB set as LS1027AE (by DIP switches) and I tried to access the Flash Programmer with the CodeWarrior (CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA) to program the eMMC integrated...
    Igor Tedeschi Franco
    last modified by Igor Tedeschi Franco
  • Code Warrior Flashing and Bringin-Up Board with On-board eMMC [T1042]

    Hello nxp community   In my custom design [t1042 processor], I have a on-board eMMC connected to SDHC interface. So it means that I can not burn U-boot into mmc card using linux "dd" command.   Can code-wa...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • who know the codewarrior how to know select lcf as ram or flash

    i have two lcf file ,one is ram and other is flash,and i can select ram or flash two mode in codewarrior. but i want to know how the codewarrior know which lcf file was select.because in project setting window, i can...
    zhangbo zhangbo
    last modified by zhangbo zhangbo
  • where can i download QCVS4.5 offline installation package for CW10.5.1 for power pc

    where can i download QCVS4.5 offline installation package for CW10.5.1 for powerpc or for eclipse offline installation package
    lixing gao
    last modified by lixing gao
  • Enable Loopback SerDes Configuration Tool

    Hi!   I am trying to do an external loopback BIST-test in QCVS SerDes Configuration Tool for Lane 0 SerDes3 on a T4240 and get the following error:   BIST-error   TCSR3: 0x a1fff04   When I rea...
    Markus Rosander
    last modified by Markus Rosander
  • U-boot start up from DRAM using Code Warrior

    I want to boot a custom board with T1014, but my boot device is not supported by Code Warrior flash programmer and u-boot cannot be written to the boot device. (MT29F4G SPI NAND Flash is mounted on the custom board.) ...
    hirobe motoharu
    last modified by hirobe motoharu
  • LS1046ARDB: Failed to start flash programming services using Code warrior TAP

    Following error is obtained while trying to initiate flash programming services on LS1046ARDB using code warrior TAP. We tried setting the RESET_REQ_B(SW4[8]) to OFF as suggested in the logs, but it didnt resolve the ...
    Jerin Baby Mathew
    last modified by Jerin Baby Mathew
  • LS1021A QCVS RCW配置冲突问题

    Hi, all     请教一个LS1021A RCW配置的问题,我们板子配置成从qSPI启动的。      使用QCVS来生成RCW时发现配置,如果CPU频率配置为1GHz(即C1_PLL_SEL为CGA_PLL1/1),这时下面的qSPI Clock就跟着变为125MHz会报错,提示qSPI接口的最大速率是62.5MHz,因此不允许我生成RCW bin。 感觉QC...
    changbao ma
    last modified by changbao ma
  • There is no  processor menus for choice while create a new Qoriq Configuration Project in CodeWarrior,what's the problem?

    There is no  processor menus for choice while create a new Qoriq Configuration Project in CodeWarrior,what's the problem?    I have Installed Products:  - CodeWarrior for Power Architecture &...
    fly dick
    last modified by fly dick
  • cw debug mode for ls1046a

    hi !     there is one eMMC(MTFC16gapalbh) in my custom  ls1046a board  ,i set rcw source 01001110B . I try to use cw flash tp program uboot to my eMMc. I disable the ddr, use ocram. but I can't re...
    jingjia shi
    last modified by jingjia shi
  • How to disable DRAM initialization in U-Boot?

    I'm working with the T1042 board. By default, DRAM is initialized so that all values read 0xdeadbeef. I want it to instead start up, and have what ever inherent values the DRAM cells happen to be.  Essentially I ...
    Jason Dejesus
    last modified by Jason Dejesus
  • DDR initialization failed

    We are seeing intermittent failures on our pilot run of boards when running the Operational DDR tests in QCVS tool.  Our initial run of prototype boards ran through the same suite of tests but did not have this f...
    Johh Boggs
    last modified by Johh Boggs
  • Question about building a customized u-boot for the t1042d4rdb board?

    I want to make some modifications to uboot for a project I'm working on. But I keep running into errors when trying to build. To test bitbake, I ran a normal bitbake fsl-image-minimal. It worked the first time. So the...
    Jason Dejesus
    last modified by Jason Dejesus
  • LS1046A DDR4 Erratum

    Looking for documents the 3 erratum document as mentioned in the Target Initialization File for CodeWarrior v11.4.3 A008511_Erratum  A009803_Erratum A009942_Erratum
    Cruz Manderico
    last modified by Cruz Manderico
  • Jtag connection issue

    Hello,   In our custom design(with out CPLD), there are two t1024 processor supplied by identical different power supplies.... I am able to connect jtag with corewarrior for one processor but not with other pr...
    gaurav verma
    last modified by gaurav verma
  • LS1021A RCW override problem

    Hi there,   Recently I tried to use CodeWarrior to override RCW on our customized board and got some trouble. We are using a Rev2 LS1021A, and there is only NAND flashes for booting up, the hardware has been ve...
    hwei
    last modified by hwei
  • Maximum trace length for JTAG lines

    Hello,   In our T1024 based custom design, there are two T1024 processor..... we are able to connect with one T1024 through JTAG but not with other.....   We have checked all JTAG lines, power supply etc f...
    gaurav verma
    last modified by gaurav verma
  • flashing algorithm for S29GL01Gs series

    hi i am trying to erase this flash S29GL01GS10TFI010 i am getting sector protection error when i create targeted task it is only having S29GL01GP series flash by default can i use this part for flashing the S29GL01G...
    agxin j
    last modified by agxin j
  • T1040 Development Environment

    Which is the best version of codewarrior to develop a bare application on QorIq T1040 processors ? Best Regards
    renato Sala
    last modified by renato Sala