• Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured

    Hello community   With using latest Code Warrior, I am trying to flash a new RCW and U-boot into T1042 based new custom board. When I set chipselects to bring up board with hardcoded-rcw, and when I try to flash...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • mingw32-make: ../../full_project_build/makefile_full_project: No such file or directory

    I have issue on compiling project . There is no problem compiling on other computer ,same project ,same builder setting ,same IDE version V11.1 . But when I compile it ,it failed .  what shows in console as belo...
    Alondra Ou
    last modified by Alondra Ou
  • Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this

    Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this
    Dharani devi Manickam
    last modified by Dharani devi Manickam
  • kit9z1j638evm problem

    I have a kit9z1j638evm board. I can't download demo program with usbddm all the time. The prompt is BDM command ack missing. KIT9Z1.J638EVMKIT9Z1J638EVM
    H YW
    last modified by H YW
  • I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

    I read AN4338 but there is no attachment with AN4338SW.zip needed to update usb tap driver for Win 7.
    Robert Patton
    last modified by Robert Patton
  • How to refer to external C functions of CW Project A from CW project B

    Hi All,  I am new to Freescale Codewarrior and so far have been able (after some hassle with asm to c and vice versa compatibility issues) to compile and run dBUG for an SenTec MCF5475 board using version CodeWa...
    Timo Schuering
    last modified by Timo Schuering
  • code warrior 11.1 with multi-link breakpoint won't go further.

    Hi. I have a codewarrior 11.1 version and a multi-link universal to debug S12Z core microcontroller. when I use break function with setting breakpoint at some line, it stops at that line. however it doesn't go f...
    SIHUN LEE
    last modified by SIHUN LEE
  • Ramdisk Deployment from Flash error

     Hi:    I get a new t2080rdb board which is made by our company.Follow the steps in the manual,I boot it from tftp,is ok. But when I use the same images boot from nor flash same wrong happen. I dont n...
    leon liu
    last modified by leon liu
  • ARM Flash Programmer Task

    Sir: Use LS1020 and  Codewarrior V11.4.4  on WIN10. But can not add flash in ARM Flash Programmer Task in attached, due to not connect the EVK board? Also try to use OCRAM,but still in Grey which can not ...
    George Li
    last modified by George Li
  • Code size limitation error-Codewarrior IDE

    Hi, We have Code warrior IDE ver 5.1 installed on our machine and observed "Code size limitation error 1856>512 bytes" error while compiling the code. We then upgraded SW to CW ver 5.2 and still observed the erro...
    Astha Ganjoo
    last modified by Astha Ganjoo
  • CodeWarrior v12.5 crashes on Windows 10

    CodeWarrior 12v5.1 crashes on Windows 10 upon exit with the following error:     CodeWarrior 12v5.2 does not crash on Windows 10 upon exit, but it does not support the HC9S12G48. Can you fix 12v5.1 ?...
    Larry Leviton
    last modified by Larry Leviton
  • RAM Overlap err,how to use  m_data (RW) ?

    Real RAM size of my project  is  over 60k,so the errors happens as follows. The MEMORY of S32K146  contains two blocks:SRAM_L and SRAM_U, now SRAM_U is used and  overload,but other block...
    z z
    last modified by z z
  • Proper Autosar Development with tresos and CW for S12X

    Hi,    I'm trying to develop my first Autosar project, using S12X microcontroller, but I would need some clearence on the step-to-step order.   I have downloaded from NXP website the AUTOSAR3.0 MCAL a...
    Eduard Badia
    last modified by Eduard Badia
  • S32 Studio:stack VMA [2000e800,2000efff] overlaps section .bss VMA

    How  to  solve this problem? tack VMA [2000e800,2000efff] overlaps section .bss VMA  
    z z
    last modified by z z
  • Can trigger a HC12 debug cmd from C code?

    Hi, We are developing motor control project using CodeWorrior IDE based on  mc9s12vr64  chip.  Can we trigger a HC12 Debugger command running from C source code? e.g. If running a command “ fprin...
    He Wei
    last modified by He Wei
  • Core is in unknown mode

    I am using CodeWarrior Development Studio for VSPA3. When I hit debug, it took a quite while in connecting and launching.   At last, it ended with the following error message: "Failed to resume target...
    Hsien Wen Chang
    last modified by Hsien Wen Chang
  • How to read/write MPC/SPC5602 ?

    what tool and software are read/write bin file to MPC/SPC 5602 ? Please advise me,
    Aphichart Hongthong
    last modified by Aphichart Hongthong
  • Codewarrior debugger to simulate ADC

    I need to use the visulaisation tool to simulate ADC in Codewarrior v5.1 . Please help. I do not have the trainer board.
    Suma Rao
    last modified by Suma Rao
  • Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2

    Hello,   We bought the parts of MC33660BEFR2 from Future, but there are different markings on the parts in one full reel.  The markings are...
    Gloria Chen
    last modified by Gloria Chen
  • Ld error: - ccalloc would have returned NULL

    Ld error: - ccalloc would have returned NULL What is the reason for this err?  
    z z
    last modified by z z