• Update for 9S12XF512?

    I have loaded CodeWarrior Classic for S12X V5.2 which is the version to use for the #9S12XF512. However, the software does not include the ability to create a project for the 9S12XF512 nor does it have the required f...
    Dermot Murphy
    last modified by Dermot Murphy
  • Metrowerks Codewarrior sur Windows 10

    Je travaillais pas le passé sur METROWERKS Codewarrior IDE (sous windows XP) pour développer des solutions sur FREESCALE (MOTOROLA) HC912D60A.   Je dois retravailler sur un ancien soft, mais dispos...
    Guillaume FANJAS
    last modified by Guillaume FANJAS
  • How to install CW_MCU_11_1_Update2_200211

    Hi,   I have download CodeWarrier v11.1 and update2. Codewarrier is installed already. How to install Update2 ?     Best Regards, Aaron
    Aaron Lee
    last modified by Aaron Lee
  • Mc9s12zvmc64 bootloader to application jump instructions

    Hi , I am currently developing CAN boot loader for micro mc9s12zvmc64 . I am not able to find bootloader to application jump instructions as well as reset instructions.
    jafarsadak peeruzada
    last modified by jafarsadak peeruzada
  • The debugging problem of freescale ZVL microcontroller in codewarror10.7

    Dear friend, Who can help me with the problem? Can freescale ZVL load ABS files or ELF files for debugging in codewarror10.7 compil? With best wishes! Lei  
    Jackie lei
    last modified by Jackie lei
  • How to change editor theme in CodeWarrior for ETPU?

    Hi, I want to change CodeWarrior for ETPU editor theme to dark theme. How can I do that? Regards,
    Turgay Kale
    last modified by Turgay Kale
  • I've set the boot location to 0x10000, but why does codewarrior still erase 0-0xFFFF when I debug with codewarrior?

    I've set the boot location to 0x10000, but why does codewarrior still erase 0-0xFFFF when I debug with codewarrior.How do I set up not to erase Flash's 0-0xffff because I put the Bootloader there.
    nnsspp ni
    last modified by nnsspp ni
  • mpc8640d supported jtag and tool for Debug

    Hi, we want to know supported Jtag for Mpc8640d and tool to Debug the Processor. i will be helpful if jtag Configuration(pins) also shared means.
    srikanth ravada
    last modified by srikanth ravada
  • MWCT1013 on WCT-15W1CFFPD

    Hi, I am trying to use CodeWarrior USB TAP with ONCE communication. FreeMASTER does not see any device. CodeWarrior IDE version 11.1 update 1 doesn't see the device. The TAP came with no documentation or downloads. Wh...
    wpsigma
    last modified by wpsigma
  • Codewarrior V4.7 can no longer load cpu beans

    Suddenly after a long period of perfect operation Codewarrior fails to read the cpu bean from the project file(s). This happened today, the first day after the holidays. I get the same problem on ”other”...
    Anders Johansson
    last modified by Anders Johansson
  • LIN Stack Problem with Processor Expert Mode

    I am facing issue while using LIN stack with processor expert mode.   If directly added LIN stack then getting issue ISR redefined.   If I allow macro redefinition   then not able to flash the pro...
    Chaitanya Kalyani
    last modified by Chaitanya Kalyani
  • JTAG chain issue

    Hi,         I`m using code warrior USB Tap and when i`m tring to program a device i get the error `` The JTAG chain does not contain any debuggable cores!``. Can you help me to understand wha...
    Daniel Terebent
    last modified by Daniel Terebent
  • How to change color theme tp dark in CodeWarrior

    I need to change color theme in CodeWarrior like VisualStudio2017 has. Is any way do it?
    Marceli Firlej
    last modified by Marceli Firlej
  • HRESET occured during transactio

    Hello NXP,    We have a custom board based on T1042 processor. We want to flash new RCW on NOR flash using Code Warrior. We can not use hard coded rcw some attributes differ from RDB.   I had 'HRESET ...
    Ahmet Demir
    last modified by Ahmet Demir
  • Real-Time OS

    Hello, I am not familiar with NXP Processors so please forgive my simple question. I have been using ARM+DSP processors from TI. Most of their processors have many high-speed communication links such as SRIO, 10G-Ethe...
    Joe Lindula
    last modified by Joe Lindula
  • RCW Override, Error:  Connect Failed. Failed to correctly configure the JTAG chain(CCSProtocolPlugin) Error: Connect Failed.

    Hello NXP, Board: T1042 D4 RDB - 64 b Problem: Unable to execute RCW override script ( <CWInstallDir>\PA\PA_Support\Initialization_Files\jtag_chains ) with NOR flash Target Task.   I want to flash s...
    Ahmet Demir
    last modified by Ahmet Demir
  • What would it take to add MPC8xx devises into CodeWarrior Development Suites for Networked Applications v11.4.0?

    I need to work on an older device that uses MPC8xx devices.  The website recommends CodeWarrior Development Suites for Networked Applications v11.4.0 as the software but after installation I found the MPC8xx...
    Jason Maurey
    last modified by Jason Maurey
  • [CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error after flashing wrong RCW/wrong Place. T1042D4RDB-64B.

    Hello NXP,   With using QCSV and T1042D4RDB - 64B, I accidentally flashed a new RCW into wrong(I guess) place in NOR flash (in both BANK 0 and BANK 4). Now the board is not booting and ASLEEP ping is always lit...
    Ahmet Demir
    last modified by Ahmet Demir
  • Code Warrior Burning new U-boot Execute command is not enabled

    Hi NXP,   I am trying to burn new U-boot on T1042 D4 RDB as described in QorIQ SDK V2.0 - 1703 (Chapter 5) using Code Warrior for T1042. It's the latest Code Warrior Development Studio. I created a sample BareBo...
    Ahmet Demir
    last modified by Ahmet Demir
  • Error : FETFSL1' is an instance of an undefined model

    I have downloaded "AFT27S010N RF high-power Model ADS Product Model Design Kit" and "RF High Power Model Kit 2020", but I do not know how to import the Model.
    ming xu
    last modified by ming xu