• Build error in CW11.1

    Hi,   We are using CW11.1 IDE and MQX 4.2 RTOS for our development of Kinetis K60 controller based hardware. Below file throws error when we trying to build K60 project in CW 11.1 C:\Freescale\CW MCU v11.1\MC...
    ANAND S
    last modified by ANAND S
  • No source available for "0xFFFFFFFE (0xFFFFFFFE)() " in a Custom KL25Z QFN32 board

    I'm using CodeWarrior IDE for programing a FRDM-KL25Z and everything is ok when i'm trying to debug the code, but i have develop an custom board with the MKL25Z128VFM4 that is a QFN32 version of the kl25z of the FRDM ...
    FERNANDO MADERA
    last modified by FERNANDO MADERA
  • Memory locations being incorrectly written to?

    I am reluctant to think this problem is with my processor, so I'm posting here under the assumption that it is perhaps a setting I am uninformed of when it comes to my dev environment / debugger.   I am writing ...
    Richard Howell
    last modified by Richard Howell
  • Generate ATD interrupt for HCS12 controller

    Hello, I am working on MC9S12XEP100 microcontroller , and as I am new to this I am able to the polling base example but I want to generate interrupts for multiple channels in scan mode. I want to generate interrupt ...
    Utkarsh Ghadge
    last modified by Utkarsh Ghadge
  • How to use P2020's interrupts in CodeWarriorV10.5?

    Thanks!
    nnsspp ni
    last modified by nnsspp ni
  • NXP Library Not working with some android devices.

    I developed an android application for write and read data to a Mifare desfire ev1 card using nxp-nfc-library-1.7(latest version). That application worked properly with the device which I used for develop the  ap...
    Lakshitha Gayashan
    last modified by Lakshitha Gayashan
  • java.lang.IllegalArgumentException

    Hello community,   I can not display SerDes1:SerDes which is created with default Code Warrior QCVS SerDes Configuration Tool. Can anyone tell me how to fix this error ? Is there any patch recommended to apply ...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • Freescale CodeWarrior Product List Add

    Hello   I am using the S9S12GNA16F0MLF model and I am using Freescale CodeWarrior 5.9.0 version.   I tried to select MC9S12GNA16F0MLF as the picture below, but I can't use it because it is not in the list....
    Seok Kim
    last modified by Seok Kim
  • Code warrior does not recognize global structure variable

    Hi,   I'm using code warrior IDE version 5.9.0 for MPC55xx/56xx.  According to my preference setting, the global variables should be purple.  I declared the struct variable such as ,    /...
    jaehak kim
    last modified by jaehak kim
  • MC56F8355MFGE

    Hello,   I use the MC56F8355MFGE DSP. I program it with the 56800E Flash Programmer. A DSP with 1628 datecode is ok after programming. A DSP with 1843 datecode doesn't start after programming. The checksum fo...
    CHRISTOPHE CHEVE
    last modified by CHRISTOPHE CHEVE
  • Questions about Code Warrior RCW Override (using T1042)

    Hello Community,   I have few questions about Code Warrior PA RCW Override Method.   1-) When I select Target Type as "T1042", does it means Code Warrior Tab is not going to bring up the board with the RCW...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • Updating gcc in CodeWarrior?

    Hi, We're using "CodeWarrior for Power Architecture Version: 10.5.2 Build Id:160624", which came with gcc 4.9.2. Specifically we're using "C:\Freescale\CW_PA_v10.5.1\Cross_Tools\gcc-4.9.2-XMe6500-linux". Our linux ...
    David Sclarsky
    last modified by David Sclarsky
  • How to refer to external C functions of CW Project A from CW project B

    Hi All,  I am new to Freescale Codewarrior and so far have been able (after some hassle with asm to c and vice versa compatibility issues) to compile and run dBUG for an SenTec MCF5475 board using version CodeWa...
    Timo Schuering
    last modified by Timo Schuering
  • Debugging U-boot T1042

    Hello community, using T1042RDB, I am trying to debug my own u-boot ( sdk compiled ) with Code warrior to learn how it works.    I have a custom board and I want to debug my customized u-boot on it later. &...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • Error -1073741811

    Have installed code warrior 11.1, update 1 and 2. after compiling the project have Error -1073741811. i am using windows10. **** Clean-only build of configuration FLASH_SDM for project sin20200 **** Build complete ...
    tony tony
    last modified by tony tony
  • Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured

    Hello community   With using latest Code Warrior, I am trying to flash a new RCW and U-boot into T1042 based new custom board. When I set chipselects to bring up board with hardcoded-rcw, and when I try to flash...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • mingw32-make: ../../full_project_build/makefile_full_project: No such file or directory

    I have issue on compiling project . There is no problem compiling on other computer ,same project ,same builder setting ,same IDE version V11.1 . But when I compile it ,it failed .  what shows in console as belo...
    Alondra Ou
    last modified by Alondra Ou
  • Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this

    Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this
    Dharani devi Manickam
    last modified by Dharani devi Manickam
  • I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

    I read AN4338 but there is no attachment with AN4338SW.zip needed to update usb tap driver for Win 7.
    Robert Patton
    last modified by Robert Patton
  • Ramdisk Deployment from Flash error

     Hi:    I get a new t2080rdb board which is made by our company.Follow the steps in the manual,I boot it from tftp,is ok. But when I use the same images boot from nor flash same wrong happen. I dont n...
    leon liu
    last modified by leon liu