• How to modify the generated code?

    I try to output a PWM signal from S9KEAZN8AMFK chip and I use Processor Expert to generate the code I want.  I set the initial conditions in the component properties tab below (which results in a 50% ratio ...
    Zhouming Wu
    last modified by Zhouming Wu
  • Repeater

    Hello,   I'm using a MKW24D Board and the SMAC communication protocol. I would like to know if NXP provides a Repeater application for this board and protocol. I'm looking for a application that  repeats al...
    Vítor Caitité
    last modified by Vítor Caitité
  • Communication range

    Hello,   I would like an indication of an nxp board that accepts the SMAC communication protocol and has a long communication range.   Thanks.
    Vítor Caitité
    last modified by Vítor Caitité
  • function that returns the time since nxp kw24d was turned on

    Hello,    I'm using a nxp kw24d board and I want to know if exists a function that returns the time since this board was turned on. I want a function similar of millis() in Arduino.   Thanks! Ví...
    Vítor Caitité
    last modified by Vítor Caitité
  • MKW24D board transmitter

    Hello.   I would like to know the approximate range (in meters) of the nxp MKW24D board transmitter. I would also like an indication of an external PA compatible with this board.   Thanks
    Vítor Caitité
    last modified by Vítor Caitité
  • Codewarrior problem for help

    When I open the codewarriror v11.1,there is an error window popping up,and the above shows ‘Microsoft Visual C++ Runtime Library’,when I click the OK button,the program crashed directly.
    liangxue 薛
    last modified by liangxue 薛
  • How to print in the IAR I/O terminal?

    Hi,    I want to know how to print in the I/O terminal of IAR workbench? My device board is a kw24d. When I use printf(), it doesn't' prints nothing in this terminal. My debugger driver is is in the PE mic...
    Vítor Caitité
    last modified by Vítor Caitité
  • How to remove c++ compiler in project

    Hello. Support team.   I want to use only C compiler without C++ compiler such as A Case. How to remove C++ compiler in 'B case' ??   A case B case C Compiler C Compiler + C++ Compiler  ...
    MinYeop Na
    last modified by MinYeop Na
  • help !!!I can't unsecure the 9S12GN32

    hello everyone! I have a problem, in codewarrior, i want to unsecure the s9S12GN32  0N48A and erase all blcok, but the flash is unchanged, and the content is the same as the original, what is the problem? ...
    Liu haifeng
    last modified by Liu haifeng
  • Unable to access PCIe registers

    I am unable to access the PCIe registers using Code Warrior.#PCIe registers
    Sahana Chandrasekar
    last modified by Sahana Chandrasekar
  • error: LS1020A: Core not responding while bringing up custom board .

    Hi All I have custom board with LS1020A . I am trying to bring it up for the first time . I am using code warrier tap (USB) . I got following error (logged in code warrier server )     check_min_version(ser...
    Dhruvalkumar Patel
    last modified by Dhruvalkumar Patel
  • Package to start learning functional safety MCU

    Good day dear all, I am new to MCU units and would like to learn how to implement ISO 26262 ASIL A/B functions in the future. So as a start, I want to build a prototype that demonstrate EPB safety function, say the ...
    Lu Zheng
    last modified by Lu Zheng
  • Illegal constant expression: copying address to a variable

    I try to compile the below mentioned code in Code-warrior 10.7 but CW throws an error "illegal constant expression"   Code:   uint32_t val1; uint32_t val2; uint32_t val2 = (uint32_t)&val2;  &...
    Amit Dhand
    last modified by Amit Dhand
  • How i can write to a bit field in IDE CWide eTPU?

    Hi, i'm using CWide or codewarrior for eTPU and when i create for example a struct:   typedef union {    struct    {       uint32_t B0:1; ...
    Demian Espina
    last modified by Demian Espina
  • enable floating point

    I have port CodeWarrior 5.1 project to CodeWarrior 10.6 and I forgot to enable floating point so I am getting the following error   ERROR L1822: Symbol _FUFLOAT in file   Is there way to change project set...
    Ronen Aharoni
    last modified by Ronen Aharoni
  • CodeWarrior v5.2 Created Watchdog Code

    Hi, I am working on converting a cosmic compiled code into a codewarrior compiled code. I've worked on changing all the pwm global names over to what codewarrior calls them. My code compiles but the log2phy generated ...
    Matthew Gardner
    last modified by Matthew Gardner
  • Exclamation marks in Device manager, Failure message in CodeWarrior

    Hi ! I connected an S9S12GA128 uC to the Multilink Universal FX debugger and installed a CodeWarrior CWS12v5.2 on my W10 Op.Sys in order to flash it. The PC has not recognized the debugger appropriate because in the d...
    László Török
    last modified by László Török
  • CodeWarrior License Server migration to Windows 10: Floating license doesn't work

    After Migrating to windows 10 floating license is not working in client machines.   I was using code warrior floating license in windows 7. After migrating to windows 10 license is not working in client machines...
    sanjay gangadharan
    last modified by sanjay gangadharan
  • How to build a CodeWarrior v6.3 Project in command line?

    MCU: MC9S08QE4   Refer to this documentation, I try to build an old Code Warrior V6.3 Project (.mcp) via command line.   PS C:\Program Files (x86)\Freescale\CodeWarrior for Microcontrollers V6.3\b...
    Pascal Schröer
    last modified by Pascal Schröer
  • question about workspace location

    I move the workspace to a new location, but I can't open it after that. It prompt that Invalid workspace in use. It seems that behave is forbidden. How to move workspace to a new location and can work properly? ...
    Mike Young
    last modified by Mike Young