• How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method)

    The Good and the Bad about CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2 Removed more than half of the supported chips for "market reasons" (see table below) Updated P&E drive...
    Rodney McGee
    last modified by Rodney McGee
  • How-to Directly Install CodeWarrior 6.3 Classic in Windows 10 or 7 x64 (Unofficial Method)

    CodeWarrior 6.3 is for most RS08, S08, ColdFire V1 Processors* *Not compatibile with (S08: RN, RNA, PA, PT, Kinetis (including Tower), ColdFire V2 ...)   This post describes installing CodeWarrior for Microcont...
    Rodney McGee
    last modified by Rodney McGee
  • MC9S12XDP512 Programming Failure

    Greetings, I'm having trouble programming several MC9S12XDP512 devices. I've seen a couple older posts with related information in the command window of the Hiwave debugger but haven't seen an actual root cause or re...
    Nicholas Schneck
    last modified by Nicholas Schneck
  • Simply program HCS08

    Hello,   here is my problem : I use CW6.3 for MCU and USB Multilink interface (PE Micro) with HCS08 microcontroler. When i want to program the HCS08 on my board i use HiWave (included in CW6.3) or i progr...
    CAPOSIENA Philippe
    last modified by CAPOSIENA Philippe
  • CW USB TAP: Driver for Windows 10 64-bit System

    I have installed on my "new" laptop the 56800E Flash Programmer but I get the error "USB open failure" when I try to program the DSP.  The USB TAP device worked the last time I used it, albeit some years ago on a...
    Evan Espina
    last modified by Evan Espina
  • Text file

    Hello; when I include,fstream and  iostream, debugger gave me error C5200. Sb
    +Sandra Gogaa
    last modified by +Sandra Gogaa
  • Checking Memory Usage for MC56F3XX

    Hi, I am using the MC56F346 device and the sdm pROM-xRAM target. How can I check my memory usage? I think I am unable to compile my code because I have ran out of ROM memory but need to confirm this.... All and any ...
    Stephan Fortune
    last modified by Stephan Fortune
  • USB TAP error: "CCS Libary Not Found"

    Hi,   I am using Codewarrior v8.3 and is connected via USB TAP to my MC56F8245 chip. Due to the design of the board (mini JTAG header), I am using a custom connector which only uses the pins: TDI, TDO, TCK, TMS...
    Xiang Chen
    last modified by Xiang Chen
  • MC56F82 beans or PE

    I have done one MQX project based on the examples included with MQX. I have been asked to add a SPI interface to a MC56F825X project. Doing a quick look around the forums I found more references to using PE beans then...
    DALE RODDA
    last modified by DALE RODDA
  • CW 10.2 for 56F8366

    I've been using CW 10.2 for the DSC 56F8366 There are many frustrating things wrong, but the 2 big ones are these: Everytime I need to download/debug, I must kill the process DE.exe using task manager otherwise I ge...
    Tim Robbins
    last modified by Tim Robbins
  • CW DSP 8.3 vs Eclipse 10.2

    I have taken over a project that is using Codewarrior 8.3 on the DSP568006.   We are investigating the benefits of switching to the new Eclipse 10.2 tool.  The 8.3 tools have some major issues, but they...
    Bryan Olinger
    last modified by Bryan Olinger
  • 56F8037 CAN TX problems

    Hi there,   I am having a bit of trouble with the MSCAN module in the 56F8037. In particular, I am currently trying to get it to transmit data. I have this sort of working, in that I can transmit data ok at va...
    Laurence McLean
    last modified by Laurence McLean
  • About MSCAN module on 56F82xx

    Hi all,   I just wonder why sequential MSCAN registers increments  by one in the memory space. Since these DSCs are 16 bit, a register should occupy two bytes in memory.  I investigated both the datas...
    HUSEYIN DEMIR
    last modified by HUSEYIN DEMIR
  • DebuggingProblem cannot step out from here

    i use CW8.3 & PE to develop programs on mc56f8366 ,and i have a problem___In debug mode, my program will jump to stack and can't jump out(as the attachment),and the chip haven't do the operation i coded...Need Hel...
    Cloud Ye
    last modified by Cloud Ye
  • CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP

    Hi all,    I've just installed CodeWarrior for Microcontrollers v10.2 which integrates the development tools for the DSC's.  I've created a simple project just to debug it using USB TAP. Pr...
    Miskha
    last modified by Miskha
  • MC56F825x, Codewarrior 8.3 and Quadrature Decoders

    Hello All,   I am using a 56F8257 and developing using Codewarrior DSC56800E 8.3 with Processor Expert.  I have the Professional license and have successfully developed a number of products with this envir...
    Dave Miller
    last modified by Dave Miller
  • MC56F8037 in-circuit debug interfaces problems

    Hi all,   I'm starting developing fw for MC56F8037 DSC, I downloaded CW 8.3SE and as a programming/debugging interface I can choose from Codewarrior USB TAP and PEmicro USB Universal Multilink, but none of...
    Alan Pastorelli
    last modified by Alan Pastorelli
  • Flash erase works in debug mode, fails in standalone

    DSP 568037 My application is designed to read and write configuration data into internal flash. It unlocks global protection, erases the desired sectors, then writes. The space reserved for that is from 0x7700 to 7AF...
    Giovanni Montefiori
    last modified by Giovanni Montefiori
  • Boot load settings in cmd file - problem with xBootCfg

    Hi   in the document Serial Bootloader for 56F82xx it says to add the following in the cmd file of the application firmware side.    .xBootCfg(RWX)RIGIN = 0x00007BFE,LENGTH = 0x2 .Application...
    Eli Arad
    last modified by Eli Arad
  • case sensitive for a few folder name if project located on network dirver

    codewarrior is DSC56800 R8.1, project name scf_sec, all folder name and file name is lowecase. we use clearcase for code control, it works OK. But now we migrate from clearcase to SVN, so development enviorment chang...
    connie ran
    last modified by connie ran