• Can this "rare" chinese made USBDM forced to accept the OSBDM firmware?

    Hello people.   I have a chinese made USBDM which I got quite cheap from some widely known chinese imports site. I live in Spain, Europe.   This USBDM's hardware includes actually a 6-pin (2x3) header in t...
    msalmeronc@yahoo.es
    last modified by msalmeronc@yahoo.es
  • USBDM with LPC1111 LPC111x

    Hi PGO,   I try to identify and program the LPC1111 with no success. It is an ARM cortex-M0 with SWD. Why it cannot answer the "detect chip" ? Do you have some TCL command that I can do to check if this chip w...
    Luciano Nicolau
    last modified by Luciano Nicolau
  • 厦门有没有NXP技术支持

    你好,厦门有没有NXP技术支持。联系电话时多少?
    5923002@qq.com
    last modified by 5923002@qq.com
  • USBDM MCUXpresso

    Are there any plans to support the new mcuxpresso_ide in usbdm or does it already support it?   I am currently thinking about setting up a system to test the new IDE but currently use a USBDM based deb...
    Ian Bentall
    last modified by Ian Bentall
  • USBDM x MCUXpresso V11

    pgo gove to me one tip at 2017 that was very helpful. It is https://community.nxp.com/thread/448562#comment-900552  But now I am thread over this issue again using MCUXpresso version 11.0.1_2563 installed at C...
    RICARDO TREVISAN
    last modified by RICARDO TREVISAN
  • USBDM CF 3.1 UsbdmScript TCL Interpreter commands

    Hello PGO, I've got some PCB's done with your USBDM_CF_3.1, assembled, intended for HCS08 programming and debugging, and it is now replacing an old P&E micro USB Multilink 12E cable. Picture attached. Works fine w...
    ROBERTO BERNER
    last modified by ROBERTO BERNER
  • Run USBDM applications in console mode

    pgo   Hello pgo,   I have a task where I need to use the USBDM applications, specifically FirmwareChanger and JS16_Bootloader in console mode. Unfortunately, I discovered that these applications do not sup...
    Chibueze Cyril Akaluka
    last modified by Chibueze Cyril Akaluka
  • command line

    no feedback when using command line "UsbdmFlashProgrammer.exe -requiredBdm=USBDM-JS16-SWD_SER-0001 -target=s12z FCA_WL_SBMD_A_02_01.sx -device=MC9S12ZVL32 -erase=mass -program -verify -secure"   but from ht...
    gable zhang
    last modified by gable zhang
  • USBDM MKE16Z64VLF4 XML file

    ARM Programmer Does Not Detect MKE16Z64 I made a big project (5000 pieces month) and asked to buy a usbdm to record the MKE16Z64VLF4, but I had the surprise that this micro is not in the list. What to do? Would it be...
    Marcel Giraldi
    last modified by Marcel Giraldi
  • I have a problem.The mc9s12xet256mal16 bit product appears to be connected, but it does not connect to the codewarrior program.I don't understand where i made a mistake.

    yusuf yildiz
    last modified by yusuf yildiz
  • USBDM and HCS12 9S12D64, read/write problems

    HI!   I would like to ask for help as i'm a bit desperated. I will try to be as clear and short as possible.   My task is to upgrade a 9S12D64 with a newer version of software (no matter about what). My fi...
    potros potros
    last modified by potros potros
  • BDM

    我新安装的CW 10.7,安装了BDM驱动,在设备管理中能识别到BDM,但是在CW10.7中就找不到。我是不是缺少什么驱动?
    永明 张
    last modified by 永明 张
  • How to make MCUXpresso support USBDM?

    Hi pgo, USBDM is very good to work. Now, I want to debug program through MCUXpresso and USBDM. but I'm first to do this. my USBDM version is 4.12.1. How to do it ? do you have document to illustrate it ?   than...
    baode wang
    created by baode wang
  • USBDM 4.12.1 can't support codewarrior?

    Hi pgo, I'm using MKE02 based on codewarrior. I update usbdm  veresion  to usbdm 4.12.1.But  i can't find patch in usbdm folder.And usbdm can't be support by codewarrior. How can i do it?   thank...
    baode wang
    last modified by baode wang
  • USBDM driver for win10

    I can connect the USBDM with Codewarrior v5.1 in Win7. But now the USBDM cannot be detected in Win10 system. Should I have a USBDM driver for Win10?
    Henry Wu
    last modified by Henry Wu
  • How to read flash and EEPROM with USBDM from HCS08?

    Hello,   my Name is Chris from Germany and I'm new at freescale µC, so pleace be patient.   My goal is to read eeprom and flash of a MC9S08AW48 and MC9S08AC48. EEPROM is definetly not fused, because...
    Christian Scha
    last modified by Christian Scha
  • Requirements for minimal installation under Linux

    Hello,   I was able to successfully install the Debian package under Linux and run UsbdmScript / UsdbmFlashProgramer.   Now I want to install it on a system without a window server / GUI. Is this possible?...
    Sven Hensel
    last modified by Sven Hensel
  • HCS08 TCL Script - Flash not blank (and still secured)

    Hello,   I wanted to flash the HCS08 (LL-MC9S08LL16) under Linux (Raspbian running on Raspberry Pi 3 B+) with the USBDM-JS16-0001. This works with the UsbdmFlashProgrammer when called as GUI program, and also v...
    Sven Hensel
    last modified by Sven Hensel
  • HCS12 PROGRAMMER failed to read s-File

    I'M using USBDM 4.12.1.240. My MCU is MC9SG128. I want to use HCS12 programmer to programme my mcu, but when load hex file, it tells me "Failed to read S-File". But when I load S19 files in "USBDM 4.12.1.240\Device...
    WEI LI
    last modified by WEI LI
  • Programming of the target flash failed! Reason: Execution of TCL script returned an error!

    I was using USBDM to program MC9S12G128,the error is as follows: Programming of the target flash failed! Reason: Execution of TCL script returned an error!
    Alonso Alonso
    last modified by Alonso Alonso