• Info - USBDM available on MyFreescaleWebPage

    Hello all,   Several people asked for it, the USBDM we have created is available back on MyFreescaleWebPage!   Based on "USBDM_SWD_JS16CWJ" schematic from PGO, it is compatible with the following families:...
    GUITTET JOEL
    created by GUITTET JOEL
  • Problem with the github repository usbdm-eclipse-makefiles-build

    There are two directories in this repository with the same name but different case - USBDM_DLL and Usbdm_DLL with different commits. I hope this is not intended as it causes problems with checkouts into case-insensiti...
    pint
    last modified by pint
  • USBDM - Version 4.10.6 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.6   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • USBDM - Version 4.10.6.110 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.6.110   Please post any queries on this version to separate threads.   Documentation available at: SourceForge Applications available at: SourceForge S...
    pgo
    last modified by pgo
  • USBDM HCS12_FlashProgrammer

    nice tools pgo,   I've got a special usage where I only need to issue a 'run', wait a couple of sec, then a 'halt' to a HCS12.  it looks like it would be pretty simple to add to the CLI interface of HCS12...
    vette
    last modified by vette
  • USBDM driver meets a question

    Hi pgo, My USBDM information is as follow. hardware:USBDM_SWD_SER_JS16CWJ_V2.0 firmware:USBDM_SWD_SER_JS16CWJ_V4 USBDM version:USBDM4.10.5 I use the BDM in win7-32bit. First , I install the driver USBDM_Drivers_...
    baode wang
    created by baode wang
  • USBDM - Version 4.10.0 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.0   Please post any queries on this version in this thread (maybe!),   Documentation available at: SourceForge Applications available at: SourceForge So...
    pgo
    last modified by pgo
  • USBDM - Version 4.10.4 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.4   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • USBDM - Version 4.10.2 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.2   Please post any queries on this version in a separate thread - I really can't cope with this new-fangled setup!   Documentation available at: SourceF...
    pgo
    last modified by pgo
  • USBDM with Tower  kit

    Hi pgo,   Is it now possible to flash USBDM image (USBDM_TWR_CFV1_V4.sx) into JM60 osbdm ?   regards, Emmanuel
    Nouchi
    last modified by Nouchi
  • USBDM JM60 Hardware

    Does anyone know where one can purchase one of the JM60 hardware (below), already populated and programmed with up-to-date firmware?   http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/USBDM_CF_SER.jpg
    Christopher Kilgour
    last modified by Christopher Kilgour
  • USBDM gerber or altium files?

    Hi I wish to build myself a USBDM but can't find the pcb files to make as gerber or altium to make the pcb fabricated Im looking for the minimal JS16 Version Anyone have it available?
    JulsPower
    last modified by JulsPower
  • MC68HC912D60A (2K38K)---CW5.0 can not connect

    Hello all, Can anyone help me a Thanks   MC68HC912D60A (2K38K)---CW5.0 can not connect     TBDML           HC912D60A 4MHZ------------EXTAL  ...