• Expected BDM command ACK missing with USBDM 4.12 and JMxx firmware

    Hi to all the community.   I have an issue with the USBDM 4.12 and JMxx firmware. The resources i´m using are the following:   *- Board: (USBDM: USBDM RS08/HCS08/HCS12/Coldfire V1,2,3,4/D...) which u...
    martin mignone
    last modified by martin mignone
  • USBDM - Version 4.10.5 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.5   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • USBDM 4.12.200 fails with DSC mass erase

    Hello PGO,   I´d like to inform you that the rev: USBDM_4_12_1_200 fails with DSC erase using "MC56F Programmer" and USBDM_CF_JMxxCLD_V3,  TCL error see the photo attached. I installed...
    Luciano Nicolau
    last modified by Luciano Nicolau
  • Memory Dump for MC56F84550

    Dear PGO, how can I read the flash content of that DSC? I saw that it's in list of MC56F programmer, but not in Memory dump.
    Vasil Kostadinow
    last modified by Vasil Kostadinow
  • How to Check Installation of USBDM in Codewarrior 10

    The process to check the installation of USBDM in Codewarrior 10.x   Assumes the following: Codewarrior 10.6 installed Current version of USBDM installed (from USBDM - Browse /Version 4.12.1/Software at Source...
    pgo
    last modified by pgo
  • USBDM Updated to 4.11.1.20

    Dear All,   USBDM has been updated to version 4.11.1.20.   A video introduction is available at: USBDM with Kinetis Design Studio and Kinetis SDK - YouTube   The software is available at: USBDM | S...
    pgo
    last modified by pgo
  • USBDM Programming Issue

    Hi ,   I am facing issue to flash Kinetis KV10 using USBDM interface. I have KV10Z128M7 and When I am trying to detect USBDM is detecting KV10Z16M7 but not able to program it.   Seems, There is no support...
    Sunil Singh
    last modified by Sunil Singh
  • kinetis M chip(MKM34Z128CLL5) support in USBDM

    Hello Pgo, Thank you for the great work you have done in USBDM. I have a kinetis M chip(MKM34Z128CLL5) that I am programming on a custom board using the FRDKL25Z board and the USBDM firmware as outlined in your tuto...
    KIRUKI COSMAS
    last modified by KIRUKI COSMAS
  • Failed to resume target process. Downloading binary to target...

    Hi all, and particularly PGO, I'm experimenting issues with CodeWarrior10.6 and the USBDM with DSC MC56F8345 or MC56F84789 device. I have created a project and keep all default options. However, it is not possible t...
    wang yongsheng
    last modified by wang yongsheng
  • Fail to program MC9S08PT60 using USBDM, still can not fix that, who can save my life??

    Hi   I asked a question for programming  MC9S08PT60 but I could not get any answer. The problem now is it is detecting PT chip as PA chip and can't write anything in. The log files I already update them in ...
    Shucheng Zhu
    last modified by Shucheng Zhu
  • USBDM programmers (made in Brazil)

    Hello,   I´d like to announce to you all that my company is assemble three models of USBDM programmers: USBDM_JMxxCLD USBDM_SWD_SER_JS16CWJ USBDM_CF_JMxxCLD   If you are from Brazil or South Amer...
    Luciano Nicolau
    last modified by Luciano Nicolau
  • Windows 8 driver for USBDM?

    Hello I am using windows 8.0,     64bit. I wanted to use my FRDM board as a programmer for programming custom designed board containing kinetis uc i.e K10. but when I am installing USBDM drivers o...
    Amit Kumar
    last modified by Amit Kumar
  • USBDM API usage problems

    Hi,   i want to develop a new app that uses the USBDM interface and i have difficulties when i try to compile the USBDM_API_Example.cpp.   I am using codeblocks and mingw to compile the app but i keep gett...
    Padelis Floudas
    last modified by Padelis Floudas
  • Where to get a pcb for USBDM/CF?

    Hi there,   i m looking for a pcb or even better a fully assembled USBDM/CF device as this one USBDM/CF (JMxx Version): USBDM/CF (combined RS08/HCS08/HCS12/Coldfire V1,2,3,4/DSC/Kinetis code) for JM32/60  ...
    Padelis Floudas
    created by Padelis Floudas
  • how to use USBDM to program ARM device?

    Hi, pgo I made a USBDM.it's hardware is USBDM_CF_JMxxCLD_V3 and  firmware is USBDM_CF_JMxxCLD_V4.sx。USBDM version is 4.10.4. I use it to program HCS08 and it work perfectly.But when i use it to debug MKL05z32 a...
    baode wang
    last modified by baode wang
  • My USBDM failed when I flash MKL05Z32.

    I use USBDM to flash MKL05Z32.But I failed.a dialog comes out. Why? I have took several days to deal with the question.But I can't. Please help me.
    baode wang
    created by baode wang
  • USBDM - Version 4.10.4 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.4   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • TWR-56F8257 Bootloader problem

    Well, I jacked up my USB bootloader.  The TWR-56F8257 tower board uses the MC9S08JM60CLD to do its OSBDM programming and to main processor: the MC56F8257.    I tried to update the MC9S08JM60CLD using ...
    Daniel Bronson
    last modified by Daniel Bronson
  • USBDM - Version 4.10.2 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.2   Please post any queries on this version in a separate thread - I really can't cope with this new-fangled setup!   Documentation available at: SourceF...
    pgo
    last modified by pgo
  • confused about OSBDM and opensource JTAG

    hi guys,   I'm a new bee, I got a TWR-56F8257(tower motor control board with a 56F8257 DSC), and I'm trying to program it using code warrior 10.2, but in the new project wizard when I select the MC56F8257 device...
    kasun beddewela
    created by kasun beddewela