• How to make MCUXpresso support USBDM?

    Hi pgo, USBDM is very good to work. Now, I want to debug program through MCUXpresso and USBDM. but I'm first to do this. my USBDM version is 4.12.1. How to do it ? do you have document to illustrate it ?   than...
    baode wang
    created by baode wang
  • Expected BDM command ACK missing with USBDM 4.12 and JMxx firmware

    Hi to all the community.   I have an issue with the USBDM 4.12 and JMxx firmware. The resources i´m using are the following:   *- Board: (USBDM: USBDM RS08/HCS08/HCS12/Coldfire V1,2,3,4/D...) which u...
    martin mignone
    last modified by martin mignone
  • USBDM - Version 4.10.5 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.5   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • How to Check Installation of USBDM in Codewarrior 10

    The process to check the installation of USBDM in Codewarrior 10.x   Assumes the following: Codewarrior 10.6 installed Current version of USBDM installed (from USBDM - Browse /Version 4.12.1/Software at Source...
    pgo
    last modified by pgo
  • USBDM Updated to 4.11.1.20

    Dear All,   USBDM has been updated to version 4.11.1.20.   A video introduction is available at: USBDM with Kinetis Design Studio and Kinetis SDK - YouTube   The software is available at: USBDM | S...
    pgo
    last modified by pgo
  • 3phase BLDC driver program upload by CVF1 OSBDM/OSJTAG device

    Hello everyone!   I have 3PHASELV-KIT: 3-Phase BLDC/PMSM Low-Voltage Motor Control Drive and I have a question for that. I'm using it with HCS08MP16 daughter board. I also have MCF51CN board which I want to use ...
  • USBDM Programming Issue

    Hi ,   I am facing issue to flash Kinetis KV10 using USBDM interface. I have KV10Z128M7 and When I am trying to detect USBDM is detecting KV10Z16M7 but not able to program it.   Seems, There is no support...
    Sunil Singh
    last modified by Sunil Singh
  • tryUSBDM utility broke when installed USBDM 4.6.10.220.

    Using libusb 0.1.2.6.  TestLibUsb reports dll version 0.1.2.6, driver version -1.-1.-1.-1, and that's the problem.  tryUSBDM finds 1 bus with no devices even though device manager says there are 2.  HiW...
    Laurence Babcock
    last modified by Laurence Babcock
  • USBDM on coldfire V4 with GDB

    Hi, I have acquired a device that looks similar to USBDM/CF V3.1. I tried to use it with a MCF54415 and GDB. While I was able to initialize the system and load a program into DRAM there are still too many problems t...
    pint
    last modified by pint
  • USBDM programmers (made in Brazil)

    Hello,   I´d like to announce to you all that my company is assemble three models of USBDM programmers: USBDM_JMxxCLD USBDM_SWD_SER_JS16CWJ USBDM_CF_JMxxCLD   If you are from Brazil or South Amer...
    Luciano Nicolau
    last modified by Luciano Nicolau
  • Windows 8 driver for USBDM?

    Hello I am using windows 8.0,     64bit. I wanted to use my FRDM board as a programmer for programming custom designed board containing kinetis uc i.e K10. but when I am installing USBDM drivers o...
    Amit Kumar
    last modified by Amit Kumar
  • USBDM Linux 64-bit glib 2.13

    Hi   Are there any 64-bit builds available against glib 2.13 (as used by Debian 7)? Doesn't need to be latest (4.10.6 appears to be built against 2.14).     Thanks   Tim
    Tim Allen
    created by Tim Allen
  • USBDM API usage problems

    Hi,   i want to develop a new app that uses the USBDM interface and i have difficulties when i try to compile the USBDM_API_Example.cpp.   I am using codeblocks and mingw to compile the app but i keep gett...
    Padelis Floudas
    last modified by Padelis Floudas
  • Where to get a pcb for USBDM/CF?

    Hi there,   i m looking for a pcb or even better a fully assembled USBDM/CF device as this one USBDM/CF (JMxx Version): USBDM/CF (combined RS08/HCS08/HCS12/Coldfire V1,2,3,4/DSC/Kinetis code) for JM32/60  ...
    Padelis Floudas
    created by Padelis Floudas
  • Problem with PEMicro Virtual Serial Toolkit (TWR-MCF5441x board)

    I have a Tower setup with the SER2 module and the MCF5441x (coldFire) board. The board has updated firmware (31.21), the PEMicro USB drivers  are up-to-date as well. With the board connected, I can see the...
    Rob Withoff
    created by Rob Withoff
  • Slow download for Cyclone Max in CodeWarrior 10.4

    I am experiencing an issue with the Cyclone Max(7.76) in CodeWarrior 10.4. I am using a Coldfire MCF5270 for this project. I also have the exact same project running in CodeWarrior 10.2 without this issue.   In ...
    David Findlay
    created by David Findlay
  • USBDM - Version 4.10.0 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.0   Please post any queries on this version in this thread (maybe!),   Documentation available at: SourceForge Applications available at: SourceForge So...
    pgo
    last modified by pgo
  • Problem USB BDM (HCS08/HCS12/CFV1) with MCF51EM

    Hi,   I have a problem with programming the CFV1 Controller MCF51EM. In my testapplication for programming the controller in our production a new or unprogrammend controller needs an Power down/off of the contro...
    Sezgin Aktunc
    last modified by Sezgin Aktunc
  • USBDM - Version 4.10.4 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)

    Dear All,   USBDM has been updated to V4.10.4   Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!   Documentation available at: SourceFo...
    pgo
    last modified by pgo
  • Flash the TWR-MCF51CN-KIT outside CW?

    Hi all.   I wonder if exist another way to flash the 51CN MCU without using CodeWarrior, or a external BDM?. Only the embedded OSBDM on the tower module. Thanks! Ángel
    angel terrones
    last modified by angel terrones