• SPI write routine in C or Assembly for MC68HC16Z1 series of MCU

    Hello,   I am working on NXP 16 bit MC68HC16Z1 series of MCU and required immediate support to get SPI write routine in C code or Assembly code. It would be good, if someone will provide verified SPI r...
    vipul prajapati
    last modified by vipul prajapati
  • MCHC11F1CFNE4 DOES NOT CYCLE POWER AT TEMPERATURE GREATER THAN 110F

    Product: MCHC11F1CFNE4 Description: IC MCU 8BIT ROMLESS 68PLCC Product Packaging marking: MCHC11F1CFNE4 0M88Y QMZFY1920J   MCHC11F1CFNE4 1E63M QMZDT1107   Manufacturer: NXP/Freescale   Problem: MCU...
    Jonathan Alvarado
    last modified by Jonathan Alvarado
  • S08PT60 Evaluation Kit, lookinf for example code in C/C++

    Hello team,   My customer plan to work with #MC9S08PL4 and the closed EVK available is #S08PT60-EVK. when I started to work with S08 SDK (using code warrior 11.1) I found out that all the example code...
    Shai Berman
    last modified by Shai Berman
  • S08PT60-EVK: looking for full manual guide

    Hello team,   I am looking for full manual guide for s08pt60-evk since I am planning to use the EVK BDM programmer to flash an external target device and the only guide I have found on NXP website is S08PT6...
    Shai Berman
    last modified by Shai Berman
  • P89LPC922 Security bits

    Hi everybody, I have microcontroller LPC922 and he has some sectors locked with security bits ( 0x07 ). In the documentation is written ( as I understood ) that "global erase" shall clear these bits with 0x00  ...
    Rafal Obirek
    last modified by Rafal Obirek
  • Problem with AN3927 using JM60 in windows 10

    Hello, i'm trying to use AN3927 for a msd booloader on JM60, but, always there's a error message "Device cannot start(code 10)" in device manager. I'm using Wireshark to see the communication between host and device(...
    Eduardo Kamada
    last modified by Eduardo Kamada
  • Bus LIN solution

    Hello,   We must design a small industrial application with some Inputs/Outputs (Logical Input/Outputs, Analog input) RS485 and then a LIN BUS (slave)   Which small CPU could you advice to me  to sup...
    arnogir
    last modified by arnogir
  • NXP Model Based Design Toolbox for S32K

    The chip I use is S32K144,The compiler is S32IDE FOR RAM.In the course of using MATLAB, I found that the supported compilers were only IAR, GCC, but no S32IED FOR RAM.How can I configure it?
    zhigang dai
    last modified by zhigang dai
  • what are the programming pins of P87C51MC2? which Programmer can i use ?

    Hello Guys,    I want to use the microcontroller P87C51MC2 of NXP, but i can't understand how to program it. can anyone help me to know which pins are used for the programming and if there is any programme...
    Karim Ben Ali
    last modified by Karim Ben Ali
  • USB Stack MSD with JM60

    Hello,  I'm trying to put a FAT(File Allocation Table) in the code of USB Stack for MC9S08JM60, but i observed the Write(10) Command never be called. Do you know how to fix this or got some example with MSD + FAT...
    Eduardo Kamada
    last modified by Eduardo Kamada
  • Using the S08RN60 MCU for controlling a DC motor with Touch electrodes.

    Open video

    CarlosCasillas
    last modified by CarlosCasillas
  • Pls help confirm if the marking of TEA1751AT/N1/S35518

    Hello,   We bought the part of TEA1751AT/N1/S35518 from Rochester,  the marking  is "CP015ND   CDT796   TXD14131".Ro...
    Chen Gloria
    last modified by Chen Gloria
  • Implementing FAT16 on JM60 USB Stack 4.11

    Hello, I need an implementation of FAT16 in a JM60 microcontroller, but i don't know how to start it. Is there an example with FAT16 and MSD with internal flash for study? I don't need to storage large files, just ne...
    Eduardo Kamada
    last modified by Eduardo Kamada
  • 68HC705 PLCC44 replacer?

    We have an old design that uses a MC68HC705C8ACFN microcontroller. The firmware really needs an update, but we are using a PLCC44 version of this part and as I see, there is really nothing that can drop down on t...
    john backman
    last modified by john backman
  • How to vector redirect S08PT

    Design bootloader and application,this is my memory map: boot address:0xE000-0xFFFF app address:0x3200-0xFDFF set flash protection higher address range is 8Kbytes This is my NVPROT register config: NVPROT_INIT @0...
    chen kean
    last modified by chen kean
  • tfa9879 audio chip python

    Hi Sir   I need to use python 2.7 to communicate with  tfa9879 audio chip  Do you have any API for python to use?   Function I need is change the audio sound level   which means I call a funct...
    Junye Ye
    last modified by Junye Ye
  • LPC922 Marking

    LPC922 Marking   Hello Is there any information regarding P89LPC922F marking ? The label which is sticked on ESD bag does not mention explicitly anywhere that the part inside the bag is LPC922 It has  a ...
    ionut Ionut
    last modified by ionut Ionut
  • MC9S08PL4 schematics review

    Hello Team,   My Customer has a plan to use MC9S08PL4 and they want to review their schematics and get your recommendations for the mass-production stage, can I open a private ticket to be able to share the...
    Shai Berman
    last modified by Shai Berman
  • S08PL 10-bit ADC not recognized by Codewarrior

    I'm downsizing some projects from S08PA to S08PL and I've got some strange behaviour on CW 10.7. CW does not recognize the 10-bit ADC option and only allows 8-bit ADC mode. I've installed CW 11.1 but the problem conti...
    Celso Monteiro
    last modified by Celso Monteiro
  • Looking for the old Freescale Learning Accademy resources

    Hello, time ago i watch some educational videos from the Freescale website about how to create a c# GUI for DEMOJM, and if I remember right also some etpu relate videos. Now I can't find that videos in the NXP site; A...
    damien darhk
    last modified by damien darhk