yocto mono layer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto mono layer

1,642 Views
tüskemáté
Contributor I

   Hi,

I'm working on a system where i can run c# applications in raspberry pi. I'm just switched to yocto rocko, and somehow now I always fail on the do_package_qa task. This is my error message:

ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(System.Xml), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Utilities.v3.5.dll contained in package mono-libs-3.5 requires mono(System), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(mscorlib), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(mscorlib), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Xml), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Configuration), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(Mono.Security), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.2-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.2 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.2? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.7-api/Mono.Debugger.Soft.dll contained in package mono-api-4.7 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.7? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/xbuild/Microsoft/NuGet/Microsoft.NuGet.Build.Tasks.dll contained in package mono-xbuild requires mono(mscorlib), but no providers found in RDEPENDS_mono-xbuild? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.1-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.1 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.1? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/gac/Mono.Messaging.RabbitMQ/4.0.0.0__0738eb9f132ed756/Mono.Messaging.RabbitMQ.dll contained in package mono-gac requires mono(mscorlib), but no providers found in RDEPENDS_mono-gac? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.5/Microsoft.CodeAnalysis.Scripting.dll contained in package mono-libs-4.5 requires mono(System.Runtime.Loader), but no providers found in RDEPENDS_mono-libs-4.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA run found fatal errors. Please consider fixing them. 
ERROR: mono-5.4.1.6-r0 do_package_qa: Function failed: do_package_qa

My mono version is 5.8.0.108 from http://download.mono-project.com/repo/ubuntu  and I'm using xenial ubuntu. The local.conf is now the sample from here:https://git.yoctoproject.org/cgit.cgi/poky/plain/meta-poky/conf/local.conf.sample . 

Any suggestion?

regards

Matthew

Labels (1)
Tags (3)
2 Replies

988 Views
a_spin
Contributor I

I'm experiencing the same problem.

Did this document solve you're problem, I didn't find a clue in it.

Regards,

Alberto

0 Kudos

988 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Matthew,

The Mono layer is not present on the i.MX BSPs so I’m not familiar with it, but there seems to be problems with dependencies for adding mono. If you are using Yocto perhaps the following document on the Yocto Project Wiki may help.

https://wiki.yoctoproject.org/wiki/Building_and_running_embedded_Linux_.NET_applications_from_first_...

Regards,