MQX系统 在 k64 总线 扩展 双网口 两个dm9000a 问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX系统 在 k64 总线 扩展 双网口 两个dm9000a 问题

3,291 Views
yongzhenyan
Contributor I

单独初始化 其中任何一个 网口都好用;把两个都开,两个都不好用,两个都配置为服务器。大牛给看下有没有遇到过
只开2口程序:(开两个时i从1开始循环)
    /* Bind IP address for each interface */
    for (i = 2; i <=2; i++)
    {
        _enet_address           address;
        uint32_t                 phy_addr;
       // uint32_t                 sock;

       // sock = socket(AF_INET,SOCK_STREAM,0);
        phy_addr = i;
        if(i==2)
        ip_addr = IPADDR(A1,B1,C1,D1);
        else
          if(i==1)
            ip_addr = IPADDR(config1[5],config1[6],config1[7],config1[8]);  

        ENET_get_mac_address(phy_addr, ip_addr, address);

        /* Init ENET device */
        error = ipcfg_init_device (phy_addr, address);
        if (error != RTCS_OK)
        {
            printf("IPCFG: Device n.%d init failed. Error = 0x%X\n", i, error);
            _task_set_error(MQX_OK);
            n_devices--;
            i--;
            continue;
        }

        #if RTCSCFG_ENABLE_IP4
        ip_data.ip      = ip_addr;
        ip_data.mask    = IPADDR(config1[9],config1[10],config1[11],config1[12]);
       // if(i==1)
        ip_data.gateway = IPADDR(config1[13],config1[14],config1[15],config1[16]);
        /* Bind IPv4 address */
        error = ipcfg_bind_staticip (phy_addr, &ip_data);
        if (error != RTCS_OK)
        {
         //   printf("\nIPCFG: Failed to bind IP address. Error = 0x%X", error);
            _task_block();
        }
        #endif

    }

网口1任务:
void net1_rev_task(uint32_t initial_data)
{
uint32_t listensock,error,length;
uint16_t len;
int32_t          value = 256;
sockaddr_in  addr,addrin;
//char str[200];
listensock = socket(AF_INET,SOCK_STREAM,0);
addr.sin_addr.s_addr = ip_addr[1];
//addr.sin_addr.s_addr = INADDR_ANY;
addr.sin_family = AF_INET;
addr.sin_port = config1[17];
error = bind(listensock,&addr,sizeof(addr));
error = listen(listensock,5);
while(1)

{任务程序}
}
网口2任务程序:
void net2_rev_task(uint32_t initial_data)
{
uint32_t sock1,listensock1,error1,length1;
uint16_t len1;
int32_t          value1 = 256;
sockaddr_in  addr1,addrin1;
//char str[1200];
listensock1 = socket(AF_INET,SOCK_STREAM,0);
addr1.sin_addr.s_addr = ip_addr[2];
//addr.sin_addr.s_addr = INADDR_ANY;
addr1.sin_family = AF_INET;
addr1.sin_port = 205;
error1 = bind(listensock1,&addr1,sizeof(addr1));
error1 = listen(listensock1,5);

//setsockopt(listensock,SOL_TCP,OPT_TBSIZE,&value,sizeof(value));
   while(1)
   {

  任务程序
}
}

0 Kudos
Reply
4 Replies

2,984 Views
yongzhenyan
Contributor I

两个网口的链路链接指示灯都能亮,但是IP ping不通。感觉是这个定义有问题:

 const ENET_IF_STRUCT ENET_1 = {
&DM9000_IF,
&phy_dm9000_IF,
DM9000_DEVICE_MAC_1,//1
DM9000_DEVICE_PHY_0,//1
BSP_ENET1_PHY_ADDR,//0
BSP_ENET1_PHY_MII_SPEED
};
const ENET_IF_STRUCT ENET_2 = {
&dm9000_1_IF,
&phy_dm9000_1_IF,
2,
2,
0,
BSP_ENET1_PHY_MII_SPEED
};

0 Kudos
Reply

2,984 Views
danielchen
NXP TechSupport
NXP TechSupport

检查下2个DM9000A的MAC地址都是唯一的吗?

0 Kudos
Reply

2,984 Views
yongzhenyan
Contributor I

从下面这几个函数看,MAC地址是IP地址生成的,是不一样的。现在两个网卡都初始化完后(两个网口的链路连接指示灯都亮起了),好像程序堵塞了,创建sock的 任务进程不能转入。创建sock的任务在初始化两个网卡函数的最后。仿真时程序能跑到_task_create(0,20, 0);,这个创建函数,但是把断点打在这个函数内部,没任何反应。暂停查看MQX任务中有TCPIP任务,但是SOCK没创建成功。

只初始化一个网卡时,就能正确的执行创建sock任务。

#define A1   192
#define B1   168
#define C1   1
#define D1   120

#define BSP_DEFAULT_ENET_OUI                { 0x00, 0x00, 0x5E, 0, 0, 0 }

const _enet_address _enet_oui = BSP_DEFAULT_ENET_OUI;

//////////////////////////////////////////////////////////////////////////

void init_net_task(void)//网卡初始化函数
{
int32_t error;
uint32_t server[BSP_ENET_DEVICE_COUNT];

uint32_t i = 0;
char* indexes[BSP_ENET_DEVICE_COUNT];
uint8_t n_devices = BSP_ENET_DEVICE_COUNT;
#if !HTTP_USE_ONE_SERVER
uint8_t n_servers = BSP_ENET_DEVICE_COUNT;
#else
uint8_t n_servers = 1;
#endif

_int_install_unexpected_isr();

/* Init RTCS */
_RTCSPCB_init = 4;
_RTCSPCB_grow = 2;
_RTCSPCB_max = 8;

_RTCSTASK_stacksize = 4500;

error = RTCS_create();
if (error != RTCS_OK)
{
printf("RTCS failed to initialize, error = 0x%X\n", error);
_task_block();
}

_IP_forward = TRUE;

/* Bind IP address for each interface */
for (i = 1; i <=2; i++)
{
_enet_address address;
uint32_t phy_addr;
// uint32_t sock;

// sock = socket(AF_INET,SOCK_STREAM,0);
phy_addr = i;
if(i==2)
ip_addr[i] = IPADDR(A1,B1,C1,D1);
else
if(i==1)
ip_addr[i] = IPADDR(config1[5],config1[6],config1[7],config1[8]);

ENET_get_mac_address(phy_addr, ip_addr[i], address);

/* Init ENET device */
error = ipcfg_init_device (phy_addr, address);
if (error != RTCS_OK)
{
printf("IPCFG: Device n.%d init failed. Error = 0x%X\n", i, error);
_task_set_error(MQX_OK);
n_devices--;
i--;
continue;
}

#if RTCSCFG_ENABLE_IP4
ip_data.ip = ip_addr[i];
ip_data.mask = IPADDR(config1[9],config1[10],config1[11],config1[12]);
if(i==1)
ip_data.gateway = IPADDR(config1[13],config1[14],config1[15],config1[16]);
/* Bind IPv4 address */
error = ipcfg_bind_staticip (phy_addr, &ip_data);
if (error != RTCS_OK)
{
// printf("\nIPCFG: Failed to bind IP address. Error = 0x%X", error);
_task_block();
}
#endif

}
//userftp_init();
_task_create(0,20, 0); //创建sock函数
}

//////////////////////////////////////////////////////////////////////////////////////////////////////

bool _bsp_get_mac_address//获取网卡地址函数
(
uint32_t device,
uint32_t value,
_enet_address address
)
{ /* Body */
if (device >= BSP_ENET_DEVICE_COUNT)
return FALSE;

switch (device) {
case 0:
address[0] = _enet_oui[0];
address[1] = _enet_oui[1];
address[2] = _enet_oui[2];
address[3] = (value & 0xFF0000) >> 16;
address[4] = (value & 0xFF00) >> 8;
address[5] = (value & 0xFF);
break;
case 1:
/* Try to get mac from eeprom first */
//dm9000_get_mac_address(address);
//if (is_valid_ether_addr(address))
// break;
address[0] = _enet_oui[0];
address[1] = _enet_oui[1];
address[2] = _enet_oui[2];
address[3] = (value & 0xFF0000) >> 16;
address[4] = (value & 0xFF00) >> 8;
address[5] = (value & 0xFF);
break;
case 2:
/* Try to get mac from eeprom first */
//dm9000_get_mac_address(address);
//if (is_valid_ether_addr(address))
// break;
address[0] = _enet_oui[0];
address[1] = _enet_oui[1];
address[2] = _enet_oui[2];
address[3] = (value & 0xFF0000) >> 16;
address[4] = (value & 0xFF00) >> 8;
address[5] = (value & 0xFF);
break;
default:
break;
}

return TRUE;

}

0 Kudos
Reply

2,984 Views
danielchen
NXP TechSupport
NXP TechSupport

先不要开启服务器, 2个网口同时启用,配置各自的IP , 两个网口能正常工作吗?

0 Kudos
Reply