Dear Community,
We are working on IMX6 SODIMM based board with Linux4.1.15 Yocto Krogoth.
Requirement:
When testing the imx6 device using USB OTG as device, internal (eMMC) and external (micro SD) on the board should be accessible simultaneously on host PC (as like in mobile phones).
We are able to test USB OTG as a device by loading and unloading the USB gadget modules but simultaneous accessing of eMMC and micro SD was not achieved. We have also checked in community discussion but could not able find any discussion on it.
Below are the steps followed with observations,
Could you please let us know the method to access both eMMC and mSD simultaneously on host PC.
Thanks in advance.
Regards,
Ambika
You can refer to https://community.nxp.com/docs/DOC-335434