Hi Daniel,
I use the S32K144 EVB. I have flashed the rbf file first. But I can’t connect with the RappID BL tool.
The trace window of RappID BL Tool is empty an then after timeout the Error message comes:
There are different kinds of the rbf file for the s32K144 CPU?
BR Lutz
Von: dumitru-daniel.popa
Gesendet: Donnerstag, 31. August 2017 11:07
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: RappID Bootloader S32K144
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: RappID Bootloader S32K144
reply from dumitru-daniel.popa<https://community.nxp.com/people/dumitru-daniel.popa?et=watches.email.thread> in S32K - View the full discussion<https://community.nxp.com/message/938696?commentID=938696&et=watches.email.thread#comment-938696>